Last edited 5 months ago

How to use the Cortex-M0+

Applicable for STM32MP25x lines

1. Article purpose[edit | edit source]

This article describes the configuration of the Cortex®-M0+ and its related resources, and how to run a Cortex®-M0+ firmware through a low power demonstration application. The purpose of this application is to demonstrate a low power use case and a communication use case between the Cortex®-M0+ and Cortex®-A35.

Information
  • ecosystem release v6.0.0  : The Cortex®-M0+ demonstration application is only available for STM32MP257x-EV1 Evaluation board .
  • ecosystem release ≥ v6.1.0  : The Cortex®-M0+ demonstration application is available for STM32MP257x-EV1 Evaluation board and STM32MP257x-DK Discovery kit .

2. Introduction[edit | edit source]

The Cortex®-M0+ acts as a remote processor with access to limited resources, peripherals, and memories. The Cortex®-M0+ processor is dedicated to executing small tasks that require few resources. It runs in a separate SmartRun domain, allowing other domains to be turned off to achieve low power consumption.

3. Resources access from Cortex®-M0+[edit | edit source]

3.1. Memories[edit | edit source]

The Cortex®-M0+ can only use the LPSRAM memories for a total of 32KB, with the following memory mapping:

  • LPSRAM1 : 0x200C0000 - 0x200C1FFF (8KB)
  • LPSRAM2 : 0x200C2000 - 0x200C3FFF (8KB)
  • LPSRAM3 : 0x200C4000 - 0x200C7FFF (16KB)
Information
In the STM32MPU Embedded Software distribution, the memory mapping of the LPSRAM must be defined between 0x200C0000 and 0x200C7FFF.

3.2. Peripherals[edit | edit source]

The Cortex®-M0+ can only access a limited set of peripherals:

  • LPTIM3, LPTIM4, LPTIM5
  • SPI8
  • LPUART1
  • I2C8
  • ADF1C
  • GPIOZ
  • LPDMA
  • RTC
  • I3C4
  • IPCC2
  • EXTI2
  • HSEM

3.3. Other resources[edit | edit source]

The Cortex®-M0+ can also access other resources such as:

  • PWR
  • CoreSight Debug through 2 ports:
    • The SWD (Serial Wire Debug)
    • The SWJ-DP (Serial Wire JTAG-Debug Port)
Information
The Cortex®-M0+ has no access to RCC resources (for clock configuration, for example). This implies that clock gating must be managed by the Cortex®-A35 (Linux kernel or OP-TEE).

3.4. Security[edit | edit source]

All memories, peripherals, and resource access rights are managed by the Resource Isolation Framework (RIF) in the Cortex®-A35 OP-TEE.

3.4.1. Memories RIF configuration example[edit | edit source]

The OP-TEE STM32MP2_firewall_configuration of the LPSRAM memories must allow loading the M0+ firmware image by the Cortex®-A35 Linux kernel remoteproc framework and execution of the firmware on the Cortex®-M0+.

In the following OP-TEE device tree example, LPSRAM 1/2/3 (RISAL_ID 1/2/3 respectively) are configured as shared memory (subregion A and subregion B) between the Cortex®-A35 (RID_CID1) and Cortex®-M0+ (RIF_CID3):

	st,risal = <
		RISALPROT(RISAL_ID(1), RIFSC_RISAL_BLOCK_A, RIF_CID1, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
		RISALPROT(RISAL_ID(2), RIFSC_RISAL_BLOCK_A, RIF_CID1, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
		RISALPROT(RISAL_ID(3), RIFSC_RISAL_BLOCK_A, RIF_CID1, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
		RISALPROT(RISAL_ID(1), RIFSC_RISAL_BLOCK_B, RIF_CID3, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
		RISALPROT(RISAL_ID(2), RIFSC_RISAL_BLOCK_B, RIF_CID3, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
		RISALPROT(RISAL_ID(3), RIFSC_RISAL_BLOCK_B, RIF_CID3, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIFSC_RISAL_SREN)
	>;

3.4.2. Peripherals RIF configuration example[edit | edit source]

The RIF access rights are applied to the peripherals and their associated RCC registers. If the Cortex®-M0+ controls the peripheral, the Cortex®-A35 must configure the associated RCC registers before starting the Cortex®-M0+. For this reason, the peripherals' RIF access rights must be allowed for both the Cortex®-A35 and the Cortex®-M0+.

In the following example, the LPUART1 is configured without any filtering to allow access to LPUART1 by both the Cortex®-A35 and the Cortex®-M0+:

&rifsc {
	st,protreg = <
	[...]
		RIFPROT(STM32MP25_RIFSC_LPUART1_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_NPRIV, RIF_UNUSED, RIF_SEM_DIS, RIF_CFDIS)
	[...]
	>;
	st,glocked = <RIFSC_RIMU_GLOCK>;
};


3.5. Low power constraints[edit | edit source]

The Cortex®-M0+ can be used during low power modes, while the Cortex®-A35 and Cortex®-M33 are stopped. A dedicated autonomous mode is available for each peripheral that can be allocated to the Cortex®-M0+ to avoid stopping peripheral clocks during Cortex®-A35 low power.

Information
On ecosystem release v6.0.0 the Cortex®-M0+ can only run during LP-Stop2 low power mode.

4. Linux Kernel configuration[edit | edit source]

  • To manage the Cortex®-M0+, activate the Cortex®-M0+ remoteproc driver by enabling the STM32_M0_RPROC build configuration.
  • To communicate with the Cortex®-M0+, activate the mailbox char device client by enabling the MAILBOX_CDEV build configuration.

5. Linux Kernel device tree configuration[edit | edit source]

The Cortex®-M0+ lifecycle is managed by the Linux kernel remoteproc framework. To configure the Cortex®-M0+, you mainly need:

  • to define the memory mapping,
  • to define the m0_rproc node in the device tree,
  • to define the mailbox char device client node configuration.

5.1. Memory configuration[edit | edit source]

In the STM32MPU Embedded Software distribution, the default memory configuration is split into 3 memory regions that can be customized:

  • Code  : 16KB (LPSRAM1 & LPSRAM2)
  • Data  : 8KB (LPSRAM3)
  • Shared Memory : 8KB (LPSRAM3)

The shared memory is used to share data between Cortex®-M0+ and Cortex®-A35 through interprocessor communication and mailbox mechanisms.

reserved-memory {
	[...]

	cm0_cube_fw: cm0-cube-fw@200C0000 {
		compatible = "shared-dma-pool";
		reg = <0x0 0x200C0000 0x0 0x4000>;
		no-map;
	};

	cm0_cube_data: cm0-cube-data@200C4000 {
		compatible = "shared-dma-pool";
		reg = <0x0 0x200C4000 0x0 0x2000>;
		no-map;
	};

	ipc_shmem_2: ipc-shmem-2@200C6000{
		compatible = "shared-dma-pool";
		reg = <0x0 0x200C6000 0x0 0x2000>;
		no-map;
	};
};
Information
This memory mapping needs to be aligned with the Cortex®-M0+ Cube Firmware memory mapping (linker script).

5.2. Remoteproc configuration[edit | edit source]

  • The memory-region property should list the memories used for firmware execution.
  • The clocks property should list the peripheral clocks used by the Cortex®-M0+.
&m0_rproc {
	memory-region = <&cm0_cube_fw>, <&cm0_cube_data>;
	clocks = <&rcc CK_CPU3>,              /* Enable Cortex-M0+ clock */
		 <&rcc CK_CPU3_AM>,               /* Enable Cortex-M0+ autonomous mode */
		 <&rcc CK_LPUART1_C3>,            /* Allocate LPUART1 to Cortex-M0+ */
		 <&rcc CK_KER_LPUART1>,           /* Enable LPUART1 clock */
		 <&rcc CK_LPUART1_AM>,            /* Enable LPUART1 autonomous mode */
		 <&scmi_clk CK_SCMI_IPCC2>,       /* Enable IPCC2 clock */
		 <&scmi_clk CK_SCMI_IPCC2_AM>;    /* Enable IPCC2 autonomous mode */
	status = "okay";
};

5.3. Mailbox client configuration[edit | edit source]

The memory-region property should list the memory used for interprocessor communication (shared memory).

mbox_client: mailbox-client@1 {
	compatible = "mbox-cdev";
	reg = <1 0>;
	memory-region = <&ipc_shmem_2>;
	mboxes = <&ipcc2 0>;
	mbox-names = "rx-tx";
	status = "okay";
};

6. Cortex®-M0+ demonstration[edit | edit source]

The Cortex®-M0+ demonstration shows the Cortex®-A35 waking up from low power mode (LP-Stop2) triggered by the Cortex®-M0+.

The demonstration application includes:

  • Starting the Cortex®-M0+ firmware through the remoteproc driver.
  • Configuring a wakeup delay in the Cortex®-M0+ firmware from Linux userland (Cortex®-A35) using IPCC communication, shared memory, and mailbox mechanisms.
  • Setting the LP-Stop2 low power mode.
  • Waking up the Cortex®-A35 from the Cortex®-M0+ firmware via an interrupt after the programmed delay expires.

6.1. STM32Cube Firmware application[edit | edit source]

The Cortex®-M0+ STM32Cube Firmware application is available as an example in the STM32CubeMP2 Firmware Package. It allows waking up the Cortex®-A35 from low power mode after a programmed delay.

This application uses the following features:

  • LPUART1: to print messages on the console.
  • IPCC2: to send/receive notifications between Cortex®-M0+ and Cortex®-A35 through interprocessor communication (interrupt).
  • Shared Memory: to share data between Cortex®-M0+ and Cortex®-A35.


The purpose of this application is to:

  • Initialize LPUART1 for printing messages on the console.
  • Initialize IPCC2 for communication between Cortex®-M0+ and Cortex®-A35.
  • Print a message on LPUART1 every 2 seconds.
  • Wait for an IPCC2 interrupt corresponding to a message received in shared memory from Cortex®-A35.
    • Once the IPCC2 interrupt is received, the firmware:
      • Reads the first 4 bytes from shared memory, representing the delay before sending a notification to Cortex®-A35.
      • Starts a delay with the value read from shared memory.
      • Once the delay has elapsed, sends a notification through IPCC2 to wake up Cortex®-A35.
  • Continues printing the default message on LPUART1 and waits for new messages from Cortex®-A35.

6.2. Board and connectors[edit | edit source]

6.2.1. STM32MP257x-EV1 Evaluation board [edit | edit source]

Main access to Cortex®-M0+ is through the MikroBUS connector.

To use LPUART1, connect a 3-wire USB-to-TTL Serial UART debug cable to the MikroBUS connector:

  • LPUART1_TX
  • LPUART1_RX
  • GND

6.2.2. STM32MP257x-DK Discovery kit [edit | edit source]

Main access to Cortex®-M0+ is through the GPIO expansion connector.

To use LPUART1, connect a 3-wire USB-to-TTL Serial UART debug cable to the GPIO expansion connector:

  • EXP_GPIO25 (LPUART1_TX)
  • EXP_GPIO26 (LPUART1_RX)
  • GND

6.3. How to debug Cortex®-M0+[edit | edit source]

Debugging the Cortex®-M0+ can be done in two ways depending on the Cortex®-A35 state:

  • When Cortex®-A35 is running, debug Cortex®-M0+ via the STLINK connector.
  • When Cortex®-A35 is in low power mode, debug Cortex®-M0+ via the SWD port.
Warning
The hardware allows using STLINK while in low power mode, but this maintains some regulators and clocks. To debug Cortex®-M0+ in LP-Stop2 low power mode, it is recommended to use the dedicated SWD port.

To use the SWD interface, you need to:

  • Connect the debugger to the MikroBUS connector pins MISO, MOSI, 3.3V, and GND.
  • Enable the SWD debug interface for Cortex®-M0+ by clearing the bit DBG_SWD_SEL_N in the DBGMCU_CR register.

6.4. How to run the Cortex®-M0+ demonstration application[edit | edit source]

The Cortex®-M0+ firmware image must be copied to the /lib/firmware folder in the Linux root filesystem. By default, the Cortex®-M0+ firmware is named CM0PLUS_Demo_NonSecure.elf.

  • Go to the firmware directory and verify that the Cortex®-M0+ firmware is available:
 cd /lib/firmware
  • Stop the Cortex®-M33 firmware:
 echo stop > /sys/class/remoteproc/remoteprocX/state
  • Configure the Cortex®-M0+ firmware:
 echo CM0PLUS_Demo_NonSecure.elf > /sys/class/remoteproc/remoteproc1/firmware
  • Start the Cortex®-M0+ firmware:
 echo start > /sys/class/remoteproc/remoteproc1/state
Example kernel log output:
[ 1245.086086] remoteproc remoteproc1: powering up Cortex-M0+
[ 1245.120304] remoteproc remoteproc1: Booting fw image CM0PLUS_Demo_NonSecure.elf, size 1017852
[ 1245.123454] remoteproc remoteproc1: remote processor Cortex-M0+ is now up


  • Enable IPCC2 wakeup source for Cortex®-A35 wakeup:
 echo enabled > /sys/devices/platform/soc@0/46250000.mailbox/power/wakeup
  • Configure the delay (in seconds) to Cortex®-M0+ before waking up Cortex®-A35 (e.g., 7 seconds):
 echo 7 > /dev/mailbox0
Cortex®-M0+ logs from LPUART1:
**** CM0PLUS Example application ****
(1) Hello from CM0+
(2) Hello from CM0+
(3) Hello from CM0+
(4) Hello from CM0+
(5) Hello from CM0+
(5) A35 wakeup request in 7s
  • Set Cortex®-A35 to low power mode (for 30 seconds):
rtcwake --date +30sec -m mem
Cortex®-A35 logs from Linux console:
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using /dev/rtc0 at Sat Jan  1 00:52:30 2000
[  797.167571] PM: suspend entry (deep)
[  797.168528] Filesystems sync: 0.000 seconds
[  797.178966] Freezing user space processes
[  797.181214] Freezing user space processes completed (elapsed 0.002 seconds)
[  797.184365] OOM killer disabled.
[  797.187645] Freezing remaining freezable tasks
[  797.193174] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  797.292727] stm32-dwmac 482c0000.eth1 end1: FPE workqueue stop
[  797.293244] stm32-dwmac 482d0000.eth2 end0: FPE workqueue stop
[  797.302189] Disabling non-boot CPUs ...
[  797.304328] psci: CPU1 killed (polled 0 ms)
INFO:    Entering Standby1 low power mode}}
  • Cortex®-A35 wakeup:
  • Cortex®-M0+ logs from LPUART1:
(5) A35 wakeup request done!
(6) Hello from CM0+
  • Cortex®-A35 logs from Linux console:
NOTICE:  CPU: STM32MP257FAI Rev.?
NOTICE:  Model: STMicroelectronics STM32MP257F-EV1 Evaluation Board
NOTICE:  Board: MB1936 Var1.0 Rev.C-01
NOTICE:  Reset reason: System exits from Standby for CA35 (0xd02030)
INFO:    PMIC2 version = 0x11
INFO:    PMIC2 product ID = 0x20
[...]
[  797.473956] Enabling non-boot CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[  797.485464] Detected VIPT I-cache on CPU1
[  797.485540] CPU1: Booted secondary processor 0x0000000001 [0x411fd040]
[  797.486106] CPU1 is up
[  797.495505] i2c 0-001a: Unbalanced pm_runtime_enable!
[  797.537097] dwmac4: Master AXI performs any burst length
[  797.537154] stm32-dwmac 482c0000.eth1 end1: No Safety Features support found
[  797.745753] stm32-dwmac 482c0000.eth1 end1: IEEE 1588-2008 Advanced Timestamp supported
[  797.748476] stm32-dwmac 482c0000.eth1 end1: FPE workqueue start
[  797.754080] stm32-dwmac 482c0000.eth1 end1: configuring for phy/rgmii-id link mode
[  797.977092] dwmac4: Master AXI performs any burst length
[  797.977134] stm32-dwmac 482d0000.eth2 end0: No Safety Features support found
[  797.983804] stm32-dwmac 482d0000.eth2 end0: IEEE 1588-2008 Advanced Timestamp supported
[  797.991954] stm32-dwmac 482d0000.eth2 end0: FPE workqueue start
[  797.997751] stm32-dwmac 482d0000.eth2 end0: configuring for phy/rgmii-id link mode
[  798.486930] onboard-usb-hub 1-1: reset high-speed USB device number 2 using ehci-platform
[  798.752327] OOM killer enabled.
[  798.752360] Restarting tasks ... done.
[  798.759329] random: crng reseeded on system resumption
[  798.766896] PM: suspend exit

7. Code source[edit | edit source]

7.1. Linux kernel[edit | edit source]

drivers/remoteproc/stm32_m0_rproc.c 
drivers/mailbox/mailbox-client_cdev.c 
arch/arm64/boot/dts/st/stm32mp257f-ev1.dts 
arch/arm64/boot/dts/st/stm32mp257f-dk.dts  (ecosystem release ≥  v6.1.0  )

7.2. STM32Cube applications[edit | edit source]

Projects/STM32MP257F-EV1/Demonstrations/CM0PLUS_DEMO 
Projects/STM32MP257F-DK/Demonstrations/CM0PLUS_DEMO  (ecosystem release ≥  v6.1.0  )