The STM32Cube MPU Packages[1] are the embedded software bricks of the STM32Cube ecosystem[2], made to run on STM32 microprocessors.
The following STM32Cube MPU Packages are available:
- STM32CubeMP13 Package, running on the Arm® Cortex®-A7 processor, for the STM32MP13x lines

STM32Cube MPU packages offer all the required embedded software bricks to operate the available set of peripherals, including:
- The hardware abstraction layer (HAL) enabling portability between different STM32 devices via standardized API calls
- Low-layer (LL) APIs, and a lightweight, optimized, expert-oriented set of APIs designed for both performance and runtime efficiency
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
- A collection of middleware components including RTOS (such as FreeRTOS or Azure RTOS ThreadX), USB library,...
- A collection of applications, running on an MPU board and allowing demonstration of a basic implementation of features from middleware
- The BSP drivers are based on HAL drivers and provide an API set for the evaluation boards and third-party components.
Pages in category "STM32CubeMP13 Package"
The following 6 pages are in this category, out of 6 total.
H
- How to ensure data coherency when cache and MMU used in STM32CubeMP13
- How to install X-TouchGFX MPU Addon
- How to load and start STM32CubeMP13 applications via eMMC storage
- How to load and start STM32CubeMP13 applications via microSD card
- How to load and start STM32CubeMP13 applications via SNOR flash