Last edited one year ago

How to tune RGMII GTX clock delay

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Introdution[edit | edit source]

RGMII requires a skew between the clock and data signals, as they are generated simultaneously by the transmitting source.

This skew is usually introduced through PCB trace routing. However, if the actual skew between the GTX clock and data signals is not large enough, it is possible to add an extra delay on the GTX clock signal from the STM32MP2 itself.

A tool named stm32mp25-rgmii-gtx-clock-delay was especially developed for that purpose.

2. How to install this tool[edit | edit source]

As of writing this, the tool is not available by default on any OpenSTLinux images. Therefore, it must be manually installed into the target root file-system. This can be done directly from the target if it has an internet connection:

wget https://github.com/STMicroelectronics/wiki-stm32mp-addons/raw/main/stm32mp25-rgmii-gtx-clock-delay/bin/stm32mp25-rgmii-gtx-clock-delay --output /usr/bin/stm32mp25-rgmii-gtx-clock-delay

Another way is to transfer the tool from a PC to the target file-system. For instance, assuming users can access the target root file system through /dev/sdXY on their PC:

mount /dev/sdXY/mnt
wget https://github.com/STMicroelectronics/wiki-stm32mp-addons/raw/main/stm32mp25-rgmii-gtx-clock-delay/bin/stm32mp25-rgmii-gtx-clock-delay --output /mnt/usr/bin/stm32mp25-rgmii-gtx-clock-delay
chmod +x /mnt/usr/bin/stm32mp25-rgmii-gtx-clock-delay
umount /mnt

3. How to use this tool[edit | edit source]

The tool 'stm32mp25-rgmii-gtx-clock-delay' can be used to automatically find the best clock delay and to get or set a clock delay manually:

stm32mp25-rgmii-gtx-clock-delay
Handle STM32MP25 RGMII GTX clock delay

Usage: stm32mp25-rgmii-gtx-clock-delay [OPTIONS] <COMMAND>

Commands:
  benchmark  Benchmark all possible RGMII GTX clock delays
  set        Set RGMII GTX clock delay
  get        Get RGMII GTX clock delay
  license    Print license & copyright for this software
  help       Print this message or the help of the given subcommand(s)

Options:
  -v, --verbose...  Increase verbosity level (once = debug, twice = trace)
  -h, --help        Print help
  -V, --version     Print version

3.1. Benchmark all possible values[edit | edit source]

To automatically find the best clock delay, use the 'benchmark' subcommand:

stm32mp25-rgmii-gtx-clock-delay help benchmark
Benchmark all possible RGMII GTX clock delays

Usage: stm32mp25-rgmii-gtx-clock-delay benchmark [OPTIONS] --device <DEVICE>

Options:
  -d, --device <DEVICE>
          Device name
  -u, --url <URL>
          Benchmark by fetching data from this URL (recommended size > 100 MiB) [default: https://cdn.kernel.org/pub/linux/kernel/v6.x/linux-6.4.3.tar.xz]
  -s, --speed-low-limit <SPEED_LOW_LIMIT>
          Skip if transfer rate is below SPEED_LOW_LIMIT bytes/second during more than TIMEOUT seconds [default: "100 kiB"]
  -t, --timeout <TIMEOUT>
          Timemout for SPEED_LOW_LIMIT and for the connection phase [default: 5]
  -h, --help
          Print help

The only required option is -d/--device. If the running system does not have access to the internet, specifically https://cdn.kernel.org, then another URL must be specified using the -u/--url option. In that case, it is strongly recommended to point to a payload which is more than 100 MiB. Other options have default values that should be suitable for all cases, and thus, they can be ignored.

Here's a typical example. This can take a couple of minutes, depending on the network speed:

stm32mp25-rgmii-gtx-clock-delay benchmark --device eth1
Using URL https://cdn.kernel.org/pub/linux/kernel/v6.x/linux-6.4.3.tar.xz
Pass 1/2
Benchmarking RGMII GTX clock delay = 0.00 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 0.30 nanoseconds... Done in 8.90s; CRC error rate was 1.43% (1363/95451)
Benchmarking RGMII GTX clock delay = 0.50 nanoseconds... Done in 2.46s; CRC error rate was 1.43% (1362/95164)
Benchmarking RGMII GTX clock delay = 0.75 nanoseconds... Done in 2.46s; CRC error rate was 1.47% (1395/95162)
Benchmarking RGMII GTX clock delay = 1.00 nanoseconds... Done in 2.48s; CRC error rate was 1.53% (1460/95165)
Benchmarking RGMII GTX clock delay = 1.25 nanoseconds... Done in 2.41s; CRC error rate was 1.46% (1393/95162)
Benchmarking RGMII GTX clock delay = 1.50 nanoseconds... [28] Timeout was reached (Operation too slow. Less than 102400 bytes/sec transferred the last 5 seconds)
Benchmarking RGMII GTX clock delay = 1.75 nanoseconds... [28] Timeout was reached (Operation too slow. Less than 102400 bytes/sec transferred the last 5 seconds)
Benchmarking RGMII GTX clock delay = 2.00 nanoseconds... [28] Timeout was reached (Operation too slow. Less than 102400 bytes/sec transferred the last 5 seconds)
Benchmarking RGMII GTX clock delay = 2.25 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.50 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.75 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 3.00 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 3.25 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Pass 2/2
Benchmarking RGMII GTX clock delay = 3.25 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 3.00 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.75 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.50 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.25 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 2.00 nanoseconds... [28] Timeout was reached (Resolving timed out after 5000 milliseconds)
Benchmarking RGMII GTX clock delay = 1.75 nanoseconds... [28] Timeout was reached (Operation too slow. Less than 102400 bytes/sec transferred the last 5 seconds)
Benchmarking RGMII GTX clock delay = 1.50 nanoseconds... Done in 4.24s; CRC error rate was 1.51% (1434/95169)
Benchmarking RGMII GTX clock delay = 1.25 nanoseconds... Done in 2.43s; CRC error rate was 1.36% (1296/95165)
Benchmarking RGMII GTX clock delay = 1.00 nanoseconds... Done in 2.51s; CRC error rate was 1.53% (1458/95162)
Benchmarking RGMII GTX clock delay = 0.75 nanoseconds... Done in 2.46s; CRC error rate was 1.50% (1426/95165)
Benchmarking RGMII GTX clock delay = 0.50 nanoseconds... Done in 2.45s; CRC error rate was 1.52% (1447/95164)
Benchmarking RGMII GTX clock delay = 0.30 nanoseconds... Done in 9.56s; CRC error rate was 1.43% (1365/95169)
Benchmarking RGMII GTX clock delay = 0.00 nanoseconds... [28] Timeout was reached (Operation too slow. Less than 102400 bytes/sec transferred the last 5 seconds)
Best RGMII GTX clock delay is 0.75 ns
To permanently use this RGMII GTX clock delay, add "st,io-delay = <0x3>;" into following device-tree node(s):
        /soc/pinctrl@44240000/eth2-rgmii-0/pins2
        /soc/pinctrl@44240000/eth2-rgmii-test-1/pins2
        /soc/pinctrl@44240000/eth2-rgmii-test-0/pins1

The most important information is delivered at the end of the benchmark. In the previous example, this is this part:

Best RGMII GTX clock delay is 0.75 ns
To permanently use this RGMII GTX clock delay, add "st,io-delay = <0x3>;" into following device-tree node(s):
        /soc/pinctrl@44240000/eth2-rgmii-0/pins2
        /soc/pinctrl@44240000/eth2-rgmii-test-1/pins2
        /soc/pinctrl@44240000/eth2-rgmii-test-0/pins1

It shows the best RGMII GTX clock delay, which is 0.75 nanoseconds in this example, and provides instructions on how to modify the device-tree to use this value permanently.


3.2. Set or get current value[edit | edit source]

This tool can also be used to manually get and set the current RGMII GTX clock delay:

stm32mp25-rgmii-gtx-clock-delay get --device eth1
 device named "eth1" is known as "eth2" in device-tree
 ↳ its RGMII GTX clock is connected to GPIO F7 (pinctrl@44240000)
   ↳ its delay can be accessed at address 0x44290040 (bits 28-32) in /dev/mem
     ↳ its value is 0x5 (1.25 nanoseconds)
stm32mp25-rgmii-gtx-clock-delay set --device eth1 --clock-delay 0.75
 device named "eth1" is known as "eth2" in device-tree
 ↳ its RGMII GTX clock is connected to GPIO F7 (pinctrl@44240000)
   ↳ its delay can be accessed at address 0x44290040 (bits 28-32) in /dev/mem
     ↳ its value is 0x3 (0.75 nanoseconds)

4. Potential issues & solutions[edit | edit source]

4.1. "No reliable RGMII GTX clock delay found"[edit | edit source]

If the tool reports "No reliable RGMII GTX clock delay found", it indicates that the signal may be too degraded to sustain megabytes of download. To avoid this situation, it is possible to specify a smaller payload using the --url option. However, it may be more suitable to redesign the PCB traces causing the issue.

4.2. "Couldn't resolve host name"[edit | edit source]

If the error message "Couldn't resolve host name" appears, it could be due to issues with the network settings. Check thenetwork settings (/etc/resolv.conf, https_proxy env. variable, ...) and make sure that they are configured correctly.

4.3. "SSL certificate problem"[edit | edit source]

If the error message "SSL certificate problem" is encountered, it probably means that some CA certificates are missing on the system. To fix this, copy the missing certificates into the directory "/usr/local/share/ca-certificates/", and then run the command "update-ca-certificates". This should solve this issue.

<noinlcude>

</noinlcude>