Last edited 11 months ago

How to develop an OP-TEE Trusted Application with STM32CubeIDE

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article is a guideline to OP-TEE trusted application support with STM32CubeIDE.

It proposes to create an OP-TEE trusted application project implementing:

  • user space executable hello world which makes a call to OP-TEE trusted application
  • OP-TEE trusted application itself, with universally unique identifier (a.k.a. UUID) support
Important
This article is based onto STM32MP13x lines  but it is also applicable to any STM32 MPU device.

1. Prerequisites[edit | edit source]

Minimum hardware

  • STM32MP1x board booted with OP-TEE
  • Linux console
  • Ethernet (or Ethernet over USB) for connection to Linux® Cortex®-A

Minimum software

Yocto SDK is required to built trusted application example and Linux project is used here only to deploy trusted application on the STM32MP1x target.

2. Create a Trusted Application project[edit | edit source]

In the root project context, named "myMp135fDk" here, right-click and select Create an OP-TEE Trusted Application Project.


Trusted application project creation shortcut

Project name is given, note that the trusted application project uses by default the SDK version associated to the STM32MP1 project.

STM32MP1 project enriched with OP-TEE Trusted Application projects

Trusted Application type project is created under root project. It contains two repositories for sources:

  • "host/", which targets user space executable sources
  • and "ta/" corresponding to trusted application sources
STM32MP1x project enriched with OP-TEE Trusted Application project

3. Build[edit | edit source]

Select your trusted application project, right-click and then Build Project.

Trusted application project build

This build generates two objects:

  • the executable, "myTrustedApp" here under "Binaries/" Eclipse artifact
  • the trusted application, "37cc9755-b605-4b7a-8c9d-257ee26aaa21.ta" under "ta/" repository.

For STM32MP2 series require two lines update inside Makefile generated at project creation to support 64-bits:

ENV?= "TA_DEV_KIT_DIR=$(SDKTARGETSYSROOT)/usr/include/optee/export-user_ta_arm64 LIBGCC_LOCATE_CFLAGS=--sysroot=$(SDKTARGETSYSROOT) TEEC_EXPORT=$(SDKTARGETSYSROOT)/usr"

For STM32MP2 series and STM32MP1 series require update inside Makefile generated at project creation to

$(MAKE) "$(ENV)" -C ta CFLAGS=--sysroot="$(SDKTARGETSYSROOT)" CROSS_COMPILE="$(TA_CROSS_COMPILE)" LDFLAGS=""


Trusted application project build

4. Prepare debug[edit | edit source]

In order to debug user space application, your target must be Linux® booted and network connected.

You can check boot messages via Linux® console opened with butterfly icon, but remember this console cannot be shared outside STM32CubeIDE (minicom,...).

In order to check network connection, start the Target Status widget in the bottom right corner of the window.

Target Status - green


Check also How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.

5. Set up Linux® deployment configuration[edit | edit source]

To run or debug the executable "myTrustedApp", it is required to download the trusted application (.ta) to the STM32MP1 device. Select the Linux project, right-click Run as... > Run Configurations, then select STM32 Cortex-A Linux Deployment'.

Linux deployment


Setup for trusted application are:

  • select as Project the trusted application project, "myTrustedApp" here
  • select as Local path the .ta file inside ta/ of trusted application project
  • select as Remote path "/lib/optee_armtz/"


Trusted application deployment configuration


Then unclick reboot and click OK, you will get the corresponding deployment message in a dedicated console.

Trusted application deployment message

6. Set up Debug Configuration[edit | edit source]

Select your trusted application project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application > New Configuration...'.
Setup C/C++ Application with Search Project... and select the executable. The default connection proposed is "MPU SSH", corresponding to the target IP address discovered by the Target Status widget. The default destination directory is /home/root.

Trusted application debug configuration

7. Debug stepping into myTrustedApp[edit | edit source]

Click Debug :

  1. Executable is downloaded to the target,
  2. GDBServer is launched on the target,
  3. GDBClient is launched on the workstation and can exchange via the network with GDBServer.
Trusted application debug


Stepping into trusted application source code, we reach the call to the trusted application on line 86. The increment is done by OP-TEE trusted application as mentioned in the console.
Note that debug of trusted application itself (.ta) is not supported.


For STM32MP2 series, absolute path to 64-bit SDK (MP2) GDB client is needed:

/local/home/<username>/SDK_6.2.1_mp2/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-gdb
Trusted application debug configuration

Launching debug

Trusted application debug
Information
In case of error; stop any GDBServer running on the target before launching a new debug session.