Last edited 5 months ago

TF-M overview

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Overview of the Trusted Firmware-M project[edit | edit source]

Trusted Firmware-M (TF-M) is an open-source project managed by TrustedFirmware group[1]:

The software environment is design to run in the Secure Processing Environment (SPE) of ARMv8-M microcontrollers following the PSA Certified guidelines[4].

TF-M uses secure partitions that offers services. They can be isolated following different isolation levels:

  • Level 1: SPE and NSPE isolation.
  • Level 2: Level 1 + Application Root of Trust (ARoT) protection from NSPE and PSA Root of Trust (PRoT) protection from NSPE and ARoT.
  • Level 3: Level 2 + Secure partition protection from NSPE and other secure partitions. PSA Root of Trust (RoT) domain protection from NSPE and all Secure Partitions.

The default secure partitions that can be isolated to the nonsecure environment:

  • Initial attestation
  • Crypto services
  • Internal trusted storage
  • Firmware update
  • Protected storage

The secure partitions are accessible using PSA dedicated API[5].

2. License[edit | edit source]

TF-M is delivered under a BSD-3-Clause style license and can run secure partitions without restriction on their licensing model. It also includes different sub-projects with their dedicated license, see documentation for details.

3. Architecture overview[edit | edit source]

Note: The above image has been imported from TF-M documentation

4. Software profile[edit | edit source]

TF-M defines different profiles offered to the user to select the security level targeted. See TF-M profile pagefor more information.

Important
STMicroelectronics implementation uses the medium profile by default.
Only medium and large profile are supported for M33-TD flavor . Indeed, CONFIG_TFM_SPM_BACKEND set to IPC is mandatory for IPCC mailbox used by SCMI and PSA services. And by definition, CONFIG_TFM_SPM_BACKEND set to SFN is mandatory for small profile.

5. Secure boot[edit | edit source]

The secure boot is driven by the platform first stage boot loader.

On STM32MP2 series, depending on the TD flavor (A35-TD or M33-TD) defined on the platform, different flavors are allowed to achieve the secure boot.

5.1. For A35-TD flavor [edit | edit source]

For A35-TD flavor , the secure boot is ensured by default trusted boot bootchain.

To complete the secure boot chain and run TF-M in TrustZone area, it has to be started following the secure coprocessor loading process.

This will ensure that the TF-M and associated nonsecure part (NSPE) is authenticated and follows the secure boot requirements.

5.2. For M33-TD flavor [edit | edit source]

For M33-TD flavor , the ROM code authenticates an FSBL-M, which is MCUboot, as it is the default secure bootloader (BL2) for TF-M. This FSBL-M authenticates (and decrypts) the defined slots to be loaded: one for the the DDR firmware, one for the TF-M image and its associated NSPE.

6. Secure Partitions[edit | edit source]

Secure services (aka Service) is the component providing secure functionalities in SPE, and Client is the user of the Service. A service acts as a client when it is accessing its depending services.

Services are grouped into Secure Partition (aka partition). A partition: Contains services with the same purpose.

The TF-M secure partitions described in the next chapters are generic and provided by default in TF-M by the TrustedFirmware group.

6.1. Crypto[edit | edit source]

Crypto partition offer PSA Crypto API[6] implementation in a dedicated RoT secure partition. The implementation is based on Mbed crypto[7].

For the keys and secrets management on STMicroelectronics products, you can also check the page How to manage keys and secrets in TF-M.

6.2. Firmware update[edit | edit source]

The firmware update partition implements the PSA Firmware update API [8]. It gives all the mandatory features to authenticate, verify and install a new updated image and manage the security about the update process.

6.3. Initial attestation[edit | edit source]

Initial attestation partition implements the PSA Attestation API [9]. It provides a verifiable report of the state of the platform.

6.4. Internal trusted storage[edit | edit source]

Internal Trusted Storage (ITS) implements PSA secure storage API [10]. The internal storage is designed to store the most secure and critical assets used by the RoT.

6.5. Protected storage[edit | edit source]

The protecte storage (PS) partition in the ARoT that implements the PSA secure storage API [10] and allows to store secure data on external storage, see Protected Storage service key management for details.

7. STM32MP2 series secure partitions[edit | edit source]

STMicroelectronics provides STM32MP2 series specific partitions and secure services to nonsecure applications running on Arm®-Cortex®-M33:

For M33-TD flavor , it has been extended to also provide system and secure services to Arm®-Cortex®-A35.

7.1. Coprocessor CPU management[edit | edit source]

This service is used to control other CPUs (Cortex®-A35 or Cortex®-M0+) from Cortex®-M33. This is only available for M33-TD flavor .
The API is described in tfm_ioctl_cpu_api.h .

7.2. Low Power[edit | edit source]

The low power service is provided by the PM partition (TFM_PARTITION_PM in platform/ext/target/stm/common/stm32mp2xx/secure_fw/partitions/pm/ ) and based on the STM32MP2 low power firmware (in platform/ext/target/stm/common/stm32mp2xx/lib/stm32mp2-low-power ).

This is only available for M33-TD flavor (STM32_M33TDCID).

The API is described in tfm_pm_api.h

This generated binary "stm32mp2_lp_fw.bin" is integrated in the PM partition and loaded in RETRAM during its initialization;
the firmware is compiled the STM32 TF-M configuration flags:

  • Select target with: STM32_SOC_NAME
  • Select DDR with STM32_DDR_TYPE, STM32_DDR_FREQ, STM32_DDR_SIZE

see page STM32MP2 power overview for details.

7.3. SCMI[edit | edit source]

The SCMI service is provided by the SCP partition (platform/ext/target/stm/common/stm32mp2xx/secure_fw/partitions/scp/ ) and based on the SCP-firmware[11]. Please check SCMI overview for more details.

This is only available for M33-TD flavor .

The API is described in tfm_scmi_api.h

7.4. Watchdog[edit | edit source]

This service is used to manage secure Cortex®-M33 watchdog.
The API is described in tfm_ioctl_wdt_api.h .

7.5. PSA ADAC[edit | edit source]

The Authenticated Debug Access Control (ADAC)[12] service is only available for STM32MP21x lines  and M33-TD flavor .
The API is described in tfm_adac_api.h

8. To go further[edit | edit source]

Please refer to the TF-M documentation :

And the WIKI pages:

9. References[edit | edit source]