1. Article purpose[edit | edit source]
This section details the TF-M stage (Trusted Firmware-M). It explains how to configure and build TF-M in the STM32 MPU context, describes the build process from sources, and shows how to deploy it on the target device.
2. Build with a bare environment or STM32CubeIDE[edit | edit source]
2.1. Prerequisites[edit | edit source]
2.1.1. Linux® PC[edit | edit source]
2.1.1.1. Installing the build environment[edit | edit source]
Install the dependencies:
sudo apt-get install -y git curl wget build-essential libssl-dev python3 \
python3-pip cmake make
Then add the CMake path to the environment:
export PATH=<CMake path>/bin:$PATH
2.1.1.2. Installing a toolchain[edit | edit source]
If using STM32CubeIDE to build TF-M, installing a toolchain is not necessary, since STM32CubeIDE comes with a built-in toolchain.
If using a command-line interface, download the toolchain and add the GNU Arm toolchain path to the environment:
export PATH=$PATH:<toolchain installation directory>/sysroots/x86_64-ostl_sdk-linux/usr/share/gcc-arm-none-eabi/bin
2.1.2. Windows® PC[edit | edit source]
2.1.2.1. Installing the build environment[edit | edit source]
Install the dependencies:
- Git client (latest version: https://git-scm.com/download/win)
- CMake (native Windows® version: https://cmake.org/download/)
- GNU make (http://gnuwin32.sourceforge.net/packages/make.htm)
- Python 3 (native Windows® version: https://www.python.org/downloads/) and the pip package manager (included in Python version 3.4 and higher)
Then add the CMake path to the environment:
set PATH=<CMake_Path>/bin;%PATH%
2.1.2.2. Installing a toolchain[edit | edit source]
If using STM32CubeIDE to build TF-M, installing a toolchain is not necessary, since STM32CubeIDE comes with a built-in toolchain.
If using a command-line interface, use the toolchain from STM32CubeIDE and update the path in .bashrc as follows:
PATH="/c/ST/<STM32 CubeIDE path>/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.2.202309201523/tools/bin":$PATH
| The plugin version may differ from one STM32CubeIDE version to another, so modify it accordingly. |
2.2. Installing sources[edit | edit source]
2.2.1. Downloading source[edit | edit source]
For the full-featured software, go to the STMicroelectronics github:
git clone https://github.com/STMicroelectronics/trusted-firmware-m.git
For the record, the official Trusted Firmware-M git repository (without STM32MP2 support) can be downloaded there:
git clone https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git/
2.3. Installing Python dependencies[edit | edit source]
From the TF-M source code installed on the PC:
pip3 install --upgrade pip \
pip3 install -r tools/requirements.txt
2.4. Build process[edit | edit source]
2.4.1. STM32CubeIDE[edit | edit source]
There is one Cortex®-M33 nonsecure STM32Cube firmware example that uses TF-M services and builds TF-M using STM32CubeIDE.
Refer to the How to build and debug secure project on Cortex-M33 coprocessor in STM32CubeIDE wiki page for a step-by-step build-and-load example with TF-M.
2.4.2. Build command lines[edit | edit source]
You can also use TF-M-tests for the tests and non-secure software example. Starting from ecosystem release v6.1.0 , TF-M is based on official release v2.1, for which build system has changed. You will need to fetch TF-M-tests:
git clone https://github.com/STMicroelectronics/tf-m-tests.git ${TF-M-TESTS_DIRECTORY}
See the Github pages for compilation steps and the different possible build options for STM32MP257-EV1 or STM32MP215F-DK
2.4.3. External device tree for the STM32MP2 series[edit | edit source]
STMicroelectronics provides device tree configurations for others boards in a dedicated git repository: stm32mp2/a35-td/tfm/ .
The repository can be used to store custom configurations. Use the following command to build with this external dt repository:
git clone https://github.com/STMicroelectronics/dt-stm32mp.git ${DT_PATH}
Depending on your configuration, you will need to add build options for the external DT files.
For A35-TD flavor
and M33-TD flavor
, more information is also given on Github pages for STM32MP257-EV1 or STM32MP215F-DK
2.4.3.1. Example for A35-TD flavor
[edit | edit source]
DT_PATH can be set to any path, but it must not be a relative path.
-DDTS_EXT_DIR=${DT_PATH}/stm32mp2/a35-td \ -DDTS_BOARD_S=tfm/stm32mp257f-ev1-ca35tdcid-ostl-s.dts
And optionally, the nonsecure DT
-DDTS_BOARD_NS=tfm/stm32mp257f-ev1-ca35tdcid-ostl-ns.dts
2.4.3.2. Example for M33-TD flavor
[edit | edit source]
DT_PATH can be set to any path, but it must not be a relative path.
-DDTS_EXT_DIR=${DT_PATH}/stm32mp2/m33-td \ -DDTS_BOARD_S=tfm/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-s.dts \ -DDTS_BOARD_BL2=mcuboot/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-bl2.dts
And optionally, the nonsecure DT
-DDTS_BOARD_NS=tfm/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-ns.dts
2.5. Extra compilation flags[edit | edit source]
2.5.1. Flags to debug TF-M faults[edit | edit source]
TF-M can print secure-partition and Secure Partition Manager (SPM) diagnostics when investigating a fault in an application using TF-M services. Add the following options to the TF-M secure-image CMake configuration command described above:
-DTFM_PARTITION_LOG_LEVEL=TFM_PARTITION_LOG_LEVEL_DEBUG \ -DTFM_SPM_LOG_LEVEL=TFM_SPM_LOG_LEVEL_DEBUG \ -DTFM_EXCEPTION_INFO_DUMP=ON \ -DTFM_LOG_FATAL_ERRORS=ON \ -DTFM_LOG_NONFATAL_ERRORS=ON \ -DTFM_LOG_ERR_FILE_AND_LINE=ON \ -DCONFIG_TFM_BACKTRACE_ON_CORE_PANIC=ON
TFM_PARTITION_LOG_LEVEL=TFM_PARTITION_LOG_LEVEL_DEBUG: Prints debug messages from secure partitions.TFM_SPM_LOG_LEVEL=TFM_SPM_LOG_LEVEL_DEBUG: Prints debug messages from the SPM.TFM_EXCEPTION_INFO_DUMP=ON: Captures exception context and prints it when the configured SPM logging level permits.TFM_LOG_FATAL_ERRORS=ON: Logs fatal errors when they occur.TFM_LOG_NONFATAL_ERRORS=ON: Logs nonfatal errors when they occur.TFM_LOG_ERR_FILE_AND_LINE=ON: Adds source filenames and line numbers to fatal and nonfatal error logs.CONFIG_TFM_BACKTRACE_ON_CORE_PANIC=ON: Prints a backtrace on a secure core panic, then halts.
The STM32MP2 platform configuration already enables exception information dumps and core-panic backtraces. Reconfigure and rebuild the secure image, deploy it using the same procedure as for the original build, and inspect the TF-M console output when reproducing the fault. Check the effective values in <BUILD_DIRECTORY>/build_spe/CMakeCache.txt if the expected logs do not appear.
2.5.2. SoC revision flags[edit | edit source]
TF-M supports 2 SoC revisions for STM32MP23x lines
and STM32MP25x lines
, Rev Y and Rev X. There are flags in TF-M to choose the revision: STM32_STM32MP23_SOC_REV for STM32MP23x lines
and STM32_STM32MP23_SOC_REV for STM32MP25x lines
. They are set by default to revY. If your SoC is a revision X, you can update the flag in the TF-M compilation command line, depending on the SoC:
-DSTM32_STM32MP23_SOC_REV=revX
or
-DSTM32_STM32MP25_SOC_REV=revX
This allows skipping the workarounds done for SoC revision Y.
3. Build with Developer package[edit | edit source]
For the A35-TD flavor
, only CubeIDE is supported to build TF-M
For the M33-TD flavor
, TF-M is managed by Developper package. please refer to the following article to understand how to install & develop: STM32MPU Developer Package
4. Build with Distribution package[edit | edit source]
The Linux Yocto-based distribution package (STM32MPU distribution package) integrates the TF-M components source code in a dedicated recipe in the OpenSTLinux distribution.
To generate the three required binaries for M33TD flavor — **MCUBoot**, **DDR firmware** and **M33 firmware** — use the command:
bitbake m33fw-stm32mp2
If you need to build them individually, use the following commands:
bitbake tf-m-stm32mp bitbake m33tdprojects-starter-stm32mp2 bitbake m33fw-stm32mp2