Last edited 4 months ago

How to create Signed FIT image from Distribution package

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


1. Article purpose[edit | edit source]

The purpose of this article is to explain how to create a signed FIT image containing a kernel image and devicetree.

Warning
With the current implementation on Yocto/Openembedded, the creation of a signed FIT image requires that you declare only one devicetree on the machine

2. Creating a signature key[edit | edit source]

By default Yocto/Openembeded can create and store a key for signing a FIT image but anyone has also the possibility to create one manually and indicate Yocto/Openembeded where to find it.


To create your own key, follow the commands below to generate a new signing key manually.

  • To generate a new signing key manually:

Create a directory to receive the signing key (uboot-sign-directory for this example)

mkdir uboot-sign-directory/

Generate an RSA private key for signing the fitImage:

 openssl genrsa -F4 \
       -out  uboot-sign-directory/my-uboot-sign-key.key \
       2048

Generate a certificate for signing the fitImage:

 openssl req -batch -new -x509 \
     -key uboot-sign-directory/my-uboot-sign-key.key \
     -out uboot-sign-directory/my-uboot-sign-key.crt

Generate an RSA private key for signing the image in fitImage:

 openssl genrsa -F4 \
       -out  uboot-sign-directory/my-uboot-image-sign-key.key \
       2048

Generate a certificate for signing the image in fitImage:

 openssl req -batch -new -x509 \
     -key uboot-sign-directory/my-uboot-image-sign-key.key \
     -out uboot-sign-directory/my-uboot-image-sign-key.crt

3. Machine configuration on the Distribution Package[edit | edit source]

In the Yocto/Openembedded machine definition (conf/machine/<machine_name>.conf) you must specify several parameters:

  • force use of a FIT image
  • request to sign the FIT image
  • specify the path of the signing key

3.1. Use the FIT image[edit | edit source]

# to use the FIT image for kernel and devicetree
 MACHINE_FEATURES += "fit"
# put the name of default devicetree to use by default:
 FIT_CONF_DEFAULT_DTB = "<name of default devicetree>"

3.2. Use the Signing FIT[edit | edit source]

UBOOT_SIGN_ENABLE = "1"
FIT_SIGN_INDIVIDUAL = "1"

3.3. Signing key[edit | edit source]

if your keys are localized in a specific directory, for example $HOME/uboot-sign-directory (put an absolute path)

 UBOOT_SIGN_KEYDIR = "$HOME/uboot-sign-directory"

or if you use a generic path (default path provided by Yocto/Openembedded)

 UBOOT_SIGN_KEYDIR = "${DEPLOY_DIR_IMAGE}"

For the signing key, you MUST specify the name of the keys (without the extension), my-uboot-sign-key for example

UBOOT_SIGN_KEYNAME = "my-uboot-sign-key"
UBOOT_SIGN_IMG_KEYNAME = "my-uboot-image-sign-key"

For the Distribution Package to generate the signing key, you must add the following key in addition to UBOOT_SIGN_ENABLE

FIT_SIGN_INDIVIDUAL = "1"
FIT_GENERATE_KEYS = "1"
UBOOT_DTB_BINARY = ""
UBOOT_DTB_SIGNED = ""
Warning
FIT_GENERATE_KEYS = "1" will generate a new key only if it does not exist
Information
UBOOT_DTB_BINARY and UBOOT_DTB_SIGNED are set to empty to not use the default signature process on class which support badly multiple configuration/dt.

3.4. Summary: Machine contents[edit | edit source]

# to use FIT image for kernel and devicetree
MACHINE_FEATURES += "fit"
#signing key
UBOOT_SIGN_KEYDIR = "${DEPLOY_DIR_IMAGE}"
UBOOT_SIGN_KEYNAME = "my-uboot-sign-key"
UBOOT_SIGN_IMG_KEYNAME = "my-uboot-image-sign-key"
# Sign FIT image
UBOOT_SIGN_ENABLE = "1"
FIT_SIGN_INDIVIDUAL = "1"
UBOOT_DTB_SIGNED = ""
UBOOT_DTB_BINARY = ""
# generate new signing key if not exist
FIT_GENERATE_KEYS = "1"
# Uboot mkimage option
UBOOT_MKIMAGE_DTCOPTS = "-I dts -O dtb -p 2000"

4. References[edit | edit source]