Last edited 9 months ago

STM32MP215x-DKx - hardware description

Applicable for STM32MP21x lines

This article provides an overview of STM32MP215x-DK Discovery kits.

1. Article purpose[edit | edit source]

This article briefly describes:

  • How to assemble the different elements provided in the commercial box and additional optional accessories
  • What are the different components on the boards
  • How to connect the boards to external material
  • How to configure the board for boot
  • What are the configurations of the connector pins

This article is valid for the STM32MP215F-DK Discovery kit: the part numbers are specified in the STM32MP21 microprocessor part numbers article.

Information
This article is an introduction to the STM32MP215x-DK Discovery kit. For more detailed information, refer to the STM32MP215x-DK Discovery kit user manuals.

2. Board assembly and connections[edit | edit source]

The STM32MP215x-DKx Discovery kit package (STM32MP215F-DK ) contains only the MB2059 motherboard.

STM32MP215F-DK Discovery kit front side (picture not contractual)
Information
Display and camera are available for purchase to complete this basic setup.

The complete set contains:

STM32MP215F-DK and additional accessories kits shown here (picture is not contractual)
Position Description
1 MB2059 main board
2 MicroSD card
3 4.3" TFT 480*272 pixels with LED Backlight and capacitive touch panel RK043FN78H-CT661C (optional)
4 Camera board FFC (provided with the B-CAMS-IMX package) (optional)
5 MB1854 camera board provided with the B-CAMS-IMX package (optional)


STM32MP215F-DK Discovery kit assembly (picture is not contractual)


2.1. Connecting the display to the board (optional)[edit | edit source]

  • Find the DISPLAY connector (CN8) on the top side of the MB2059 main board
  • Flip the connector’s latch up
Display board assembly - step 1 (picture is not contractual)
Display board assembly - step 2 (picture is not contractual)


  • Insert the LCD’s cable with the exposed contacts facing down
Display board assembly - step 3 (picture is not contractual)


  • Flip the connector’s latch down to secure the cable
Display board assembly - step 4 (picture is not contractual)


2.2. Connecting the MB1854 camera board to the board (optional)[edit | edit source]

Camera board assembly (picture is not contractual)


  • Find the camera ports on the STM32MP215x-DK Discovery kit (CN4) (#1 in the image above) and MB1854 (CN1) (#2 in the image above). The camera box contains one FFC.
  • For each port:
    • Pull the plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)


2.3. Connecting USB to TTL serial cables[edit | edit source]

To have 2 consoles on your workstation , one for Cortex-M33 and one for Cortex-A35, 2 "USB to TTL serial cables" are needed.

(picture is not contractual)



2.4. STM32MP215x-DK Discovery kit assembled and connected[edit | edit source]

The picture below presents the recommended board connections for getting started with the STM32MP215x-DKx Discovery kits

Warning
To start the board, it is recommended to go through the corresponding Starter Package article first.

As shown in the board overview, other connectors are available for this board (for example, the GPIO expansion connector).


MB2059 motherboard: STM32MP215F 14x14MicroSD<sup>™</sup> card slotReset buttonEthernet (network)USB Power Delivery Type-C (Power) and USB3.0 DRD/OTG Type-C (programmable through STM32CubeProgrammer)CSI cameraLTDC displayUSB to TTL serial cables
STM32MP215x-DKx Discovery kit connections (picture is not contractual)





3. 3D printed display holder - optional[edit | edit source]

3D printer files (.stl) are available on github[1] to allow you making the above assembly. The OpenSCAD[2] source file (.scad) is also provided to help you doing your own customized holder or casing. For best result with Ultimaker printer, we recommend using "tree" supports[3].

4. Board overview[edit | edit source]

Main board MB2059, revision B: part of the STM32MP215F-DK Discovery kit .

STM32MP215x-DK Discovery kit front side STM32MP215F-DK shown here (picture is not contractual)


Warning
USART2-RX and USART2-TX are wired to ST-Link connector (CN5) and VCPA35 connector (CN2). ST-LINK and Cortex-A35 Linux console can not used simultaneously via those both connectors.
  • To allow the Cortex-A35 Linux console : The VCPA35 connector (CN2) needs to be plugged and ST-Link connector (CN5) to be unplugged
  • To allow debugging over ST-LINK and Cortex-A35 Linux console : CN5 needs to be plugged and CN2 to be unplugged. In such case, the Cortex-A35 Linux console is available through ST-LINK.

Details about the LEDs:

  • The LD1 LED turns yellow when the power cable is inserted into the CN10 connector.
  • The red LED (LD5) is used as a BOOTFAIL indicator and to indicate developer boot mode.
  • Two general-purpose color LEDs (LD2 and LD3) are available as light indicators:
    • The blue LED (LD2) is used as the Linux® Heartbeat LED, which is blinking as long as Linux® is alive on the Cortex®-A.
    • The orange LED (LD3) is used as a STM32Cube example verdict LED.
  • The green indicator LED (LD4) is connected to the STM32MP215 MPU.


5. Boot switches[edit | edit source]

The STM32MP215x-DK Discovery kit can boot on SD card or USB based on ROM code boot device selection.

Warning
Pay attention to the boot pins order: Boot[3:0] in ROM code boot device selection article mentionned above, but Boot[0:3] in the table below, to be in line with the pictures.
Boot mode Boot 0 Boot 1 Boot 2 Boot 3 The boot-related switches (SW1 and SW2
in the board overview picture)
Storage device used for the Cortex-A35 boot Storage device used for the Cortex-M33 boot
Forced USB boot for flash memory programming 0 0 0 0
USB/UART boot
for flash programming
NA
Boot from microSD card
for A35-TD flavor
1 0 0 0
SD card NA
Boot from microSD card
for M33-TD flavor
1 1 1 0
SD card SD card
Developer mode 1 1 0 0
NA NA

When the switch is set to the "ON" position, the BOOTx value is "1"; otherwise it is "0".

6. GPIO mapping[edit | edit source]

6.1. GPIO expansion connector[edit | edit source]

The table below describes the pins of the GPIO expansion connector (CN12 in the board overview picture):

Function STM32 pin Pin Pin STM32 pin Function
3V3 - 1 2 - 5V
GPIO2 / I3C1.SDA PA2 3 4 - 5V
GPIO3 / I3C1.SCL PG13 5 6 - GND
GPIO4 / MCO1 PF11 7 8 PF13 GPIO14 / USART6.TX
GND - 9 10 PH9 GPIO15 / USART6.RX
GPIO17 / USART6.RTS PC3 11 12 PA9 GPIO18 / SAI2.SCKB
GPIO27/ SDMMC3.D3 PD14 13 14 - GND
GPIO22 / SDMMC3.CK PB13 15 16 PH8 GPIO23 / SDMMC3.CMD
3V3 - 17 18 PB14 GPIO24/SDMMC3.D0
GPIO10 / SPI1.MOSI PI5 19 20 - GND
GPIO9 / SPI1.MISO PD1 21 22 PD13 GPIO25/SDMMC3.D1
GPIO11 / SPI1.SCK PD11 23 24 PD2 GPIO8 / SPI1.NSS
GND - 25 26 PC7 GPIO7
I3C2.SDA   PG0 27 28 PC12 I3C2.SCL
GPIO5 / TIM11.CH1 PH13 29 30 - GND
GPIO6 / TIM13.CH1 PC9 31 32 PC8 GPIO12 / TIM8.CH2
GPIO13 / TIM8.CH4 PC10 33 34 - GND
GPIO19 / SAI2.FSB PA6 35 36 PF15 GPIO16 / USART6.CTS
GPIO26 / SDMMC3.D2 PB12 37 38 PA5 GPIO20 / SAI2.SDB
GND - 39 40 PG1 GPIO21 / SAI2.SDA

6.2. User buttons and LEDs[edit | edit source]

The tables below describe the GPIO assignments for the user buttons and LEDs. Refer to the LEDs and buttons on STM32 MPU boards article and #Board overview chapter for more details.

GPIO for LEDs

LED color and label GPIO
Green LD4 PF10
Red LD5 PH4
Orange LD3 PH12
Blue LD2 PZ3

GPIO for user buttons

Button GPIO
USER1 PC4
USER2 PF7