Last edited 9 months ago

Software distributions for STM32MP23 microprocessor

Applicable for STM32MP23x lines

Important
To help you get started with the evaluation of the STM32MP23x product lines, you can rely on the STM32MP257F-DK Discovery kit, and the applicable STM32 MPU embedded software, running with the STM32MP23 software configuration (peripherals, features, and performance).

The embedded software distributions[1] supported for the STM32MP235 line  are listed below.

For each distribution, up to three software packages are delivered:

  • Starter Package (software image)
  • Developer Package (SDK for cross-development, source code for the BSP of the distribution)
  • Distribution Package (build framework on Linux host PC, source code for the whole distribution)
  1. ↑ The STM32 MPU ecosystem release note details the latest delivered embedded software distributions
  2. ↑ The Which STM32MPU Embedded Software Package better suits your needs article provides hints for selecting the most appropriate Package.



Yocto-based OpenSTLinux embedded software[2]

Rely on the

Yocto-based OpenSTLinux Starter Package for STM32MP25 Discovery kits with characteristics relative to the STM32MP235 line 


Yocto-based OpenSTLinux Developer Package for STM32 MPUs

Yocto-based OpenSTLinux Distribution Package for STM32 MPUs
OpenSTLinux expansion packages can be applied on the top of the OpenSTLinux distribution to enable the use of additional components for a specific feature (such as AI-based computer vision).
Buildroot-based Linux embedded software
Important
Buildroot-based Linux distribution is validated against the ecosystem release v6.2.0 (see release note). It will not be ported on ecosystem release v6.2.1 .

Buildroot-based Linux Starter Package for STM32MP25 Discovery kits with characteristics relative to the STM32MP235 line 

Buildroot-based Linux Developer Package for STM32 MPUs

Buildroot-based Linux Distribution Package for STM32 MPUs
OpenWrt-based Linux embedded software
Important
OpenWrt-based Linux distribution is validated against the ecosystem release v6.1.0 (see release note). It has not been ported yet on ecosystem release v6.2.1 .


OpenWrt-based Linux Starter Package for STM32MP25 Discovery kits with characteristics relative to the STM32MP235 line 

OpenWrt-based Linux Distribution Package for STM32 MPUs