This article describes the content of the last release of the OpenWrt-based Linux ecosystem based on Yocto-based OpenSTLinux BSP v6.1.0.
1. Ecosystem content[edit | edit source]
The OpenWrt-based Linux ecosystem releases aim at:
- providing a full ecosystem for the STM32MP1 series and STM32MP2 series
- working efficiently with STM32 MPU boards
, using OpenWrt-based Linux embedded software provided by STMicroelectronics' partner.
This ecosystem release consists of:
- Development tools:
- STM32DDRFW-UTIL,
- STM32PRGFW-UTIL,
- STM32MPUSSP-UTIL.
- STM32 referenced tools
- STM32CubeIDE
- STM32CubeMX
- Programming tools
- STM32CubeProgrammer
- Keygen tool
- Signing tool
- Trusted package creator tool
- STM32PRG-TOOLBOX
- STM32PRG-TOOLBOX-DFU
- STM32PRG-TOOLBOX-FB
- STM32CubeProgrammer
2. Scope of OpenWrt version based on OpenSTLinux BSP v6.1.0[edit | edit source]
This OpenWrt-based Linux ecosystem release is dedicated to the STM32MP1 series and STM32MP2 series.
The purpose on this release is :
- to update this ecosystem with the Yocto-based OpenSTLinux BSP v6.1.0.
- to update this ecosystem with OpenWrt 24.10.6.
2.1. Main changes[edit | edit source]
Visit the OpenWrt release notes to discover main updates coming with this release.
2.2. Main restrictions[edit | edit source]
Visit the OpenWrt release notes to discover main restrictions coming with this release.
3. Intended audience[edit | edit source]
The targeted audience is STM32 MPU customers and partners.
4. Licensing[edit | edit source]
All licenses corresponding to this OpenWrt-based Linux ecosystem are available here
5. Supported development boards[edit | edit source]
Supported ST boards are listed here
6. Embedded software[edit | edit source]
6.1. OpenWrt-based_Linux_embedded_software[edit | edit source]
The OpenWrt-based Linux® embedded software is part of the STM32 MPU embedded software offer.
It is a set of software (see architecture overview), system build and development tools created to ease the development to be done on top of STM32 MPU devices.
It is made up of:
- an open-source Linux® distribution, based on the OpenWrt framework, running on the Arm® Cortex®-A processor(s),
- firmwares, running on the Arm® Cortex®-M processor: FwST-M Packages (not supported for STM32MP13x lines
)
OpenWrt[1] is a Linux operating system targeting embedded devices. OpenWrt provides a fully writable filesystem with package management. OpenWrt is the framework to build an application without having to build a complete firmware around it; for users this means the ability for full customization, to use the device in ways never envisioned.
The Linux® distribution relies on the OpenSTLinux board support package (U-Boot, TF-A, OP-TEE, Linux kernel) complemented with a user-space with a features set.
The partner's repository[2] is "OpenWrt feed"[3] dedicated to supporting the STMicroelectronics STM32MPU platforms.
Several examples of OpenWrt configurations[4] are provided:
- the minimal configuration relies on the OpenSTLinux BSP[5]: TF-A, U-Boot, OP-TEE, Linux
- "demo" configurations include additional packages like a web interface to configure the device
This feed also shows how use the OpenWrt image Builder and how to run benchmarks[6].

6.1.1. OpenWrt-based Linux Distribution for Arm® Cortex®-A[edit | edit source]
Updated 6.x.y should not be used in wiki V7 is the version delivered with the OpenWrt-based Linux ecosystem-v6.1.0.
The release note and readme files give information and details about the features / content / restrictions of the OpenWrt-based Linux Distribution.
| Firmware | Release note | Version |
| OpenWrt Linux Distribution | Readme file and Release notes file | 6.x.y should not be used in wiki V7 |
6.1.2. FwST-M packages for Arm® Cortex®-M[edit | edit source]
The release notes give information and details about the features / content / restrictions of the Packages.
| Firmware | Release note | Version |
| STM32CubeMP2 Package | STM32CubeMP2 Package release note - v1.3.0 | STM32CubeMP2 Package v1.2.0 |
| STM32CubeMP15 Package | STM32CubeMP15 Package release note - v1.7.0 | STM32CubeMP1 Package v1.7.0 |
7. Development tools[edit | edit source]
The tools version has to match the version of the ST BSP components, aka Yocto-based OpenSTLinux BSP v6.1.0, available in Yocto-based OpenSTLinux ecosystem v6.1.0 release note.
8. Documentation[edit | edit source]
To discover the detailed explanation on this release content and to learn how to use it, refer to the "doc" folder of the release
You can also find visit this page Category:STM32 MPU technical literature ; and selecting the relevant STM32 MPU documentation set, you will have access to all information related to the full ecosystem.
9. How to download the software and start with this release[edit | edit source]
Refer to OpenWrt-based Linux embedded software article.
10. Archives
[edit | edit source]
All the release notes for the OpenWrt-based Linux ecosystem are available here . The previous releases are based on older versions of Yocto-based OpenSTLinux BSP and/or OpenWrt. Older versions can be directly found in github.
| OpenWrt-based Linux ecosystem | Major software components | Release note |
|---|---|---|
| openstlinux-6.6-openwrt-24.10.5-mpu-v25.06.11 (Feb 2026) for STM32MP1 series and STM32MP2 series | OSTL BSP v6.1.0 OpenWrt v24.10.5. |
Release note |
| openstlinux-6.6-openwrt-24.10.4-mpu-v25.06.11 (Dec 2025) for STM32MP1 series and STM32MP2 series | OSTL BSP v6.1.0 OpenWrt v24.10.4. |
Release note |
| openstlinux-6.6-openwrt-24.10.2-mpu-v25.06.11 (Nov 2025) for STM32MP1 series and STM32MP2 series | OSTL BSP v6.1.0 OpenWrt v24.10.2. |
Readme file |
| openstlinux-6.6-openwrt-24.10.1-mpu-v24.11.06 (June 2025) for STM32MP1 series and STM32MP25 lines | OSTL BSP v6.0.0 OpenWrt v24.10.1. |
Readme file |
11. References[edit | edit source]
[[Category:OpenWrt-based_OpenSTLinux_ecosystem_release_notes]]