Last edited 4 months ago

STM32MP25 Evaluation boards - OpenSTDroid Starter Package

Applicable for STM32MP25x lines

This article shows how to start up a STM32MP257x-EV1 Evaluation boards (high-end development platforms for the STM32MP25 microprocessor devices) with the software image for the Android-based OpenSTDroid embedded software. It is valid for the STM32MP257F-EV1 Evaluation boards: the part numbers are specified in the STM32MP25 microprocessor part numbers article.

It lists the required material, points to the board features description, and gives the step-by-step process to set up the system.

Finally, it proposes to run some basic use cases and to discover some of the board capabilities.

1. Starter Package content[edit | edit source]

This Starter Package provides:

  • the OpenSTDroid distribution binaries
  • the partition layout required to flash the device with STM32CubeProgrammer

2. Checking the material[edit | edit source]

Mandatory

PC Linux or Windows operating systems. See PC prerequisites for more details on the required configurations
STM32MP257x-EV1 evaluation board High-end development platform for the STM32MP25 microprocessor device including:
microSDTM card It is populated with OpenSTLinux distribution (Linux software), and provides extra storage capacity. An 8-Gbyte minimum microSD card is needed
USB type-C cable It connects the STM32MP257x-EV1 evaluation board to the PC through the USB type-C (ST-LINK/V3) connector
USB type-C cable It connects the STM32MP257x-EV1 evaluation board to a USB OTG device through the USB micro-AB connector


Optional

LCD screen Several types of screen are possible : LVDS, DSI, or HDMI
Power supply (Optional) Power supply block (5 V, 3A) for the MB1936 board.
USB keyboard and mouse Thanks to the USB type A connectors, the STM32MP257x-EV1 Evaluation board can be equipped with a full-size keyboard and mouse
Ethernet cable It can connect the STM32MP257x-EV1 evaluation board to a network through the RJ45 connector
RS232 cable It can connect the STM32MP257x-EV1 evaluation board to the PC through the UART connector as an alternative of the ST-LINK/V2-1 connection
CAN cable It can connect the STM32MP257x-EV1 evaluation board to CAN devices through the CAN FD/TT connectors
Trace cable It can connect the STM32MP257x-EV1 evaluation board to an external tool through the Trace connector
JTAG cable It can connect the STM32MP257x-EV1 evaluation board to an external tool through the JTAG connector

Optionally, devices and extension boards might be plugged to the STM32MP257x-EV1 evaluation board thanks to connectors such as:

  • the GPIO expansion connector
  • the PCIe connector
  • the Mikro bus connector
  • ...


The following figure shows the material not included in STM32MP25 Evaluation board package which is used in this Starter Package.

Recommended material for this Starter Package

3. Assembling the board[edit | edit source]

The STM32MP257x-EV1 Evaluation board packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include the items listed below.

STM32MP257F-EV1 shown here (picture is not contractual)
Position Description
1 MB1936 main board
2 B-LVDS7-WSVGA 7” LVDS WSVGA display module with touch panel (optional)
3 LVDS display cable, provided with the B-LVDS7-WSVGA package (optional)
4 B-CAMS-IMX MB1854 MIPI CSI-2 camera board (optional)
5 Camera board FFC, provided with the B-CAMS-IMX package (optional)


B-LVDS7-WSVGA display and B-CAMS-IMX camera are available for purchase to complete the setup.

The complete set looks like this:

STM32MP257x-EV1 Evaluation board assembly
STM32MP257F-EV1 shown here (picture is not contractual)

3.1. Connecting the LVDS display to the board[edit | edit source]

Display board assembly (picture is not contractual)
  • Check the cable orientation shown above using the black mark and the white twisted pairs.
  • Find the LVDS ports on the STM32MP257x-EV1 Evaluation board (CN2) and the display (CN1). The LVDS display box contains one cable.
  • Insert the cable into each port as shown below:
Display board assembly (picture is not contractual)

3.2. Connecting the MB1854 camera board to the board[edit | edit source]

Camera board assembly (picture is not contractual)
  • Find the camera ports on the STM32MP257x-EV1 Evaluation board (CN4) and MB1854 (CN1). One FFC is provided in the camera box.
  • For each port:
    • Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the black plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)

3.3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]


STM32MP257x-EV1 Evaluation board assembled
STM32MP257F-EV1 shown here (picture is not contractual)


4. Installing the tools[edit | edit source]

4.1. Installing the STM32CubeProgrammer tool[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.23.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.23.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .


4.2. Preparing the USB serial link for flashing[edit | edit source]

It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.

Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.

  • For Linux host PC or Windows host PC with VMWare:

The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:

sudo apt-get install libusb-1.0-0

To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:

cd <your STM32CubeProgrammer install directory>/Drivers/rules 
sudo cp *.* /etc/udev/rules.d/
  • For Windows host PC:

Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.

In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.

To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.

5. Downloading the image and flashing it on the board[edit | edit source]

5.1. Image download[edit | edit source]

Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
STM32MPU distribution for Android™
Tag Flash device Link Release note
st-android-16.0.0-2026-05-26 eMMC Go on st.com to download the STM32MP2 OpenSTDroid Starter Package for STM32MP25 (select the adapted board) st-android-16.0.0-2026-05-26 release note (v6.2.0)
st-android-16.0.0-2026-09-08 Go on st.com to download the STM32MP2 OpenSTDroid Starter Package for STM32MP25 (select the adapted board) st-android-16.0.0-2026-09-08 release note (v6.2.1)
Installation
  • Go to the host PC directory where to install the Starter Package (<Starter Package installation directory>); for example:
cd <working directory path>/Android-Starter-Package
  • Download the tarball file (*.tar.gz)) in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the flash layout files:
tar xvf st-android-<version>-<date>-stm32mp257f-<board>-<flash device>-starter.tar.gz


5.2. Flashing the eMMC images[edit | edit source]

The STM32CubeProgrammer tool is used to flash the STM32MP25 Evaluation board with the downloaded image.

Several flash devices (microSD, eMMC...) are available on this board: see the STM32 MPU Flash mapping for Android article to know more about the supported Flash memory technologies, and the flash partitions. The steps below consider the eMMC as the flash device.

Let's flash the downloaded image on the eMMC card:

  • Set the boot switches to the off position (boot from UART/USB).
Boot from UART/USB
  • Connect the USB type-C (OTG) port (4) to the host PC that contains the downloaded image.
  • Connect the USB type-C (power supply) port (1) to the power connector or a host PC, and check the power jumper position.
  • Press the reset button (7) to reset the board.
Evaluation board connections for flashing
STM32MP257A-EV1 shown here (picture is not contractual)
  • Go to the Starter Package directory that contains the binaries and the flash layout files.
cd <Starter Package installation directory>/st-android-<version>-<date>-stm32mp257f-ev1-<flash device>-starter
Information
The commands below are for a Linux® host PC; however, they are similar for a Windows host PC except that STM32_Programmer_CLI is replaced by STM32_Programmer_CLI.exe.
  • Check that the STM32CubeProgrammer tool is installed and accessible; if not, go to the installation procedure (installing the tools).
STM32_Programmer_CLI --h
      -------------------------------------------------------------------
                        STM32CubeProgrammer <tool version>                  
      -------------------------------------------------------------------
  • Get the device port location for the USB link.
STM32_Programmer_CLI -l usb
       -------------------------------------------------------------------
                         STM32CubeProgrammer <tool version>                  
       -------------------------------------------------------------------

=====  DFU Interface   =====

Total number of available STM32 device in DFU mode: 1

  Device Index           : USB1
  USB Bus Number         : 003
  USB Address Number     : 005
  Product ID             : DFU in HS Mode @Device ID /0x505, @Revision ID /0x2000
  Serial number          : 001900364136500100373653
  Firmware version       : 0x0110
  Device ID              : 0x0505
  • Fuse the eMMC RPMB with the RPMB test key
Important
Please read carefully

The starter is using RPMB as secure storage. For that purpose, the RPMB key must be fused on the eMMC.

This procedure must be followed only if the RPMB key has not already been fused on your STM32MP25 Evaluation Board.

By default, the RPMB TEST KEY is used : rpmb/rpmbk.bin

Follow the procedure described in rpmb/README.md of the starter package

Warning
This procedure is not yet available on Windows Host. Waiting availability, please load, flash and start the OpenSTDroid v5.1.1 starter package on st.com. It integrates an automatic mechanism to fuse the RPMB key if not already performed with the TEST KEY
  • Flash the eMMC with the partition images.
STM32_Programmer_CLI -c port=usb1 -w flashlayout/FlashLayout_emmc_cm33tdcid.tsv

This operation takes several minutes.

See the STM32CubeProgrammer article to know more about the flashing operation.

6. Booting the board[edit | edit source]

Now that the image is flashed on the STM32MP257x-EV1 Evaluation board, let's finalize the system configuration:

  • Step 0: Check that the LVDS display board is well connected.
  • Step 1: Check the configuration of the switches and jumpers:
    • The boot related switches must be configured so that the device (e.g. eMMC) on which the image has been flashed is selected as boot source.
The figure below shows the boot switches for the recommended boot from eMMC (for M33-TD flavor ).
Boot from eMMC for M33-TD flavor
  • Step 2: (optionally) Connect a USB keyboard and/or a USB mouse (not provided) using the USB type-A ports (3 in the picture below).
  • Step 3: (optionally) Connect an Ethernet cable (not provided) to the dedicated connector (2).




USB Power Delivery Type-C (Power or STLINK)ETHERNET 2/PHY ETH2 (Ethernet)2 x USB type A (host) (such as a mouse or keyboard USB driver)USB2.0 DRD Type-C  (programmable through CubeProgrammer)microSD<sup>™</sup> card slotMB1936 5V/3A power supply jack (Power)RESET button
STM32MP257x-EV1 Evaluation board connections

STM32MP257F-EV1 shown here (picture is not contractual)
Warning
If the supply is provided via the USB Power Delivery Type-C (1), to have the possibility to use ST-Link or the consoles, the USB Power Delivery Type-C (1) must be connected to a PC with USB Type-C/Type-C cable. The USB Type-C on the PC must be a USB Power Delivery Type-C.
Information
Via ST-LINK, it is possible to have access to 2 consoles: one for Cortex-M and one for Cortex-A.



  • Step 4: Check the power jumper position and connect:
    • either the USB Power – TypeC cable to the connector (1).
    • or power supply (5V, 3A) to the power connector (6) of the MB1936
  • Step 5: (optionally) Install and configure a remote Terminal program (e.g. Minicom on Ubuntu Linux PC or Tera Term on Windows PC) onto your host PC, and connect the ST-LINK/V3 USB type-C port (1) to a host PC that runs a Terminal program with ST-LINK/V3 virtual port.
  • Step 6: Press the reset button (7) to reset the board.

The board boots and the system is available after few seconds.

7. How to go further?[edit | edit source]

Now that the image is flashed on the STM32MP25 Evaluation board, you might want to switch to the STM32MPU OpenSTDroid Distribution Package, in order to modify or tune the STM32MPU Embedded Software distribution with your own developments.