Last edited 2 months ago

Android-based OpenSTDroid ecosystem release note

Applicable for STM32MP25x lines


This article describes the content of the v6.2.1 release of the OpenSTDroid (st-android-16.0.0-2026-09-08 tag).

1. Delivery scope and purpose[edit | edit source]

The OpenSTDroid distribution provides all the components required for running, developing and/or making your own platform based on Android™ framework. It runs on the Arm® Cortex®-A35 processors, and is a fundamental part of the Android-based OpenSTDroid embedded software.

It is compatible with Android 16.0.0.

It is provided as an example. The Android certifications are not guaranteed.

2. Release content[edit | edit source]

2.1. Main software components[edit | edit source]

  • Embedded software components
    • Android version v16.0.0 (AOSP android-16.0.0_r4 tag)
    • Kernel version v6.6.129 (AOSP common kernel) + updates for STM32MP25 and associated boards
    • TF-A version v2.10.24 + updates for STM32MP25 and associated boards
    • U-Boot version v2023.10 + updates for STM32MP25 and associated boards
    • Trusty (AOSP android-16.0.0_r4 tag) + updates for STM32MP25 and associated boards
    • TF-M version v2.1.4 (MCUBoot is also part of the TF-M project)
    • GCC version v15.2.Rel1 (used only for MCUBoot, TF-M, TF-A and U-Boot)
    • OpenOCD version v0.12.0
    • GCnano version v6.4.21

2.2. Detailed features[edit | edit source]

2.2.1. BSP features[edit | edit source]

The OpenSTDroid v6.2.1 is based on the OpenSTLinux BSP v6.2.1, which is described in the following chapters :


The OpenSTDroid v6.2.1 adopts the M33-TD flavor architecture. It is based on the FwST-M BSP, which is described in the following chapters :

Additionally, the OpenSTDroid v6.2.1 integrates a dedicated secure OS: Trusty

2.2.2. Android features[edit | edit source]

Domain Feature STM32MP25
boards
Comment
Flash & Recovery Fastboot (U-Boot) Yes This mode can be entered by connecting an ST-Link console to the UART interface or by hardware control (button) or with adb reboot bootloader. It's useful to flash physical partitions.
Recovery Yes This mode can be entered with adb reboot recovery.
Fastbootd (recovery) Yes This mode can be entered with adb reboot fastboot. It's useful to flash logical partitions (ex: generic system image).
Boot Android Verified Boot Yes Verification with Trusty
Secure Boot Yes Full implementation available on RevX only (limited on RevY)
Update Partially Boot partition selection available (boot from _a is selected by default)
Security SELinux Yes
Runtime verification (dm-verity) Yes Based on vbmeta information provided by U-Boot
Disk encryption Partially Using adiantum software solution
Trusted environment Yes Trusty
Keystore Yes Keymint based on Trusty
Gatekeeper Yes Gatekeeper based on Trusty
Display & Graphics OpenGLES 3.1 Yes Restriction: AEP ES31A is not supported
Vulkan 1.3 Yes Restriction: only for application purpose
Display (LVDS) Yes Maximum resolution: 1080p
HDMI Yes Maximum resolution: 1080p; Audio is not supported
Multimedia Audio output Partially No audio output on the STM32MP257F-EV1 and limited to HDMI output for the STM32MP257F-DK boards.
Audio input No No audio input on the STM32MP257F-EV1 and on the STM32MP257F-DK boards.
Camera Yes imx335 connected on CSI connector (maximum resolution (4K page configuration): 1920x1440)
Video HW decode Yes H.264 and VP8 (maximum resolution: 1080p60)
Video SW decode Yes Maximum resolution: 480p30
Video HW encode No
Network and connectivity Ethernet Yes Only ETH2 enabled for STM32MP257F-EV1 board
Wifi Yes With Wi-Fi USB adapter (ex: NETGEAR AC1200) for STM32MP257F-EV1 board
Wifi hotspot Yes With Wi-Fi USB adapter (ex: NETGEAR AC1200) for STM32MP257F-EV1 board
BT / BLE No Bluetooth available on STM32MP257F-DK board, but not integrated in Android.
USB Yes USB2.0 on the STM32MP257F-EV1 board. USB3.0 on the STM32MP257F-DK board.
Mass storage / MTP / PTP / NCM.
Systems Boot control Partially Use boot control based on misc partition
Power control Partially Use power HAL example (stub)
Thermal control Partially Use thermal HAL example (stub)
Sensors Sensors No No sensor available on the STM32MP257F-EV1 and on the STM32MP257F-DK boards.
Hub No No sensor available on the STM32MP257F-EV1 and on the STM32MP257F-DK boards.
Debug ADB (USB) Yes
ADB (Ethernet) Yes
Perfetto Yes
Storage USB storage Yes Only for external storage
microSD card Yes For default user data (eMMC / microSD card hybrid configuration) or for external storage
eMMC Yes For read-only partitions and for default user data (eMMC configuration)
Others Lights Yes
Touchscreen Yes

3. Restrictions[edit | edit source]

3.1. BSP restrictions[edit | edit source]

The OpenSTDroid v6.2.1 is based on the OpenSTLinux BSP v6.2.1, see the associated restrictions.

Trusty restrictions :

  • Embedded HW crypto is not integrated

3.2. Android restrictions[edit | edit source]

OpenSTDroid is provided as example.

In this context, compliance tests (VTS/CTS) are not ensured (but they are executed and treated as much as possible).

Warning

It's important to notice that the kernel version (6.6) is not the one expected for Android 16 (6.12). It means that some kernel tests can't be executed and that you can get a pop-up window on start with the GSI.

Main restrictions concerning the OpenSTDroid distribution:

  • Embedded HW video encoder is not integrated
  • FOTA mechanism for first boot stage not available
Information

The eMMC RPMB must be provisioned with the TEST KEY (see RPMB authentication key setting) when using the STM32MP25 reference boards

4. Minor release updates[edit | edit source]

STMicroelectronics can deliver corrections and some light changes on purpose through github® components.

5. How to get started with OpenSTDroid[edit | edit source]

Refer to Android-based OpenSTDroid embedded software article.

6. Intended audience[edit | edit source]

The targeted audience is STM32MPU customers and partners.

7. Licensing[edit | edit source]

This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).

All packages use the same source components. All components and their respective licenses are listed here.

8. Supported hardware[edit | edit source]

This software delivery is compatible with the following boards:

STM32MP25 boards
Boards PCBs list Main features Ordering

STM32MP257F-EV1 Evaluation board
  • MB1936 (main board)
  • STM32MP257FAI3[1] Rev.Y
    • Arm®-based dual Cortex®-A35 1500 MHz
    • Secure boot and cryptography
    • 2 x 16-Gbit DDR4, 32 bits, 1200 MHz
  • PMIC STPMIC25 Cut1.1
  • Optional expansion boards
    • LVDS WSVGA display B-LVDS7-WSVGA board
    • 5-megapixel image sensor raw Bayer B-CAMS-IMX board
    • DSI to HDMI adapter Full HD 30fps B-LCDAD-HDMI1 board

Evaluation board with STM32MP257F MPU


STM32MP257F-DK Discovery kit
  • MB1605 (main board)
  • STM32MP257FAK3[1] Rev.Y
    • Arm®-based dual Cortex®-A35 1500 MHz
    • Secure boot and cryptography
    • 32-Gbit LPDDR4, 32 bits, 1200 MHz
  • PMIC STPMIC25 Cut1.1
  • Optional expansion boards
    • LVDS WSVGA display B-LVDS7-WSVGA board
    • 5-megapixel image sensor raw Bayer B-CAMS-IMX board

Discovery kit with STM32MP257F MPU


9. Associated tools[edit | edit source]

Refer to the Development tools release notes .

10. Demonstration applications[edit | edit source]

The OpenSTDroid distribution is delivered with several applications provided as example.

10.1. STLauncher[edit | edit source]

Simple launcher application example.

The associated application project is available on GitHub® (compatible with Android Studio IDE): STLauncher application.

10.2. STVideo[edit | edit source]

Simple video application illustrating how to play a video. The video files must be stored in the Movies directory on an external storage (such as a USB storage).

The associated application project is available on GitHub® (compatible with Android Studio IDE): STVideo application.

10.3. STCamera[edit | edit source]

Simple camera application illustrating how to use the camera (preview and take picture services). The Camera imx335 must be connected on the CSI connector.

The associated application project is available on GitHub® (compatible with Android Studio IDE): STCamera application.

10.4. STGraphics[edit | edit source]

Simple 2D and 3D graphics application illustrating usage of OpenGLES v2.0.

The associated application project is available on GitHub® (compatible with Android Studio IDE): STGraphics application.

10.5. STPerf[edit | edit source]

Performance overlay application used to demonstrate in foreground the device performance (CPU usage, GPU usage, frame rate). The application can be configured and stopped via a notification system interface.

Limitation: this application is available only in debug build. GPU performance is not yet available.

The associated application project is available on GitHub® (compatible with Android Studio IDE): STPerf application.

11. References[edit | edit source]


12. Archives [edit | edit source]

STM32MPU release OpenSDroid release note
STM32 MPU-Ecosystem-v6.2.0 Android-based OpenSTDroid ecosystem release note - v6.2.0
STM32 MPU-Ecosystem-v5.1.0 STM32 MPU OpenSTDroid release note - v5.1.0 page for the v5 ecosystem releases (in archived wiki)