Last edited 9 months ago

STM32MP21 microprocessor

Applicable for STM32MP21x lines

If you are looking for a cost effective and power efficient microprocessor with a state-of-the-art Linux distribution, the STM32MP21 may be your solution!
Still want an heterogeneous architecture, like the other STM32MP2 Series microprocessors? No problem, the STM32MP21 embeds an Arm® Cortex®-A35 and an Arm® Cortex®-M33.
And, if you want to scale up to the STM32MP23 and STM32MP25, we deliver the STM32MP21 in the same 10x10 package that is pin compatible with the rest of the family.

This article introduces the STM32MP21x lines , and gives information about the part number codification and block diagram. Then technical aspects are introduced, providing information on:

  • STM32MP21 documentation,
  • articles dedicated to internal peripherals that make the transition towards the software frameworks required to control these peripherals,
  • the board supporting STM32MP21 microprocessors,
  • the supported software distributions, that can be downloaded into the STM32MP21 microprocessors.


1. Introduction[edit | edit source]

STM32MP21 microprocessors are targeting industry 4.0, human-machine interfaces (up to 1080p60), and a wide range of smart products that require a very high level of security, such as IoT and payment applications.

STM32MP21 microprocessors are based on a heterogenous architecture embedding an Arm® Cortex®-A35 core and an Arm® Cortex®-M33 coprocessor, both supporting Arm®Trustzone® mode for secure operations.

Either the Arm® Cortex®-A35 dual core or the Arm® Cortex®-M33 can be selected as the boot core and trusted domain (TD), allowing to match various use cases and system constraints, as described in How to choose the STM32MP2 boot flavor article.

On top of this, it relies on the connectivity foundations from the STM32MP2 series with dual Gigabit ETH (with TSN end-point support), that enlarge the possibilities in industrial, smart city and smart home applications.

The STM2MP21 also comes with a resource isolation framework (RIF) that is a very flexible and powerful infrastructure allowing to decide which Arm® Cortex® will boot first and to associate each peripheral to a hardware execution context or traffic initiator (like a DMA).

2. Part number codification[edit | edit source]

The figure below shows the differences between the three STM32MP21x lines, with their security and frequency options. Each line can be delivered in one of four packages represented on the right side: refer to the technical documentation to get details on the available features per package.

The tables below explain how the part numbers are encoded for all the above combinations.

2.1. STM32MP21x lines[edit | edit source]

Cortex-A35 Cortex-M33 Display Camera FDCAN Gigabit Ethernet interfaces
STM32MP215 Single Yes Yes Parallel and MIPI CSI-2 2 2
STM32MP213 Single Yes No Parallel 2 2
STM32MP211 Single Yes No Parallel No 1

2.2. Security and Arm Cortex-A35 frequency[edit | edit source]

Security Cortex-A35 frequency
STM32MP21xA Basic 1200 MHz[1]
STM32MP21xC Secure boot + Cryptography 1200 MHz[1]
STM32MP21xD Basic 1500 MHz[1]
STM32MP21xF Secure boot + Cryptography 1500 MHz[1]

2.3. Packages[edit | edit source]

STM32MP21xxAM TFBGA289, 14x14mm, pitch 0.8mm 123 GPIOs
STM32MP21xxAN VFBGA273, 11x11mm, pitch 0.5mm 123 GPIOs
STM32MP21xxAL VFBGA361, 10x10mm, pitch 0.5mm 123 GPIOs
STM32MP21xxAO VFBGA225, 8x8mm, pitch 0.5mm 98 GPIOs

2.4. Junction temperature[edit | edit source]

STM32MP21xxxx3 - 40 to + 125 °C

3. Block diagram[edit | edit source]

Here below the STM32MP215F block diagram offering the richest set of features of the STM32MP21 microprocessor.

The figure above shows a functional view of the design that does not aim to be aligned with the real design: it shows the available features and not how they are implemented into the microprocessor.

4. Technical documentation[edit | edit source]

5. Internal peripherals[edit | edit source]

Internal peripherals

STM32MP21 peripherals overview article gives a description of all the internal peripherals available on STM32MP21 devices, with direct links to the articles where is introduced:

  • an overview of each peripheral,
  • the list of instances available for each peripheral type,
  • information on the way each instance can be shared between Arm® Cortex®-A35 and Cortex®-M33 cores,
  • direct links to the software frameworks used to control the peripheral from different Arm® cores and security modes such as Cortex®-A35 nonsecure, Cortex®-A35 secure, Cortex®-M33 nonsecure, or Cortex®-M33 secure.

6. How to get further with STM32MP21 ecosystem[edit | edit source]

6.1. Boards[edit | edit source]

The list of boards that integrate STM32MP21 devices can be found in STM32MP21 boards article.

6.2. Supported software distributions[edit | edit source]

The embedded software distributions supported for the boards that integrate STM32MP21 devices can be found in the following articles:

7. References and foot notes[edit | edit source]

  1. ↑ 1.0 1.1 1.2 1.3 Exposure to maximum rating conditions for extended periods may affect device reliability. Device mission profile (application conditions) is compliant with JEDEC JESD47 qualification standard. Refer to the STM32MP21 datasheets and AN5729 for further information.