Last edited 2 months ago

Device life cycle

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


1. Article purpose[edit | edit source]

The purpose of this article is to:

  • Explain the different life cycle available on STM32 MPU.
  • Explain when they will be used.
  • Explain how to manage the transitions.

2. Life cycle purpose[edit | edit source]

The STM32 MPU life cycle manages the device behavior of some security features during different development phases. It enables some secure mechanisms that are specific to every device family to enforce the security of the system.

3. Life cycle overview[edit | edit source]

The life cycle of the STM32 MPU is following the below diagram state:

Each state of the diagram refers to a specific device behavior:

3.1. Unsecured[edit | edit source]

This is the unique and final state for devices that do not embed the secure features:

  • STM32MP13xA/D lines 
  • STM32MP15xA/D lines 
  • STM32MP2 series

The device is ready for production, there is no possibility to enable secure features. OTP (including upper) are available to store data. TrustZone® remains still available to manage software isolation and allow access to context isolation configuration and upper OTP sections.

In this state, only unsigned firmware is supported for booting the device. The development boot is also supported to allow the user to directly connect the target with the debugger.

3.2. Secured_Unlocked[edit | edit source]

The device is delivered in this state of the product life cycle.

It allows to use unsigned firmware for booting.

In this state, all the security features can be enabled:

  • OTP upper to store secrets
  • HUK management (not supported on STM32MP15x lines )
  • Hardware cryptographic support
  • Secure boot (for test purpose)
  • Debug access

The development boot is allowed to directly connect the target with the debugger.

This state is targeted to be used for development purpose, non secure device, or to design and evaluate the security features of the device. It allows the user to simulate all the security of the platform such as secure boot implementation, secret provisioning in fuses, and cryptographic implementation without locking the device.

Warning
On STM32MP1 series, this state was also named Secured_Opened state.

3.3. Under_Provisioning[edit | edit source]

This transitioning and optional provisioning state is a specific state where the device is only limited to execute the SSP use case.

The switch to this state is done by the ROM code when:

  • The chip certificate is requested on STM32MP1 series.
  • The SSP firmware is started on STM32MP2 series.

All the OTP are available for provisioning.

As soon as the SSP process is done, the firmware will directly set the Secured_Locked life cycle.

3.4. Secured_Locked[edit | edit source]

This state is a final secure state.

On STM32MP13x lines  and STM32MP2 series, the device has been certified (SESIP3) in this state.

Once the device achieves this state, all the hardware secure mechanism are enabled:

  • Secure boot is enabled: The first booted images must be signed with the provisioned keys.
  • Isolation mechanisms are in place and must be guaranteed to guarantee the low power mechanism:
    • Backup registers security is enforced.
    • Peripheral assignment.

On STM32MP2 series, the configuration that impact the ROM code is detailed in the ROM isolation description.

Warning
On STM32MP1 series, this state was also named Secured_Closed state.

3.5. RMA[edit | edit source]

RMA is a specific analysis state where it becomes possible to debug device issues. It is protected by a password and required a specific processing to enter in this state describe in AN5827.

Information
AN5827 only describes STM32MP1 RMA process, STM32MP2x AN coming soon

It ensures that all the secrets stored in the upper OTP are no more accessible (including the hardware unique key usage).

The switch between RMA and secure closed device state is limited by a counter:

  • 1 on STM32MP13x lines 
  • 3 on STM32MP15x lines 
  • 4 on STM32MP2 series
Information
It's possible to permanently disable the RMA function by setting related OTP bit. On STM32MP1 series write all 3 bits to logic 1 on OTP word 8. On STM32MP2 series the same result can be done by setting OTP_HW_WORD3 to 0xFFFFFFFF.

4. Encoding life cycle[edit | edit source]

The life cycle uses a set of OTP words to encode the different states.

4.1. STM32MP13x lines [edit | edit source]

Secured_Unlocked
OTP word Bit Name Value
0 CFG0
Bit [9:0] OTP mode b0000010111
Under_Provisioning
OTP word Bit Name Value
0 CFG0
Bit [9:0] OTP mode b0000010111
9 CFG9
Bit [5] SSP_REQ b1
Secured_Locked
OTP word Name Value
0 CFG0
Bit [9:0] OTP mode b0000111111
9 CFG9
Bit [6:5] SSP_REQ / SSP_SUCCESS b11

4.2. STM32MP15x lines [edit | edit source]

Secured_Unlocked
OTP word Bit Name Value
0 CFG0
Bit [6] Closed_device 0
Under_Provisioning
OTP word Bit Name Value
0 CFG0
Bit [6] Closed_device 0
8 CFG8
Bit [8] SSP_REQ b1
Secured_Locked
OTP word Name Value
0 CGF0
Bit [6] Closed_device b1
8 CFG8 (only in case of SSP)
Bit [9:8] SSP_REQ / SSP_SUCCESS b11

4.3. STM32MP2 series[edit | edit source]

Secured_Unlocked
OTP word Bit Name Value
0 OTP_HW_WORD0 0xAAAA5555
Under_Provisioning
(Directly set when SSP provisioning is used)
OTP word Bit Name Value
0 OTP_HW_WORD0 0xAAAA5555
8 OTP8 0xF
18 BOOTROM_CONFIG_9
Bit [3:0] secure_boot 1 - 15
124 HCONF1
Bit 20 DISABLE_SCAN 1
Secured_Locked
OTP word Bit Name Value
0 OTP_HW_WORD0 0xAAAA5555
8 OTP8 0xFF
18 BOOTROM_CONFIG_9
Bit [3:0] secure_boot 1 - 15
Bit [7:4] prov_done 1 - 15
Bit [15:12] otp_prov_done
(Automatically set if SSP used,
remains 0 otherwise)
1 - 15
124 HCONF1
Bit 20 DISABLE_SCAN 1
Warning
To close the device, write as below the 3 OTP before a reset.

• Write 0xFF in the word 8

• Write 0xFF in the word 18.

• Write 0x100000 in the word 124 to the disabled scan state.

If these bit fields are set with different combinations than the ones listed above, then, at the next reset, the lifecycle state is seen as illegal and the device get BRICKED.

OTP can be fused in any order before reset.

stm32key command is recommended to avoid errors but any other way are possible, see below.

5. How to change the life cycle[edit | edit source]

Different ways are available to change the device life cycle:

  • In a trusted environment:
  • In an untrusted environment:
    • SSP process that directly managed the life cycle transition.