Last edited one week ago

STM32CubeMX release note

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. STM32CubeMX v6.18.0 - MPU support[edit | edit source]

1.1. Main changes[edit | edit source]

  • OpenSTLinux v6.2.1 device tree generation,
  • STM32CubeMP2 v1.3.1 & v1.3.2 code generation,
  • Starter application (StarterAppM33TD) generation for M33-TD flavor :
    • Enhance TF-M Dependency Handling in Arm®-Cortex®-M33 nonsecure project.
  • Fix OpenAMP support,
  • The STM32MP257F-DK Discovery kit is supported for M33-TD flavor .

1.2. Main restrictions[edit | edit source]

  • No restrictions

2. How to get STM32CubeMX[edit | edit source]

STM32CubeMX for Linux®, Windows® and macOS ® - STM32CubeMX v6.18.0
Download
  • Download the preferred all-in-one installer from www.st.com
    • Generic Linux® installer - STM32CubeMX-Lin
    • Windows® installer - STM32CubeMX-Win
    • macOS® installer - STM32CubeMX-macOS (Intel)
    • macOS® installer - STM32CubeMX-macOS (Apple Silicon)
Installation guide
  • Refer to the installation guide section of the STM32CubeMX user manual (UM1718) available on www.st.com.
User manual
  • When the installation is completed, see additional information about STM32CubeMX from www.st.com in the STM32CubeMX user manual (UM1718)
Detailed release note
  • Details about the content of this tool version are available in the release note from www.st.com

Minor releases may be available from the update site.

3. Archives [edit | edit source]

3.1. STM32CubeMX v6.17.0 - MPU support[edit | edit source]

3.1.1. Main changes[edit | edit source]

  • OpenSTLinux v6.2.0 device tree generation,
  • STM32CubeMP2 v1.3.0 code generation,
  • Starter application (StarterAppM33TD) generation for M33-TD flavor :
    • Add support of the Arm®-Cortex®-A35 processor start via the Arm®-Cortex®-M33 non-secure project,
    • Add TF-M API / interfaces that provides secure services,
    • Add the M33TD_NSAppCore utility that uses FreeRTOS and TF-M to handle Arm®-Cortex®-A35 processor,
    • Update project settings to handle the TF-M and non-secure binaries merging and signing,
    • Generate CMake non-secure project for OSTL integration,
  • Generation of TF-M configuration platform directory to specify some boards specific parameters for all STM32MP25/STM32MP23 project contexts,
  • Allow sharing GPIO pins between different firmware.

3.1.2. Main restrictions[edit | edit source]

  • T he STM32MP215F-DK Discovery kit is supported for M33-TD flavor , while STM32MP257x-EV1 Evaluation board and the STM32MP215F-DK Discovery kit are.

3.2. STM32CubeMX v6.16.0 - MPU support[edit | edit source]

3.2.1. Main changes[edit | edit source]

  • In the STM32CubeMX project for the A35-TD flavor ,
    • the entire clock configuration (including GPIO clock enable) has been removed from the generated HAL_<IP>_MspInit() function,
    • the GPIO clock settings has been removed from the generated from MX_GPIO_Init() function.

3.2.2. Main restrictions[edit | edit source]

Same restrictions than previous version, refer to Main restrictions of STM32CubeMX v6.15.0 - MPU support .

3.3. STM32CubeMX v6.15.0 - MPU support[edit | edit source]

3.3.1. New features supported in this release[edit | edit source]

  • Support of STM32MP21x lines 
  • Support of M33-TD flavor for STM32MP2 series.
  • New "Pin to Pin" compatibility feature for migration of STM32MP21 to STM32MP25/23 (and vice versa).
  • RIF support for STM32MP21-A35TD, STM32MP21-M33TD and STM32MP25/23-M33TD.

3.3.2. Main changes[edit | edit source]

  • OpenSTLinux v6.1.0 device tree generation
  • STM32CubeMP2 package v1.2.0 code generation

3.3.3. Main Restrictions[edit | edit source]

  • Given the major changes introduced in the current release, it is not recommended to load an IOC file in STM32CubeMX v6.15.0 if it was created with a prior version without migration. Please note that manual updates are needed in the device tree files to avoid conflicts between STM32CubeMX generated nodes and user sections.
3.3.3.1. With STM32MP2[edit | edit source]
  • The Cortex-M0+ core is currently not supported within the STM32MP2 product family at the STM32CubeMX configuration level. As a result, peripherals specifically intended for the Cortex-M0+ such as IPCC2 cannot be configured or used through STM32CubeMX.
  • When generating device tree files for the STM32MP2XxA and STM32MP2XxD products, STM32CubeMX creates references to stm32mp2Xxa.dtsi and stm32mp2Xxd.dtsi. However, OpenSTLinux-v6.1.0 does not provide these specific .dtsi files.
    • To avoid falling into this issue, we recommend to manually add empty files, named as follow stm32mp2Xxa.dtsi and stm32mp2Xxd.dtsi in the project folder. [please note that the X digit could be 1,3 or 5]
  • The DDR_UIS_SWIZZLE parameters are initially generated with the correct values for the STM32MP23 projects when activating the DDR3L memory. However, upon subsequent re-opening of the IOC, these correct values are overwritten with erroneous ones.
    • To fix the issue, the user should save the initial generated values found in the dtsi file and if s.he desires opening the IOC for a second time, s.he should update the dtsi file with the saved values of DDR_UIS_SWIZZLE
  • When reloading an existing project using STM32MP257DALx MPU with the VFBGA361 10x10 Package, and the DDR_CTRL_PHY peripheral configured, the memclk parameter in the "Parameter Settings" tab is set to 3200 MHz with a red cross, the user should adjust the value in Clock Configuration Tab, set PLL2 output frequency to 600 MHz.
  • The assignments of the RCC feature xxxRAM_CFGR is not automatically synchronized with the assignments of its hardware resources (RAM regions); therefore, these assignments must be done manually to ensure the hardware resources are correctly clocked.
  • Only STM32CubeIDE is supported.
3.3.3.2. With STM32MP13x[edit | edit source]
  • For STM32MP13 Bare metal - RTOS projects using the FreeRTOS and EWARM toolchain, the linker script chosen during the project generation is stm32mp13xx_a7_sysram.icf. This is erroneous because FreeRTOS applications on the STM32MP13 typically require the larger memory space provided by DDR, which is defined by stm32mp13xx_a7_ddr.icf.Consequently, users may face the following issue:
Error[Lp011]: section placement failed due to insufficient memory allocation (e.g., 'unable to allocate space for sections/blocks with a total estimated minimum size of 0x597c bytes').


  • The user needs to set the linker stm32mp13xx_a7_ddr.icf instead of stm32mp13xx_a7_sysram.icf when FreeRTOS is enabled in the configuration.
  • The build process for an STM32MP135F-DK (Bare Metal) project, generated via STM32CubeMX and utilizing FreeRTOS CMSIS_V2, failed in STM32CubeIDE (v1.19.0) due to a memory overflow
    • To solve the issue the user should edit the linker file STM32MP135FAFX_RAM.ld by assigning DDR_BASE alias to the RAM alias instead of SYSRAM_BASE:

REGION_ALIAS("RAM", SYSRAM_BASE); must be replaced by REGION_ALIAS("RAM", DDR_BASE);

3.4. STM32CubeMX v6.14.0 - MPU support[edit | edit source]

3.4.1. Main changes[edit | edit source]

  • Generating the build files for OpenSTLinux components with the device tree in the project folder.

3.4.2. Main Restrictions[edit | edit source]

3.4.2.1. With STM32MP25x[edit | edit source]
  • When reloading an existing project using STM32MP257DALx MPU with the VFBGA361 10x10 Package, and the DDR_CTRL_PHY peripheral configured, the “package” parameter in the “Parameter Settings” tab is set 1 instead of 2 with a red cross, the user should adjust the value from 1 to 2 to get a working project.
  • The assignments of the RCC features xxxRAM_CFGR is not automatically synchronized with the assignments of its hardware resources (RAM regions); therefore, these assignments must be done manually to ensure the hardware resources are correctly clocked.
  • Only STM32CubeIDE is supported.


3.5. STM32CubeMX v6.13.0 - MPU support[edit | edit source]

3.5.1. New features supported in this release[edit | edit source]

  • Support of STM32MP23x lines 

3.5.2. Main changes[edit | edit source]

  • OpenSTLinux-v6.0.0 device tree generation
  • STM32CubeMP2-v1.1.0 code generation
  • DDR configuration improvements for RIF feature
  • Support of STM32MP235/3/1 lines
  • Support of STM32MP25 "TFBGA 361 16x16" packages

3.5.3. Main Restrictions[edit | edit source]

3.5.3.1. With STM32MP25x[edit | edit source]
  • The MDF1 IP can't be fully configured for the projects which are using STM32MP257F-DK Discovery kit . It is partially configured in the STM32CubeMX user interface, but in the generated Device Tree the unconfigured parts are added in the User Section to avoid pin configuration redundancy.
  • When reloading an existing project using STM32MP257DALx MPU with the VFBGA361 10x10 Package, and the DDR_CTRL_PHY peripheral configured, the “package” parameter in the “Parameter Settings” tab is set 1 instead of 2 with a red cross, the user should adjust the value from 1 to 2 to get a working project.
  • The synchronization between the OSPI1/2 peripheral assignment and the RCC features OSPI1/2_CFGR assignment is not automatic; therefore, the OSPI1/2_CFGR feature assignment must be manually configured in the RCC module whenever OSPI1 or OSPI2 peripherals are used to ensure they receive the correct clock signals for proper operation.
  • The assignments of the RCC features OCTOSPIx_CFGR and xxxRAM_CFGR are not automatically synchronized with the assignments of their hardware resources (OCTOSPIx peripherals and RAM regions); therefore, these assignments must be done manually to ensure the hardware resources are correctly clocked. STM32CubeMX provides tips to help for each of these features.
  • IOM/OSPI: to handle properly the clocks when OSPIx is used in Multiplexed mode and OSPIy is not used, the (RCC) OSPIy_CFGR feature should have the same assignment as OSPIx_CFGR one.
  • When FMC is assigned to a Cortex®-M33 non-secure Cube firmware (HAL & LL) context, the NVIC panel is not displayed.
  • Only STM32CubeIDE is supported.
3.5.3.2. With STM32MP13x[edit | edit source]
  • When using the STM32CubeMP13 bare-metal firmware and activating Azure® RTOS ThreadX or FreeRTOS, the user should Copy the startup_stm32mp13xxyy_ca7_rtos.c and system_stm32mp13xx_A7_rtos.c from the firmware side and ensure that they are correctly included in the project.
  • The limitations encountered with STM32CubeMx V6.12.0 regarding STM32MP13x persist in theSTM32CubeMx V6.13.0

3.5.4. How to compile device tree in OpenSTlinux[edit | edit source]

An example of the device tree, generated by STM32CubeMX, compilation, with OpenSTlinux, is described in How_to_compile_the_device_tree_with_the_Developer_Package article.

3.6. STM32CubeMX v6.12.1 - MPU support[edit | edit source]

3.6.1. Main fixed issues[edit | edit source]

The STM32CubeMX V6.12.1 solves the following issues:

  1. Device tree generation: Misconfiguration of some peripherals in the STM32MP257F-EV1 and STM32MP257F-DK ".ioc" files is causing issues in the device tree generation.
  2. DDR mapping: The address A19 cannot be assigned in DDR mapping.
  3. RCC configuration in Cortex®-M33: When configuring a peripheral in the Cortex®-M33 context, the FLEXCLKGEN settings for the RCC node in the device tree (DT) are not generated.

3.7. STM32CubeMX v6.12.0 - MPU support[edit | edit source]

3.7.1. New features supported in this release[edit | edit source]

  • Support of STM32MP25x lines 

3.7.2. Features already supported in previous releases[edit | edit source]

  • Support of STM32MP13x lines 
  • Support of STM32MP15x lines 
  • Support for Azure RTOS ThreadX, FileX, LevelX, NETX and USBX, for STM32CubeMP13 package release

3.7.3. Main changes[edit | edit source]

  • Add new Intropack openstlinux-6.1-yocto-mickledore-mpu-v24.06.26 for STM32MPU (STM32MP1 series & STM32MP2 series).

3.7.4. Main Restrictions[edit | edit source]

3.7.4.1. With STM32MP25x[edit | edit source]
  • Only STM32CubeIDE is supported.
  • STM32CubeMX configurations (IOC) for STM32MP257F-EV1 Evaluation board and STM32MP257F-DK Discovery kit do not configure LTDC in secure mode (trusted UI is disabled). This differs from OpenSTLinux software configuration where the trusted UI is enabled for these boards.
  • The synchronization between OSPIx peripherals assignments and the RCC features OSPI1/2_CFGR assignments is not "automatically" performed. OSPI1/2_CFGR features assignments should be done whenever OSPI1/2 are used in order to clock correctly the peripheral(s).
  • The assignments of the RCC features OCTOSPIx_CFGR and xxxRAM_CFGR are not automatically synchronized with the assignments of their hardware resources (OCTOSPIx peripherals and RAM regions). These assignments should be done manually to clock correctly the hardware resources. STM32CubeMX displays tips helpers for each of these features.
  • In the pinout & configuration view, the U-Boot context assignments are not synchronized with the Linux® context assignments. Whenever a peripheral is assigned for U-Boot, it should be also assigned for Linux®. (the opposite is not true).
  • IOM/OSPI: to handle properly the clocks when OSPIx is used in Multiplexed mode and OSPIy is not used, the (RCC) OSPIy_CFGR feature should have the same assignment as OSPIx_CFGR one.
  • When FMC is assigned to a Cortex®-M33 non-secure Cube firmware (HAL & LL) context, the NVIC panel is not displayed.
  • The device trees generated by STM32CubeMX for the STM32MP257F-DK Discovery kit and STM32MP257F-EV1 Evaluation board boards are fully functional. Although these device trees are close to the "STM32 MPU embedded software device tree" configuration, some differences may exist. Refer to the chapter External_device_tree for details on "STM32 MPU embedded software device tree".
  • When creating a STM32MP25 empty project, a partial configuration of the (RIF) RISAFx and RISABx sub-system is pre-filled. This configuration is the OpenSTLinux one but limited to the definition of the regions name and size (security not defined).

These are the complete OpenSTLinux configuration including security aspects:


RISAF1(BKPSRAM)



RISAF1(BKPSRAM)



RISAF2(OCTOSPI1&2)



RISAF2(OCTOSPI1&2)



RISAF4(DDR)



RISAF4(DDR)



RISAF5(PCIE)



RISAF5(PCIE)



RISAB1(SYSRAM1)



SYSRAM1(BKPSRAM)



RISAB2(SYSRAM2)



RISAB2(SYSRAM2)



RISAB3(SRAM1)



RISAB3(SRAM1)



RISAB4(SRAM2)



RISAB4(SRAM2)



RISAB5(RETRAM)



RISAB5(RETRAM)



RISAB6(VDERAM)



RISAB6(VDERAM)

3.7.4.2. With STM32CubeMP13 package[edit | edit source]
  • Only STM32CubeIDE is supported.
  • Only application context is supported.
  • Standard version of LevelX, USBX, NetX middlewares integrated without STM32MP13 platform specific patches.
  • When using the STM32CubeMP13 package and activating Azure® RTOS ThreadX, the STM32CubeIDE linker file must contain the following section to avoid compilation issues:
.stack :
{
_stack_bottom = ABSOLUTE(.) ;
/* Allocate room for stack. This must be big enough for the
IRQ, FIQ, and SYS stack if nested interrupts are
enabled.*/
. = ALIGN(8) ;
. += 32768 ;
_sp = . - 16 ;
_stack_top = ABSOLUTE(.) ;
} >RAM
_end = .;