Last edited 4 months ago

STM32CubeMP13 Package release note - v1.2.0

Applicable for STM32MP13x lines


This article describes the content of STM32CubeMP13 package release version v1.2.0, which is part of the STM32 bare metal - RTOS embedded software.

1. Delivery purpose and scope[edit | edit source]

The STM32CubeMP13 package is a software package running on Arm® Cortex®-A7 processor.

This release includes:

  • The STM32Cube HAL: STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
  • Low-layer APIs (LL APIs) offering a fast, lightweight, expert-oriented layer that is closer to the hardware than the HAL.
    LL APIs are only available for a limited set of peripherals.
  • A consistent set of middleware components such as AzureRTOS or FreeRTOS (new in this release).
  • All embedded software utilities delivered with a full set of examples.

It also includes:

  • BSP for the STM32MP135F-DK Discovery kit (LED, button, camera, LCD, SD card, and COM ports)
  • Projects: several projects (examples, applications, external loader, and templates) are implemented in IDEs.
    • STM32CubeIDE delivered by ST
      • All the STM32MP135F-DK projects are available on STM32CubeIDE.

2. Intended audience[edit | edit source]

The targeted audience is STM32 MPU customers and partners.

3. Licensing[edit | edit source]

All licenses applicable to STM32CubeMP13 package are available here.

4. Supported devices[edit | edit source]

The drivers provided within this package support all STM32MP13x lines .

5. Supported hardware[edit | edit source]

The software examples and the drivers delivered in this package are applicable for the following boards:

6. Release content[edit | edit source]

This release is the maintenance release of the STM32CubeMP13 software package running in standalone on the Arm® Cortex®-A7 of STM32MP13x lines .

The full content is available in STM32CubeMP13 package content. This STM32CubeMP13 package can then be used as any STM32Cube package running on STM32 MPU of STMicroelectronics.

6.1. Main changes[edit | edit source]

Main changes, compared to STM32CubeMP13-v1.1.0 package are:

  • FreeRTOS as middleware (in addition to AzureRTOS)
  • LwIp middleware
  • LwIp Dual ethernet example
  • USB Host based on USB OTG IP example
  • Interoperability with PRG_TOOLBOX_DFU
  • FSBLA project for IAR
  • External Loader as source code
  • OpenBootLoader as source code
  • Various fixes
  • CVE fixes

6.2. Changes per component[edit | edit source]

6.2.1. HAL drivers[edit | edit source]

  • Support for 2 ETH interface at same time.
  • Check overview and all available HAL drivers in HAL drivers

6.2.2. LL drivers[edit | edit source]

  • No major changes in LL drivers.
  • Check overview and all available LL drivers here LL drivers

6.2.3. BSP[edit | edit source]

  • No major changes in BSP drivers. 
  • Refer to BSP Drivers section here BSP drivers.

6.2.4. CMSIS[edit | edit source]

  • Bit and registers definition for STM32MP13x lines .
  • Support for IAR workbench has been added.
  • For more details, refer main section CMSIS

6.2.5. Middleware[edit | edit source]

  • AzureRTOS (ThreadX, LevelX, FileX, USBX, NetXDuo)
  • USB Library (Device and Host)
  • OpenBootloader
  • LWIP
  • Free RTOS
  • Check overview of middleware's in STM32CubeMP13 Package article

6.2.6. Projects[edit | edit source]

  • Check project section here Projects for details of projects implemented.
Information
Note: For detailed information, read file Release_Notes.html delivered with the STM32CubeMP13 Package.

6.3. Released components[edit | edit source]

6.3.1. Drivers[edit | edit source]

Component Version Notes
CMSIS CoreA v5.8.0 CMSIS CoreA Release Notes
STM32MP13x CMSIS v1.2.0 STM32MP13xx CMSIS Release Notes
STM32MP13x HAL v1.2.0 HAL Release Notes
BSP STM32MP13x_DISCO v1.2.0 BSP Release Notes

Find here the list of available HAL, LL and BSP drivers.

6.3.2. Middleware[edit | edit source]

Component Version Notes
ThreadX v6.2.0 -
NetXduo v6.2.0 -
USBX v6.2.0 -
FileX v6.2.0 -
LevelX v6.4.0 -
cmsis_rtos_threadx v1.1.0 -
STM32 USB Device Library v2.11.0 -
STM32 USB Host Library v3.5.1 -
OpenBootloader v5.0.0 -
FreeRTOS v10.6.2 -
LwIP v2.2.0 -

6.4. Released projects[edit | edit source]

The STM32CubeMP13 package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported development environment is STM32CubeIDE (works on multiple operating systems) and uses the GNU toolchain.

  • All STM32MP135F-DK projects are available with STM32CubeIDE.

IDE ready projects:

STM32MP135F-DK
Number of projects 91

Find in this article STM32CubeMP13_Package#Projects, the exhaustive list of available projects for STM32MP135F-DK Discovery kit :

Information
Note: Refer to article Introduction to boot mode to get more information about different boot modes in STM32MP135F-DK Discovery kit

The recommended supported toolchain for STM32MP13 is STM32CubeIDE (All-in-one multi-OS development tool).

7. Restrictions[edit | edit source]

  • None.

8. How to get started with STM32CubeMP13 Package[edit | edit source]

Refer to STM32CubeMP13 Package - Getting started article.

9. Associated tools[edit | edit source]

Refer to Referenced tools release notes