Last edited 10 hours ago

Latest wiki

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This page aims to provide link to the main/flagship wiki

The wiki is versioned (through different URLs), and its versions correspond to major developments in the Yocto-based OpenSTLinux flagship ecosystem, of which the BSP serves as the basis for the other Linux-based ecosystems.

A release flow for the Yocto-based OpenSTLinux ecosystem designates all the releases of the Yocto-based OpenSTLinux ecosystem which are based on the same versions of the major software components such as the Linux® kernel (see details in the table).
Each vx release flow groups together all the vx.y.z releases of the Yocto-based OpenSTLinux ecosystem, and has its own wiki.

Thus, the wiki versioning is driven by the vx release flow (implied meaning, of the Yocto-based OpenSTLinux ecosystem), but any wiki contains also releases for other ecosystems such as the bare metal - RTOS ecosystem or the Android-based OpenSTDroid ecosystem.
The most recent flow is associated with the latest wiki also known as main/flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

This current wiki is the wiki for the v6 flow (v6.y.z ecosystem releases): if you need information about this ecosystem releases flow, continue browsing this wiki.

However, if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to browse the main/flagship wiki that contains the latest STM32 MPU ecosystems release notes:

Wiki Yocto-based OpenSTLinux ecosystem releases Major software components
STM32 MPU flagship/latest wiki for v7 flow

(for STM32 Arm® Cortex® MPUs )

v7.0.0 (Nov 2026) (for STM32MP1 series and STM32MP2 series)

Linux® kernel v6.18 (LTS)
U-Boot v2026.04
TF-A v2.14
OP-TEE v4.8.0
OpenEmbedded v6.0 (wrynose)

This wiki - Wiki for v6 flow

(for STM32 Arm® Cortex® MPUs )

v6.2.1 (Jun 2026) (for STM32MP1 series and STM32MP2 series)
v6.2.0 (Feb 2026) (for STM32MP1 series and STM32MP2 series)
v6.1.0 (Jun 2025) (for STM32MP1 series, STM32MP23x lines  and STM32MP25x lines )
v6.0.0 (Nov 2024) (for STM32MP1 series and STM32MP25x lines )

Linux® kernel v6.6 (LTS)
U-Boot v2023.10
TF-A v2.10
OP-TEE v4.0.0
OpenEmbedded v5.0 (Scarthgap)