Last edited one month ago

STM32 MPU ecosystems release notes

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

An STM32 MPU ecosystem is composed of:

  • embedded software (distributions and packages),
  • STM32 MPU boards,
  • set of developments tools,
  • set of documents.

This category regroups all release notes constituting the different STM32 MPU ecosystems provided in this wiki (for the v6 flow - v6.y.z ecosystem releases).

There are 2 STM32 MPU ecosystem flagships:

  • the Yocto-based OpenSTLinux ecosystem, whose embedded software running on Arm® Cortex®-A processor(s) is a Linux® distribution. The other Linux-based ecosystems align their embedded software on the BSP of this Yocto-based OpenSTLinux ecosystem.
  • the bare metal - RTOS ecosystem, whose embedded software running on Arm® Cortex®-A processor(s) is a STM32Cube MPU package (similar to the well-known the STM32 MCU packages for STM32 MCU series) with a RTOS or without (bare metal).

Below are listed all STM32 MPU ecosytems provided in this wiki and pointing on their associated release notes

STM32 MPU ecosystems Suppliers Supported devices Last ecosystem release note For Linux-based ecosystems, version of the last ported OSTL BSP
Yocto-based OpenSTLinux ecosystem ST STM32MP1 series
STM32MP2 series
Yocto-based OpenSTLinux ecosystem release note v6.2.1
Bare metal - RTOS ecosystem ST STM32MP13x lines  STM32CubeMP13 bare metal - RTOS ecosystem release note Not applicable
Android-based OpenSTDroid ecosystem ST STM32MP25x lines  Android-based OpenSTDroid ecosystem release note v6.2.1
OpenBMC-based Linux ecosystem ST STM32MP25x lines  OpenBMC-based Linux ecosystem release note v6.2.0
Buildroot-based Linux ecosystem via partner STM32MP1 series
STM32MP2 series
Buildroot-based Linux ecosystem release note v6.2.0
OpenWrt-based Linux ecosystem via partner STM32MP1 series
STM32MP2 series
OpenWrt-based Linux ecosystem release note v6.1.0