Android-based OpenSTDroid embedded software


The Android-based OpenSTDroid embedded software is part of the STM32 MPU embedded software offer.
It is a set of software (see architecture overview), system build and development tools created to ease the development to be done on top of STM32 MPU devices.

Android-based OpenSTDroid embedded software includes:


OpenSTDroid distributionFwST-M PackagesAndroid-based OpenSTDroid embedded software

The Android-based OpenSTDroid embedded software offers two development packages that let developers select the support that best meets their needs:

  • the OpenSTDroid starter package to quickly and easily start with the evaluation boards. It delivers a software image (binary).
  • the OpenSTDroid distribution package to create your own Android-based embedded software, as well as your own starter package. It delivers the source code of all the software components of the Android-based OpenSTDroid embedded software, and uses the Android build process.


OpenSTDroid starter packagesOpenSTDroid distribution packagesDevelopment packages for Android-based OpenSTDroid embedded software

STM32 supported device Boards Starter Package Distribution Package Ecosystem release note
STM32MP25x lines  STM32MP25 Evaluation boards STM32MP25 Evaluation boards - OpenSTDroid Starter Package STM32MPU OpenSTDroid Distribution Package Android-based OpenSTDroid ecosystem release note
STM32MP25 Discovery kits STM32MP25 Discovery kits - OpenSTDroid Starter Package

If you are not yet familiar with the STM32MPU Embedded Software Packages, please read also this article Which Package better suits your needs.


Subcategories

This category has the following 4 subcategories, out of 4 total.