Last edited one month ago

MB1605

Applicable for STM32MP23x lines, STM32MP25x lines

This article provides an overview of the MB1605 main board.

1. Board overview[edit | edit source]


Main board MB1605, revision C-01 : part of the STM32MP257x-DK Discovery kit .

STM32MP257x-DK Discovery kit front side
STM32MP257F-DK shown here (picture is not contractual)


Details about the LEDs:

  • LD11 turns green when a power connection is established (the power cable is inserted into the CN21 connector).
  • Two general-purpose color LEDs (LED1 and LD9) are available as light indicators:
    • The blue LED (LED1) is used as the Linux® Heartbeat LED, which blinks as long as Linux® is running on the Arm® Cortex®-A.
    • The orange LED (LD9) is used as an STM32Cube example verdict LED.
  • The two LEDs, LD7 (red) and LD8 (green), are free user LEDs that can be by configured by the user for any purpose, as explained in the LEDs and buttons on STM32 MPU boards wiki article.
  • The LD5 and LD6 LEDs are used as an ST-LINK status indicator.


STM32MP257x-DK Discovery kit back side
STM32MP257F-DK shown here (picture is not contractual)



2. Links[edit | edit source]

MB1605 schematics