Last edited 5 months ago

OpenSTDroid distribution

Applicable for STM32MP25x lines

The OpenSTDroid distribution runs on Arm® Cortex®-A processors. It is a subset of the Android-based OpenSTDroid embedded software.

It includes the following collection of software components:

  • OpenSTLinux BSP with TF-A, U-Boot and Linux® kernel (but without OP-TEE secure OS)
  • Trusty TEE secure OS
  • Application frameworks that rely on the services provided by the OpenSTLinux BSP and The Trusty secure OS to provide specific functionalities (such as code libraries, APIs, and tool sets) to ease the development of software applications:
    • Android™ application frameworks running in Linux OS user space (see AOSP[1] for more details).
    • Trusty user space library used for developing Trusted Applications (TA).

The OpenSTLinux BSP for Android has some specificities:

  • The Linux kernel source is based on the Common Kernel available from AOSP[2].
  • The Linux kernel configuration is based on the reference configuration available from AOSP[3].

Android application frameworks are based on the AOSP platform manifest[4]. By default, one of the Google tags[5] is used as a reference.

The Google services (for example Cast, Drive, or Maps) are neither embedded nor validated within this Android-based OpenSTDroid embedded software.

1. How to get the software for this distribution?[edit | edit source]

The OpenSTDroid distribution is available through the two Packages (Starter and Distribution) of the Android-based OpenSTDroid embedded software.

2. References[edit | edit source]