Last edited 2 months ago

STM32MP21 OTP mapping

Applicable for STM32MP21x lines

1. Memory mapping[edit | edit source]

The table below gives an overview of the BSEC OTP memory mapping with useful information in the context of this Wiki reading. It gives the global mapping view including the SoC restricted layout (immutable) and the additional ecosystem choice that is used with OpenSTLinux ecosystem.

  • OTP words 0 to 127 are called lower OTP and are bit wise programmable.
  • OTP words 128 to 255 are called middle OTP and are bulk programmable.
  • OTP words 256 to 383 are called upper OTP and are bulk programmable. These OTP are the one where sensitive information (such as password or private keys) must be stored.


Further information for the words and fields that are not explicitly described here can be found in the reference manual.

Important
The user-modifiable OTPs are listed in the reference manual OTP mapping table and are identified as Customer in the Owner column.

1.1. Lower OTP region[edit | edit source]

For both TD flavor (A35-TD or M33-TD)
OTP word Bit field (size) Name Description
0 OTP_HW_WORD0 OTP Check Word (virgin -> non virgin)
1 OTP_HW_WORD1 OTP Security word to close security state BSECXW, see device life cycle page
2 OTP_HW_WORD2 OTP Word for re-opening via RMA password : RMA bits
3 OTP_HW_WORD3 OTP Word for re-opening via RMA password : RMA tries bits
4 OTP_HW_WORD4 OTP word for TK Retries (ECIES)
5 to 7 ID0 / ID1 / ID2 Device Unique ID
8 OTP_CID_PROV SSP firmware lifecycle status
  • 0x0F : life cycle state is UNDER_PROVISIONING
  • 0xFF : life cycle state is SECURED_LOCKED
Warning
Setting only this bitfield is not enough to close the product and will brick it.

Please refer to device life cycle for the appropriate sequence.

9 RPN_CODING STM32MP21 Reference Manuals
10

BOOTROM_CONFIG_1

0-0 (1 bit) chip cpbk y sign Chip Public key sign of Y
  • 0 : Chip public key Y is positive
  • 1 : Chip Public key Y is negative
1-1 (1 bit) stkeyprov ecies ok Status of ECIES ST key provisionning when it was attempted.
  • 0: ECIES ST key provisionning last attempt was failed
  • 1: ECIES ST key provisionning last attempt was successfull
2-2 (1 bit) stkeyprov hwkey done ST HW Key provisionning done
  • 0: HWKEY not provisionned
  • 1: HWKEY was provisioned
10-3 (8 bits) security counter security counter involved in productID for chip certificate verification by HSM-OEM in RSSe_prov context
14-11 (4 bits) st pub key id ST ECDSA Public Key ID (ST Key Instance fuse part) involved in productID for chip certificate verification by HSM-OEM in RSSe_prov context
22-15 (8 bits) rssefw active signing key 8 possible ST public keys (ST key revocation feature for RSSe_FW authentication)
  • [1-0xFF] -> [1-8] : Value of monotonic counter is X where X is position of the most significant bit at 1.
28-23 (6 bits) nb added stsecrets Number of additional ST secrets words provisionned
  • 0 : no additional ST secrets
  • [1-63] : nb of OTP words located in upper area [360-nb_added_stsecrets..359] that were provisionned with ST secrets.
31-29 (3 bits) Reserved
11

BOOTROM_CONFIG_2

0-0 (1 bit) Reserved
1-1 (1 bit) sdmmc1 not default af SDMMC1 default Afmux usage
  • 0 : SDMMC1 uses default hard coded AFmux.
  • 1 : SDMMC1 uses AFmux defined in OTP.
2-2 (1 bit) sdmmc2 not default af SDMMC2 default Afmux usage
  • 0 : SDMMC2 uses default hard coded AFmux.
  • 1 : SDMMC2 uses AFmux defined in OTP.
4-3 (2 bits) Reserved
5-5 (1 bit) no cpu pll CPU PLL usage
  • 0 : PLLs for CPU/AXI are enable for cold boot.
  • 1 : PLLs for CPU/AXI are not enable for cold boot
9-6 (4 bits) Reserved
14-10 (5 bits) disable uart Disable UART instances
  • 0b00001: disable USART2
  • 0b00010: disable UART5
  • 0b00100: disable UART6
15-15 (1 bit) no data cache Data cache usage
  • 0: Data cache is used by bootrom.
  • 1: Data cache is not used by bootrom.
23-16 (8 bits) boot source disable Each bit disable a boot source.

Default to UART if all disabled.

  • 0b00000001: disable FMC boot source.
  • 0b00000010: disable QSPI NOR boot source.
  • 0b00000100: disable eMMC boot source.
  • 0b00001000: disable SD boot source.
  • 0b00010000: disable UART boot source.
  • 0b00100000: disable USB boot source.
  • 0b01000000: disable QSPI NAND boot source.
  • 0b10000000: disable QSPI HyperFlash boot source.
25-24 (2 bits) bootpins layout sel Bootpins layout selection
  • [0-3]: Select one among the three possible bootpins layout
29-26 (4 bits) boot source sel Boot source selection
  • [0-15]: Select one among the 16 possible boot source of the selected bootpins layout
30-30 (1 bit) dont boot on cfm tamper Disable boot on confirmed tamper feature
  • 0: boot on confirmed tamper
  • 1: do not boot on confirmed tamper
31-31 (1 bit) Reserved
12

BOOTROM_CONFIG_3

BOOTROM / FSBL-A version monotonic counter
13

BOOTROM_CONFIG_4

7-0 (8 bits) Reserved
11-8 (4 bits) RNG configuration 3 STM32MP21 Reference Manuals (RNG CR register)
12 (1 bit) NIST custom STM32MP21 Reference Manuals (RNG CR register)
15-13 (3 bits) RNG configuration 2 STM32MP21 Reference Manuals (RNG CR register)
19-16 (4 bits) Clock divider factor STM32MP21 Reference Manuals (RNG CR register)
27-20 (8 bits) RNG configuration 2 STM32MP21 Reference Manuals (RNG CR register)
31-28 (4 bits) Reserved
14

BOOTROM_CONFIG_5

17 -0 (18 bits) RNG health test control configuration (HTCR0) STM32MP21 Reference Manuals (RNG HTCR0 register)
31-18 (14 bits) Reserved
15

BOOTROM_CONFIG_6

8-0 (9 bits) RNG noise source control STM32MP21 Reference Manuals (RNG NSCR register)
31-10 (22 bits) Reserved
16

BOOTROM_CONFIG_7

0-0 (1 bit) disable traces Disable bootROM traces
  • 0: bootROM traces are enabled
  • 1: bootROM traces are disabled
1-1 (1 bit) disable hse freq detect Disable HSE frequency autodetection
  • 0: HSE frequency autodetection is enabled
  • 1: HSE frequency autodetection is disabled
2-2 (1 bit) disable hse bypass detect Disable HSE bypass detection
  • 0: HSE bypass detection is enabled
  • 1: HSE bypass detection is disabled
3-3 (1 bit) disable blocking failure traces Disable traces done by blocking failure process
  • 0: blocking failure traces are enabled
  • 1: blocking failure traces are disabled
4-4 (1 bit) a35 mode Select a35 architecture mode
  • 0: FSBL-A is AArch64
  • 1: FSBL-A is AArch32
5-5 (1 bit) fmc force sw reset FMC is used by CA35 to connect a NAND and by CM33 to connect a NOR or PSRAM
  • 0: Use RCC to reset FMC
  • 1: Use sw procedure to reset FMC witout impacting CM33
6-6 (1 bit) emergency debug req Emergency debug request
  • 0: emergency debug is not requested
  • 1: emergency debug is requested
7-7 (1 bit) emmc 128k boot partition Support eMMC with 128Kb boot partition
  • 0: bootROM does not support eMMC with 128Kb boot partition.
  • 1: bootROM supports eMMC with 128Kb boot partition.
8-8 (1 bit) fsbl decrypt prio FSBL decryption priority (speed or security)
  • 0: use CRYP (fast but no DPA protection)
  • 1: use SAES (slow but DPA protection))
9-9 (1 bit) Reserved
10-10 (1 bit) Reserved
13-11 (3 bits) HSE value HSE value
  • 0b000: HSE value is autodetected among 16, 20, 24, 28, 32, 36, 40, 48MHz
  • 0b001: HSE = 24MHz
  • 0b010: HSE = 25MHz
  • 0b011: HSE = 26MHz
  • 0b100 (19_2 Mhz): HSE = 19.2MHz
  • 0b101: HSE = 40MHz
  • 0b110: HSE = 48MHz
  • 0b111: Reserved
14-14 (1 bit) snand need plane select 1 NAND parameters bank1 - Serial NAND plane selection
  • 0: Serial NAND plane select is not needed.
  • 1: Serial NAND plane select is need
17-15 (3 bits) pnand number of ecc bits 1 NAND parameters bank1 - Number of Error Correction Code (ECC) bits
  • 0: ECC unset.
  • 1: ECC 1bit (Hamming).
  • 2: ECC 4bit (BCH4).
  • 3: ECC 8bit (BCH8).
  • 4: on-die ECC.
18-18 (1 bit) pnand bus width 1 NAND parameters bank1 - Parallel NAND data witdh
  • 0: data width is 8 bits
  • 1: data width is 16 bits
26-19 (8 bits) nand nb of blocks 1 NAND parameters bank1 - Number of blocks in unit of 256 blocks
  • [1-256]: Number of block = 256 * value
28-27 (2 bits) nand block size 1 NAND parameters bank1 - Block size in number of pages
  • 0: 64 pages per block
  • 1: 128 pages per block
  • 2: 256 pages per block
30-29 (2 bits) nand page size 1 NAND parameters bank1 - Page size
  • 0: 2Kbytes
  • 1: 4Kbytes
  • 2: 8Kbytes
31-31 (1 bit) pnand param stored in otp Parallel NAND parameters stored in OTP bank1 or bank2
  • 0: BootROM uses ONFI parameter table to get parallel nand parameters.
  • 1: parallel nand parameters are defined in bank1 or bank2, depending on nand_config_distribution value.
17

BOOTROM_CONFIG_8

7-0 (8 bits) oem active signing key1 Eight possible OEM public keys (OEM key revocation feature for OEM-FSBL authentication)
  • [1-256] -> [1-8] : Value of monotonic counter is X where X is position of the most significant bit at 1.
8-8 (1 bit) oem keys2 enable Enable second ECDSA OEM key set for FSBL-M authentication and decryption[fsblm-keys 1]
  • 0: keys2 are not used; keys1 are used for both FSBLA and FSBLM
  • 1: keys2 are enabled; keys1 are used for FSBLA; keys2 are used for FSBLM
31-16 (16 bits) Reserved
18

BOOTROM_CONFIG_9

3-0 (4 bits) secure boot Enable enforced secure boot
  • 0: Chip is in CLOSED_UNLOCKED state. Secure boot is not enforced (FSBL authentication is not mandatory).
  • [1-15]: Chip is in CLOSED_LOCKED state. Secure boot is enforced (FSBL authentication is mandatory)
Warning
Setting only this bit is not enough to close the product and will brick it.

Please refer to device life cycle for the appropriate sequence.

7-4 (4 bits) prov done RSSE provisioning done
  • 0: RSSE provisioning is not done
  • [1-15]: RSSE provisioning is done
11-8 (4 bits) debug lock Lock debug enabling until next reset when chip is CLOSED-LOCKED
  • 0: Don't lock debug enabling
  • [1-15]: Lock debug enabling
15-12 (4 bits) otp prov done RSSe OTP provisioning done
  • 0: RSSe OTP provisioning is not done
  • [1-15]: RSSe OTP provisioning part done, used to manage RSSe extension issue
21-16 (6 bits) Reserved
22-22 (1 bit) ns epoch enable Enable non secure EPOCH use
  • 0: bootROM does not manage NS_EPOCH. BOOTROM_NS_EPOCH monotonic counter fuse bits are free for other use.
  • 1: bootROM manages NS_EPOCH. bootROM uses BOOTROM_NS_EPOCH monotonic counter fuse bits.
26-23 (4 bits) fingerprint enable Enable fingerprint feature
  • 0: fingerprint feature is disabled
  • 1: fingerprint feature is enabled
31-27 (5 bits) free for future use
19

BOOTROM_CONFIG_10

31-0 (32 bits) fsblm_monotonic BOOTROM / OEM-FSBLM version monotonic counter
20

BOOTROM_CONFIG_11

0-0 (1 bit) nand config distribution NAND configurations distribution
  • 0: pNAND config in nand*_2 fields / sNAND config in nand*_1 fields
  • 1: pNAND config in nand*_1 fields / sNAND config in nand*_2 fields
1-1 (1 bit) snand need plane select 2 idem BOOTROM_CONFIG_7.snand_need_plane_select_1
4-2 (3 bits) pnand number of ecc bits 2 idem BOOTROM_CONFIG_7.pnand_number_of_ecc_bits_1
5-5 (1 bit) pnand bus width 2 idem BOOTROM_CONFIG_7.pnand_bus_width_1
13-6 (8 bits) nand nb of blocks 2 idem BOOTROM_CONFIG_7.nand_nb_of_blocks_1
15-14 (2 bits) nand block size 2 idem BOOTROM_CONFIG_7.nand_block_size_1
17-16 (2 bits) nand page size 2 idem BOOTROM_CONFIG_7.nand_page_size_1
18-18 (1 bit) hyperflash 3V3 device Is HyperFlash a 3.3V device
  • 0: hyperflash is not a 3.3V device
  • 1: hyperflash is a 3.3V device
21-19 (3 bits) rng htcr value RNG HTCR value
  • 0: 0xA2B3
  • 1: 0xA2B3
  • 2: 0xAA74
  • 3: 0xA6BA
  • 4: 0x9AAE
  • 5: 0x72AC (corresponds to the default value of IP after reset)
  • 6: 0xAAC7 value set by engineering in OTP
  • 7: 0xA2B3 only other possible value for OTP after engineering set above "6: 0xAAC7" value
22-22 (1 bit) ospi io speed ovrw OSPI IO speed overwrite enable
  • 0: OSPI io speed is not overwritten by otp configuration
  • 1: OSPI io speed is overwritten by otp configuration
24-23 (2 bits) ospi io speed clk nclk OSPI IO speed of clk nclk IO
  • 0b00: low speed.
  • 0b01: medium speed.
  • 0b10: high speed
  • 0b11: very high speed
25-24 (2 bits) ospi io speed data cs OSPI IO speed of CS IO
  • 0b00: low speed.
  • 0b01: medium speed.
  • 0b10: high speed
  • 0b11: very high speed
31-26 (6 bits) Reserved
21

BOOTROM_CONFIG_12

31-0 (32 bits) rsse_monotonic BOOTROM / RSSe FW version monotonic counter
22

BOOTROM_CONFIG_13

7-0 (8 bits) oem active signing key2 Eight possible OEM public keys (OEM key revocation feature for OEM-FSBL authentication)
  • [1-256] -> [1-8]: Value of monotonic counter is X where X is position of the most significant bit at 1.
31-8 (24 bits) Reserved
23 H32ENCPRVKEY BOOTROM / Hash of E1CPvK
24 31-0 (32 bits) BOOTROM TZ EPOCH0 Secure side Epoch counter
25 31-0 (32 bits) BOOTROM TZ EPOCH1
26 31-0 (32 bits) BOOTROM TZ EPOCH2
27 31-0 (32 bits) BOOTROM TZ EPOCH3
28 31-0 (32 bits) BOOTROM TZ EPOCH4
29 31-0 (32 bits) BOOTROM TZ EPOCH5
30 31-0 (32 bits) BOOTROM TZ EPOCH6
31 31-0 (32 bits) BOOTROM TZ EPOCH7
32 31-0 (32 bits) BOOTROM NS EPOCH0 Non Secure Epoch counter
33 31-0 (32 bits) BOOTROM NS EPOCH1
34 31-0 (32 bits) BOOTROM NS EPOCH2
35 31-0 (32 bits) BOOTROM NS EPOCH3
36 31-0 (32 bits) BOOTROM NS EPOCH4
37 31-0 (32 bits) BOOTROM NS EPOCH5
38 31-0 (32 bits) BOOTROM NS EPOCH6
39 31-0 (32 bits) BOOTROM NS EPOCH7
40 to 100 Available for customer
101 ADAC_SOC_MASK Control the maximum debug level possible via ADAC
102 ID STM32MP21 Reference Manuals
103 CRC_HSM
104 CAL1 STM32MP21 Reference Manuals
105 Reserved
106 CAL3 STM32MP21 Reference Manuals
107 Reserved
108 CAL5 STM32MP21 Reference Manuals
109 Reserved
110 CAL7 STM32MP21 Reference Manuals
111 Reserved
112 ENGI1 Engineering
113 ENGI2 Engineering
114 ENGI3 Engineering
115 ENGI4 Engineering
116 ENGI5 Engineering
117 ENGI6 Engineering
118 ENGI7 Engineering
119 ENGI8 Engineering
120 ATRIM1 STM32MP21 Reference Manuals
121 ATRIM2 STM32MP21 Reference Manuals
122 ATRIM3 STM32MP21 Reference Manuals
123 ATRIM4 STM32MP21 Reference Manuals
124 HCONF1 STM32MP21 Reference Manuals
125 MREPAIR1
126 MREPAIR2
127 MREPAIR3

1.2. Middle OTP region[edit | edit source]

For both TD flavor (A35-TD or M33-TD)
OTP word Name Description
128 STM32CERTIF0 STM32 chip certificate (public key)[key-formats 1]
129 STM32CERTIF1
130 STM32CERTIF2
131 STM32CERTIF3
132 STM32CERTIF4
133 STM32CERTIF5
134 STM32CERTIF6
135 STM32CERTIF7
136 STM32CERTIF8
137 STM32CERTIF9
138 STM32CERTIF10
139 STM32CERTIF11
140 STM32CERTIF12
141 STM32CERTIF13
142 STM32CERTIF14
143 STM32CERTIF15
144 STM32CERTIF16
145 STM32CERTIF17
146 STM32CERTIF18
147 STM32CERTIF19
148 STM32CERTIF20
149 STM32CERTIF21
150 STM32CERTIF22
151 STM32CERTIF23
152 OEM KEY1 ROT0 OEM Key1 Root of Trust Hash[key-formats 1][fsblm-keys 1]
153 OEM KEY1 ROT1
154 OEM KEY1 ROT2
155 OEM KEY1 ROT3
156 OEM KEY1 ROT4
157 OEM KEY1 ROT5
158 OEM KEY1 ROT6
159 OEM KEY1 ROT7
160 OEM KEY2 ROT0 OEM Key2 Root of Trust Hash[key-formats 1][fsblm-keys 1]
161 OEM KEY2 ROT1
162 OEM KEY2 ROT2
163 OEM KEY2 ROT3
164 OEM KEY2 ROT4
165 OEM KEY2 ROT5
166 OEM KEY2 ROT6
167 OEM KEY2 ROT7
168 STM32PUBKEY0 STM32 chip public key[key-formats 1]
169 STM32PUBKEY1
170 STM32PUBKEY2
171 STM32PUBKEY3
172 STM32PUBKEY4
173 STM32PUBKEY5
174 STM32PUBKEY6
175 STM32PUBKEY7
176 STM32PUBKEY8
177 STM32PUBKEY9
178 STM32PUBKEY10
179 STM32PUBKEY11


A35-TD flavor M33-TD flavor
OTP word Name Description Name Description
180* RPROC-FW-PKH_0 Hash of the Public Key for remote processor firmware[key-formats 2] Available for customer
181* RPROC-FW-PKH_1 Available for customer
182* RPROC-FW-PKH_2 Available for customer
183* RPROC-FW-PKH_3 Available for customer
184* RPROC-FW-PKH_4 Available for customer
185* RPROC-FW-PKH_5 Available for customer
186* RPROC-FW-PKH_6 Available for customer
187* RPROC-FW-PKH_7 Available for customer
188* Available for customer FSBLM-M33-FW-PKH_0 Hash of the Public Key for M33TDCID M33 Firmware[key-formats 2]
189* Available for customer FSBLM-M33-FW-PKH_1
190* Available for customer FSBLM-M33-FW-PKH_2
191* Available for customer FSBLM-M33-FW-PKH_3
192* Available for customer FSBLM-M33-FW-PKH_4
193* Available for customer FSBLM-M33-FW-PKH_5
194* Available for customer FSBLM-M33-FW-PKH_6
195* Available for customer FSBLM-M33-FW-PKH_7
196* Available for customer FSBLM-DDR-FW-PKH_0 Hash of the Public Key for M33TDCID DDR Firmware[key-formats 2]
197* Available for customer FSBLM-DDR-FW-PKH_1
198* Available for customer FSBLM-DDR-FW-PKH_2
199* Available for customer FSBLM-DDR-FW-PKH_3
200* Available for customer FSBLM-DDR-FW-PKH_4
201* Available for customer FSBLM-DDR-FW-PKH_5
202* Available for customer FSBLM-DDR-FW-PKH_6
203* Available for customer FSBLM-DDR-FW-PKH_7
204* Available for customer FSBLM-A35-FW-PKH_0 Hash of the Public Key for M33TDCID A35 bare metal Firmware[key-formats 2]
205* Available for customer FSBLM-A35-FW-PKH_1
206* Available for customer FSBLM-A35-FW-PKH_2
207* Available for customer FSBLM-A35-FW-PKH_3
208* Available for customer FSBLM-A35-FW-PKH_4
209* Available for customer FSBLM-A35-FW-PKH_5
210* Available for customer FSBLM-A35-FW-PKH_6
211* Available for customer FSBLM-A35-FW-PKH_7
212 to 237 Available for customer

*For OTP word from 180 to 211 : In Reference manual, those OTP words are available for customer but they have been used in OpenSTLinux distribution.


For both TD flavor (A35-TD or M33-TD)
OTP word Name Description
238* OEM ADAC ROTPK HASH0 OEM ADAC key Root of Trust Hash
239* OEM ADAC ROTPK HASH1
240* OEM ADAC ROTPK HASH2
241* OEM ADAC ROTPK HASH3
242* OEM ADAC ROTPK HASH4
243* OEM ADAC ROTPK HASH5
244* OEM ADAC ROTPK HASH6
245* OEM ADAC ROTPK HASH7
246* ST_BOARD_ID Identifier for ST boards (or available to customer for their own board)
247* MAC_ADDR_0 Mac address [coding 1]
248* MAC_ADDR_1
249* MAC_ADDR_2
250* MAC_ADDR_3
251* MAC_ADDR_4
252* MAC_ADDR_5
253 MAC_ADDR_6
254* MAC_ADDR_7
255 ST_RSSE_EDMK_DERIV_CSTE_FUSE (SoC dependent) ST Encryption Decryption Master Key Derivation constant

*For OTP word from 238 to 254 : In Reference manual, those OTP words are available for customer but they have been used in OpenSTLinux distribution.

1.3. Upper OTP region[edit | edit source]

For both TD flavor (A35-TD or M33-TD)
OTP word Name Description
256* OTP_RMA_LOCK_PSWD0 RMA lock password (128 bit)
257* OTP_RMA_LOCK_PSWD1
258* OTP_RMA_LOCK_PSWD2
259* OTP_RMA_LOCK_PSWD3
260** FIP-EDMK0 FIP encryption decryption master key (256-bit)
261** FIP-EDMK1
262** FIP-EDMK2
263** FIP-EDMK3
264** FIP-EDMK4
265** FIP-EDMK5
266** FIP-EDMK6
267** FIP-EDMK7
268 to 323 OEM Secrets available for customer

* For OTP word from 256 to 259 : SoC dependent, to be filled by customer. They are protected by the hardware so they cannot be read back. These OTPs must be programmed locked after provisioning.
**For OTP word from 260 to 267 : In Reference manual, those OTP words are available for customer but they have been used in OpenSTLinux distribution.


A35-TD flavor M33-TD flavor
OTP word Name Description Name Description
324* Available for customer TFM_PRVK_ECIES_KEY0 BL2 Asymmetric private key for ECIES encryption[key-formats 2]
325* Available for customer TFM_PRVK_ECIES_KEY1
326* Available for customer TFM_PRVK_ECIES_KEY2
327* Available for customer TFM_PRVK_ECIES_KEY3
328* Available for customer TFM_PRVK_ECIES_KEY4
329* Available for customer TFM_PRVK_ECIES_KEY5
330* Available for customer TFM_PRVK_ECIES_KEY6
331* Available for customer TFM_PRVK_ECIES_KEY7
332* RPROC-FW-ENC-KEY0 Encryption/Decryption Key for remote processor firmware Available for customer
333* RPROC-FW-ENC-KEY1 Available for customer
334* RPROC-FW-ENC-KEY2 Available for customer
335* RPROC-FW-ENC-KEY3 Available for customer
336* RPROC-FW-ENC-KEY4 Available for customer
337* RPROC-FW-ENC-KEY5 Available for customer
338* RPROC-FW-ENC-KEY6 Available for customer
339* RPROC-FW-ENC-KEY7 Available for customer

*For OTP word from 324 to 339 : In Reference manual, those OTP words are available for customer but they have been used in OpenSTLinux distribution.


For both TD flavor (A35-TD or M33-TD)
OTP word Name Description
340* TF-M IAK0 Initial attestation 256-bit key (Symmetric or Asymmetric key)
341* TF-M IAK1
342* TF-M IAK2
343* TF-M IAK3
344* TF-M IAK4
345* TF-M IAK5
346* TF-M IAK6
347* TF-M IAK7
348** OEM KEY2 EDMK0 OEM master key used to derive FSBLM decryption key[key-formats 1][fsblm-keys 1]
349** OEM KEY2 EDMK1
350** OEM KEY2 EDMK2
351** OEM KEY2 EDMK3
352** OEM KEY2 EDMK4
353** OEM KEY2 EDMK5
354** OEM KEY2 EDMK6
355** OEM KEY2 EDMK7
356** OEM KEY1 EDMK0 OEM master key used to derive FSBLA or M decryption key[key-formats 1]
357** OEM KEY1 EDMK1
358** OEM KEY1 EDMK2
359** OEM KEY1 EDMK3
360** OEM KEY1 EDMK4
361** OEM KEY1 EDMK5
362** OEM KEY1 EDMK6
363** OEM KEY1 EDMK7
364 STM32PRVKEY0 STM32 ECC chip private key
365 STM32PRVKEY1
366 STM32PRVKEY2
367 STM32PRVKEY3
368 STM32PRVKEY4
369 STM32PRVKEY5
370 STM32PRVKEY6
371 STM32PRVKEY7
372 STM32PRVKEY8
373 STM32PRVKEY9
374 STM32PRVKEY10
375 STM32PRVKEY11
376 HWKEY0 Secret hardware unique key
377 HWKEY1
378 HWKEY2
379 HWKEY3
380 HWKEY4
381 HWKEY5
382 HWKEY6
383 HWKEY7

*For OTP word from 340 to 347 : In Reference manual, those OTP words are available for customer but they have been used in OpenSTLinux distribution.
**For OTP word from 348 to 363 : reserved for BootRom, to be filled by customer. They are protected by the hardware so they cannot be read back. These OTPs must be programmed locked after provisioning.

2. References[edit | edit source]

2.1. Key storage in OTP[edit | edit source]

Keys are represented as a string of byte to be stored in consecutive OTP words.

For example, a 64-bit key (0xAABBCCDDEEFF5566) is stored into two consecutive OTP words KEY0 and KEY1.

A key is stored in OTP words using one of the following formats:

  1. ↑ 1.0 1.1 1.2 1.3 1.4 1.5
    KEY0 = 0xAABBCCDD, KEY1 = 0xEEFF5566
  2. ↑ 2.0 2.1 2.2 2.3 2.4
    KEY0 = 0xDDCCBBAA, KEY1 = 0x6655FFEE

2.2. MAC address[edit | edit source]

  1. ↑
    Mac addresses are stored as octets list using the following coding convention:
    • OTP 247: mac_addr_1[4 first octets]
    • OTP 248: mac_addr_2[2 first octets] | mac_addr_1[2 last octets]
    • OTP 249: mac_addr_2[4 last octets]
    • OTP 250: mac_addr_3[4 first octets]
    • ...
    Example: 247 = 0xE37AE710 / 248 = 0xE710F495 / 249 = 0xF595E37A
    • mac_addr1 : 10:E7:7A:E3:95:F4
    • mac_addr2 : 10:E7:7A:E3:95:F5
    • ...
    Each MAC address is associated in U-Boot to an ethernet device with alias in device tree: ethernet0, ethernet1, ...
    On STM32MP257F-EV1 Evaluation board the ETH2 use the first mac address (ethernet0 = &eth2), ETH1 use the second mac address (ethernet1 = &eth1).
    On STM32MP257F-DK Discovery kit the ETH1 use the first mac address (ethernet0 = &eth1).
    On the default mapping the MAC 3, 4 and 5 are assigned to TSN switch (depending on product version).
    A unused MAC address (for example when TSN is not used) should be set to FF:FF:FF:FF:FF:FF, to avoids the trace "invalid MAC address" in U-Boot.

2.3. FSBL-M keys[edit | edit source]

  1. ↑ 1.0 1.1 1.2 1.3
    By defaultSTM32MP21x lines  use OEM_KEY1_ROT and OEM_KEY1_EDMK for FSBLA and FSBLM. To use the dedicated FSBLM keys (OEM_KEY2_ROT and OEM_KEY2_EDMK) you must program bit 8 from OTP17.