Last edited 11 months ago

How to import SW4STM32 project in STM32CubeIDE

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

Important
This article has been written with the example of STM32MP1 series but it is applicable to any lines present in applicability field displayed on the top of this article

1. Import an SW4STM32 project with an ioc file[edit | edit source]

If the project already contains an ioc file, the easiest way to import the project into a working STM32CubeIDE environment is to copy it and open the copy through STM32CubeMX stand alone, then, in the Project Manager, change the Toolchain / IDE to STM32CubeIDE and regenerate the project.

After the project is regenerated, go to [File]>[Import...] and choose to import it as an Existing projects into Workspace.

Import an existing project with an ioc file

Then copy the code inside the different /* USER CODE BEGIN */ blocks that exist in the project into the new STM32CubeIDE environment.

2. Import an SW4STM32 project without an ioc file[edit | edit source]

To make sure that the project gets a hierarchical structure, the recommended way is to go to [File]>[New]>[STM32 Project] as shown below.

Menu option for a new STM32 project

Select the device for the project being imported and click on [Next >].

When setting up the project as shown below, make sure the Targeted Project Type is set to Empty and click on [Finish].

Error creating thumbnail: Unable to save thumbnail to destination
Project setup with targeted project type selected as empty.

After the empty hierarchical project is generated:
1- Go to [File]>[Import...]

Import ac6 System Workbench for STM32 Project


2- Import the SW4STM32 project as Import ac6 System Workbench for STM32 Project
3- Copy and paste the project content into the sub-project of the empty project by means of STM32CubeIDE project explorer as shown below

Copy project content to empty sub-project.
Information
It is not recommended to import the .cproject, .project or .settings files.

It is important to remember to configure also the same build settings used previously while the project was in the SW4STM32 environment. If the project contains linked resources, they must be updated to point to the correct resources in the file system. This process is necessary because importing a project made for SW4STM32 without any special treatment and without an ioc file results in a flat project structure in STM32CubeIDE.