Last edited 3 months ago

STM32MP23-25 ecosystem errata sheet

Applicable for STM32MP25x lines


1. Article purpose[edit | edit source]

The STM32MP23xx/25xx device errata sheet[1] lists the different device limitations and explains the corresponding workarounds (software and/or hardware) if any.

The objective of this article is to explain which of the workarounds, described in this errata sheet, are applicable and implemented in ecosystem release v6.2.0 .
This article lists

  • errata to be workaround by the customers,
  • errata workaround implemented in STM32MPU Ecosystem releases,
  • and errata not applicable in STM32MPU Ecosystem releases.

Errata, present in STM32MP23xx/25xx device errata sheet[1] and not listed in this article, have no workaround implemented in STM32MPU Ecosystem releases.

2. Legend[edit | edit source]

The section column refers to the number of the erratum chapter in the errata sheet document.

Rev.Y columns , present in the tables below, refer to the availability and status of a given errata workaround for the described erratum in errata sheet document:

  • A = workaround available
  • P = partial workaround available
  • N = no workaround available
  • “-” = limitation absent

OpenSTLinux and CubeMP1 columns , present in the tables below, refer to the availability of a workaround for a given STM32MP13 ecosystem release:

  • U = workaround to implement by User
  • I = workaround Implemented
  • NA= Errata Not Applicable in ST software release

Wave your mouse over a status in the table to display the corresponding legend.

3. Workarounds to implement by customer[edit | edit source]

Function Section Limitation Rev.Y Rev.X Comment
SYSTEM 2.3.23 Standby1/2 exit stuck in Secured_Locked state in A35-TD flavor A - U Restriction for low-power mode in A35-TD flavor : not supported on secure chips for old revisions.

OpenSTLinux does not provide a workaround (no revision and secure-chip detection). The limitation must be handled in the customer board TF‑A device tree by declaring the supported low-power modes.

2.3.31 CPU1 core cannot be reset by CPU0 in 64-bit development boot

mode

A - NA U Warning: The errata is incorrect: the issue is not CPU0 vs CPU1 but core0 vs core1 (both are named CPU1 in the reference manual).

Not applicable to OpenSTLinux, as development boot is not used.
For STM32CubeMP2, STM32CubeIDE works only on a single CPU (not SMP), so this is also not applicable.
Users, developing on Cortex‑A35 SMP (CPU1) in development boot, must follow the workaround described in the errata: halt core1, set the PC to WFI, and then resume execution.

FMC 2.4.1 NOR flash memory/PSRAM incorrect bus turnaround timing A A U OpenSTLinux distribution: Delays to apply by customer at device tree level.
OCTOSPI 2.5.6 Indirect write mode limited to 256 Mbytes N N U OpenSTLinux distribution: Memory with a density greater than 256 MB should be avoided.
I3C 2.16.2 I3C controller: SCL clock is not stalled during address ACK/NACK phase following a frame start, when enabled through I3C_TIMINGR2 register A A U OpenSTLinux distribution: STALLA is not set in current I3C implementation. If it is required to be set because of a slow target, workaround have to be implemented by customer.
2.16.4 I3C controller: no timestamp on IBI acknowledge when timing control is used in Asynchronous mode 0 A A U OpenSTLinux distribution: SETXTIME CCC defined but not used yet in Linux OS. This prevents to operate in asynchronous mode.
ETHSW 2.23.3 TSN switch controller tags management traffic when the PVID is configured differently on internal and external ports P P U OpenSTLinux distribution: workaround not implemented in the current TTTech TSN switch driver, because the driver allows the PVID to be configured independently on each port and no mechanism was found to enforce identical PVID settings across internal and external switch ports. The workaround must be ensured by the user or the system integrator when configuring the network. 
2.23.4 TSN switch controller tags management traffic when the PVID is configured differently on internal and external ports P P U OpenSTLinux distribution: The workaround not implemented in the current TTTech TSN switch driver, because the express/preemptable selection is configured per queue through the frame preemption status table, and no mechanism was found to enforce that express and preemptable priorities are mapped to different queues.

4. Workarounds implemented in STM32MP23-25 ecosystem releases[edit | edit source]

Function Section Limitation Rev.Y Rev.X Comment
SYSTEM 2.3.5 Compartment filtering of PWR_CR11 and PWR_CR12 registers is not functional A A I Workaround implemented in OP-TEE and TF-M: change RIF configuration before register access
2.3.6 STGEN is reset when D1 domain is in DStandby low power mode N N I TF‑BL31: restart STGEN on exit from low-power mode, as STGEN is reset in D1 DStandby mode
2.3.19 STOP and Standby entry failed when DDR is in shared mode A A I Done for A35-TD, but not as described in the errata: DDR shared mode is deactivated before executing the low-power sequence in TF‑A BL31
2.3.24 System resources configuration modification by ROM code during D1 DStandby exit A - I A35-TD flavor : OpenSTLinux keeps the SYSRAM content, and TF‑A BL31 does not allow the behavior described in the errata ( LEGACY_BEN = 1 and Stop2 exit point saved in a BKP register ).

M33-TD flavor : Workaround implemented in TF‑M and RIF device tree: the default RIF configuration in OpenSTLinux follows these rules, and IAC generated by the ROM code are discarded.

2.3.26 M0+ hang risk on low-power modes Entry (Standby1, LPLV-Stop1 and LPLV-Stop2) A A PI For OpenSTLinux, partially implemented as only M0 demo example
2.3.27 M0+ hang risk on low-power modes Exit (Standby1, LPLV-Stop1 and LPLV-Stop2) A A PI For OpenSTLinux, partially implemented as only M0 demo example
2.3.28 I/O compensation could alter duty-cycle of high-frequency output signal A A I For OpenSTLinux, IOCOMP is set to static values in TF‑A, OP‑TEE, and TF‑M
2.3.29 Incorrect instance value in boot ROM for eMMC™single device mode in M33-TD flavor A - I Workaround available in TF-A for Rev.Y, issue fixed on Rev.X
OCTOSPI 2.5.4 Deadlock or write-data corruption after spurious write to a misaligned

address in OCTOSPI_AR register

N N I OpenSTLinux distribution: Misaligned addresses are handled at driver side when DQSE is set.
2.5.9 Setting the ABORT bit does not generate an error on the AHB bus for

undefined-length incremental burst transfers

P P I OpenSTLinux distribution: The software waits for the end of the transfer before setting the ABORT bit.
LTDC 2.10.1 Ongoing AXI write never completes if disabling LTDC A A I OpenSTLinux distribution: Driver implemented to go through this problem.
2.10.3 Rotation for wide landscape display can causes artifacts N N I OpenSTLinux distribution: Driver implemented to go through this problem.
2.10.4 Layer 1 cannot read YUV420 multibuffer data N N I OpenSTLinux distribution: Driver implemented to go through this problem.
VDEC 2.12.1 VDEC hardware self-reset after internal timeout is unstable A A I OpenSTLinux distribution: As a workaround, disable hardware timeout feature and

replace it by a software timeout. This is implemented by checking if G1 is idle before each run, if it is not the case hardware is aborted: this will clean all the bus left transactions..

I2C 2.15.1 Wrong data sampling when data setup time (tSU;DAT) is shorter than one

I2C kernel clock period

P P I Workaround implemented in device tree with a clock tree that configures the I2C kernel clock source to a frequency higher than 20 MHz.
I3C 2.16.1 I3C controller: unexpected read data bytes during a legacy I2C read A A I OpenSTLinux distribution: STALLT is not set in current I3C implementation. If it is required to be set because of a slow target, workaround is IMPLEMENTED: all I3C/I2C transfers implement a software timeout to inform that neither FCF nor ERRF was raised and FIFOs are flushed.
2.16.3 I3C controller: unexpected first frame with a 0x7F address when the I3C

peripheral is enabled

A A I OpenSTLinux distribution: Workaround implemented in device tree with an 'init' pinctrl state with pull-up on SDA, until I3C controller is enabled.
ETH 2.22.2 ETH1 RMII mode could have CRC errors A - I OpenSTLinux distribution: This issue is solved on Rev X but if RevY, workaround is available inside software

5. Workarounds not applicable in STM32MP23-25 ecosystem releases[edit | edit source]

Function Section Limitation Rev.Y Rev.X Comment
SYSTEM 2.1.6 ATS12NSOPR instruction might incorrectly translate when the HCR.TGE bit is set A A NA Not applicable in OpenSTLinux, as boot is EL3 AArch64 only, while the errata requires EL3 AArch32.
SYSTEM 2.3.10 LSEDRV description is swapped N N NA This errata is for an old reference manual (as indicated).

The new reference manual is updated and OpenSTLinux uses the correct value (TF‑A / OP‑TEE / TF‑M). This is a documentation issue rather than a device limitation.

SYSTEM 2.3.13 Boot ROM writes in SYSRAM during LPLV-Stop2 wake-up A - NI Applicable for OpenSTLinux but no workaround and no impact (the modifed code is not called).

The TF-A BL31 firmware is loaded SYSRAM and use these addresses (0x0E000080- 0x0E000084 and bl31_entrypoint is located at 0xe000000) For LPLV-Stop2 exit, TF-ABL31 code have no workaround for this erata but this ROM code have today no impact.
The modified function bl31_entrypoint is no more used in OpenSTLinux for low power mode exit (bl31_warm_entrypoint at 0xe00010c is used) except for Standby exit, when SYSRAM content is lost and BL31 is reloaded.

SYSTEM 2.3.14 Instruction fetch access to PWR register leads to unwanted write A A NA No workaround needed, as PWR is not mapped as code area but as device in both CA35 MMU and CM33 MPU.
SYSTEM 2.3.17 ETHx kernel clock is gated if ETHxMACEN register bit is not set A A NA RCC, Ethernet (Linux® kernel, U‑Boot): ETHxMACEN bit is always enabled by default on all STM32 MPU platforms.
SYSTEM 2.3.30 Boot ROM hangs during D1-standby wake-up if e•MMC GPT format is used and FSBL size is less than 512 bytes in M33-TD flavor A - NA FSBL‑A is TF‑A BL2, loaded by the ROM code at the end of SYSRAM, so the stm32image size is greater than 512. The beginning of SYSRAM is reserved for TF‑A BL31, and the TF‑A BL2 stm32 file loaded by the ROM code is filled with 0x0, so its size is larger than the load offset in SYSRAM (0x16000).
SYSTEM 2.3.31 CPU1 core cannot be reset by CPU0 in 64-bit development boot mode A - NA Warning: The errata is incorrect: the issue is not CPU0 vs CPU1 but core0 vs core1 (both are named CPU1 in the reference manual).

Not applicable to OpenSTLinux, as development boot is not used. For STM32CubeMP2, STM32CubeIDE works only on a single CPU (not SMP), so this is also not applicable. Users developing on Cortex‑A35 SMP (CPU1) in development boot must follow the workaround described in the errata: halt core1, set the PC to WFI, and then resume execution.

FMC 2.4.2 Incorrect FMC_CLK clock period when CLKDIV value is changed on-the-fly in continuous clock mode A A NA OpenSTLinux distribution: CLKDIV cannot be changed on the fly, CLKDIV is configured when the driver is probed.
OCTOSPI 2.5.1 Memory-mapped write error response when DQS output is disabled P P NA OpenSTLinux distribution: memory-mapped write is not used by the software.
2.5.3 Memory wrap instruction not enabled when DQS is disabled N N NA OpenSTLinux distribution: memory wrap instruction is not used by the software.
2.5.5 Deadlock on consecutive out-of-range memory-mapped write operations P P NA OpenSTLinux distribution: memory-mapped write is not used by the software.
2.5.7 Read-modify-write operation does not clear the MSEL bit A A NA OpenSTLinux distribution: MSEL bit is never set by the software.
2.5.8 Automatic status-polling mode cannot be used with HyperFlash™ memories N N NA OpenSTLinux distribution: automatic status-polling mode is not used by the software with HyperFlash memories.
2.5.10 Read data corruption when a wrap transaction is followed by a linear read to the same MSB address N N NA OpenSTLinux distribution: memory wrap instruction is not used by the software.
2.5.11 Transactions are limited to 8 Mbytes in OctaRAM™ memories N N NA OpenSTLinux distribution: OctaRAM memories are not supported by the software (the driver is not available).
2.5.12 Variable latency is not supported when a refresh collision occurs during a write access to some OctaRAM™ memories P P NA OpenSTLinux distribution: OctaRAM memories are not supported by the software (the driver is not available).
2.5.13 In automatic status-polling and multiplexed modes, the controller does not request the port if less than two bytes are sent per cycle when

OCTOSPI_DLR is cleared

N N NI OpenSTLinux distribution: DLR should be set to 2 in case of automatic status-polling mode is used

Impact on kernel side only

OCTOSPIM 2.6.1 Certain quad memories may be reset during arbitration while in single-SPI mode A A NA OpenSTLinux distribution: not an issue from software side, as the frameworks (SPI NOR/SPI NAND) start by setting the memory in quad mode.
SDMMC 2.7.1 Command response and receive data end bits not checked N N NA OpenSTLinux distribution: not an issue from software side, as it is not visible by the software.
ADC 2.8.1 JEOS may be set before the last injected data are available in ADC_JDRx A A NA The injected mode is not supported in Linux ADC STM32MPx driver, These limitations have no impact on adc linux driver.
2.8.2 In combined regular simultaneous plus alternate trigger mode, stopping injected conversion may delay regular conversion A A NA The injected mode is not supported in Linux ADC STM32MPx driver, These limitations have no impact on adc linux driver.
2.8.3 When the ADC clock is derived from the AHB clock, the injected conversion latency is not respected if the injected trigger coincides with the stopping of the regular conversion A A NA The injected mode is not supported in Linux ADC STM32MPx driver, These limitations have no impact on adc linux driver.
2.8.4 The OVR flag is set if EOC is cleared by writing 1 to the EOC bit of ADC_ISR instead of reading the data register A A NA OpenSTLinux distribution: Drivers read the DR (data register) to clear the EOC (end of conversion)
LPTIM 2.13.2 ARRM and CMPM flags are not set when APB clock is slower than kernel clock A A NA OpenSTLinux distribution: drivers not affected as repetition counter not used
RTC 2.14.1 Alarm flag may be repeatedly set when the core is stopped in debug N N NA OpenOCD does not stop any device during debug so, even if one device send an interrupt (likethe RTC alarm), OpenOCD is able to continue.
I2C 2.15.2 Spurious bus error detection in controller mode A A NA In order to get real bus error notifications, this workaround is not implemented in the OpenSTLinux distribution.
I3C 2.16.6 I3C target: device can report target error 0 before dynamic address assignment A A NA OpenSTLinux distribution: I3C Target mode is not implemented
2.16.7 I3C target: nonparticipation in dynamic address procedure after NACKed hot-join request A A NA OpenSTLinux distribution: I3C Target mode is not implemented
2.16.8 I3C target: device fails to resynchronize with Sr or P condition in specific cases A A NA OpenSTLinux distribution: I3C Target mode is not implemented
USART 2.17.1 Wrong data received by SPI slave receiver in autonomous mode with CPOL = 1 A A NA OpenSTLinux distribution: SPI slave mode is not implemented.
2.17.2 Received data may be corrupted upon clearing the ABREN bit A A NA OpenSTLinux distribution: condition never reached in Linux OS thanks to the specific implementation (ABREN bit never cleared in USART_CR2 register).
2.17.3 Noise error flag set while ONEBIT is set N N NA OpenSTLinux distribution: not applicable as the Linux framework does not handle the noise error indication.
LPUART 2.18.1 Possible LPUART transmitter issue when using low BRR[15:0] value P P NA OpenSTLinux distribution: LPUART kernel clock and baudrate ratio prevent these cases. To reach these cases, LPUART kernel clock should be 3 or 4 times greater than the baudrate, but LPUART kernel clock sources are ≥ 16 MHz.
SPI 2.19.1 RDY output failure at high serial clock frequency N N NA The APB clock and SPI kernel clock ratio defined in the OpenSTLinux distribution prevent these cases from occurring. The APB clock is set to 200 MHz, and the SPI kernel clock is set to either 133 MHz or 200 MHz.
FDCAN 2.20.1 Desynchronization under specific condition with edge filtering enabled A A NA In driver CAN used for STM32MPU platforms, bit CCCR_EFBI is never set, so no issue possible.
2.20.2 Tx FIFO messages inverted under specific buffer usage and priority setting A A NA The workaround is inherently implemented in the Linux m_can driver, because on M_CAN IP v3.1+ (we are in v3.2 version on our hardware) transmission is configured and handled in TX FIFO mode only, so the erratum condition requiring mixed dedicated TX buffers and TX FIFO operation cannot occur by design.
2.20.3 DAR mode transmission failure due to lost arbitration A A NA The DAR mode lost-arbitration workaround is not implemented in the current Linux m_can driver, because although one-shot mode enables DAR, the driver does not perform the required recovery sequence of clearing the pending transmission request in TXBRP, handling the corresponding cancellation status in TXBCF, and explicitly restarting the transmission.
ETH 2.22.1 Incorrect gate control list switching for intermediate cycles when CTR is less than the GCL execution time A A NA The DWMAC EST erratum workaround does not appear to be implemented in the current Linux stmmac driver, because the driver programs the cycle time directly from the TAPRIO configuration without checking or adjusting it to ensure that CTR is either equal to the sum of the fully executed GCL intervals or greater than that sum by at least 8 PTP clock periods.
ETHSW 2.23.1 Reported bridge delays do not match measured values P P NA The workaround for this bridge delay reporting erratum not implemented in the current TTTech Ethernet switch driver, because no logic was found to monitor or enforce traffic below 90% line rate, nor any specific handling of the ETHSW_FES_I_TO_G_MAX_* and ETHSW_FES_G_TO_O_MAX_* delay reporting registers.
2.23.2 Tagged link local frames are discarded if the port is not part of the VLAN N N NA The workaround for this erratum not implemented in the current TTTech Ethernet switch driver, because no dedicated handling was found to exempt tagged link-local frames from the normal VLAN membership checks; therefore, VLAN tagging must not be used for link-local frames.

6. References[edit | edit source]