Last edited one month ago

STM32MPU OpenSTDroid Distribution Package

Applicable for STM32MP25x lines

This article describes how to obtain and use the Distribution Package of the Android-based OpenSTDroid embedded software for any development platform of the STM32MP25x lines  (STM32MP25 boards), in order to modify or add pieces of software, and to create the right Android™ distribution for the targeted product.

It lists some prerequisites in terms of knowledge and development environment and gives step-by-step instructions to download and install this Distribution Package.

1. Distribution Package content[edit | edit source]

If you are not familiar with the Android-based OpenSTDroid embedded software and its packages, it is recommanded to read the following articles:

In summary, this Distribution Package provides:

  • An Android build framework (also known as a distribution builder)
  • For the OpenSTDroid distribution (development on Arm® Cortex-A processor):
    • The BSP (Linux® kernel, U-Boot, TF-A, Trusty TEE) pieces in binary (prebuilt). Several scripts are provided to load source code and re-build them.
    • The application frameworks (including hardware abstraction code) pieces in source code.
  • For the FwST-M Packages (development on Arm® Cortex-M processor),
    • The BSP (MCUboot, TF-M) pieces in binary (prebuilt). Several scripts are provided to load source code and re-build them.
  • For the STM32Cube MPU Package (development on Arm Cortex-M processor), all pieces of software in source code: BSP, HAL, middlewares and applications.
  • A toolset to tune the system for your needs and to handle the built image (for example STM32CubeProgrammer to install the built image on the board).

2. Prerequisites[edit | edit source]

2.1. Knowledge[edit | edit source]

The STM32MPU Distribution Package aims to create an Android distribution for the targeted product: solid knowledge of Linux and Android are recommended to make the most of this Package.

The STM32MPU distribution for Android is an Android distribution based on the Android build framework: a short introduction about Android is available in AOSP[1].

Reading the Android-based OpenSTDroid software architecture overview is also highly recommended.

2.2. Development setup[edit | edit source]

The recommended setup for the development PC (host) is specified in the following article: PC prerequisites.

Whatever the development platform (board) and development PC (host) used, the range of possible development setups is illustrated by the picture below.

Development setup for Developer and Distribution Packages


The following components are mandatory:

  • Host PC for cross-compilation and cross-debugging, installed as specified above
  • Board assembled and configured as specified in the associated Starter Package article
  • Mass storage device (for example, microSD card) to load and update the software images (binaries)

The following components are optional, but recommended:

  • A serial link between the host PC (through Terminal program) and the board for traces (even early boot traces), and access to the board from the remote PC (command lines)
  • An Ethernet link between the host PC and the board for cross-development and cross-debugging through a local network. This is an alternative or a complement to the serial (or USB) link
  • A display connected to the board, depending on the technologies available on the board: DSI LCD display, HDMI monitor (or TV) and so on
  • A mouse and a keyboard connected through USB ports

Additional optional components can be added by means of the connectivity capabilities of the board: cameras, displays, JTAG, sensors, actuators, and much more.

3. Installing the OpenSTDroid distribution[edit | edit source]

Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

The installation relies on the repo command. If the Repo tool (a Google-built repository management tool that runs on top of Git) is not already installed and configured on the host PC, refer to the PC prerequisites article.

Create a working directory for the distribution (we recommended using the distribution name):

mkdir <working directory>
cd <working directory>

1- Initialize repo in the working directory:

repo init -u https://github.com/STMicroelectronics/android-manifest  -b refs/tags/<Tag> -m stm32mp2droid.xml

With

  • <Tag> = tag selecting the required version of the STM32MPU distribution for Android (see following table)
OpenSTDroid distribution
Tag android-<version> Release note
st-android-16.0.0-2026-05-26 android-16.0.0_r4 st-android-16.0.0-2026-05-26 release note (v6.2.0)
st-android-16.0.0-2026-09-08 android-16.0.0_r4 st-android-16.0.0-2026-09-08 release note (v6.2.1)

2- Synchronize the local project directories with the remote repositories specified in the manifest:

repo sync 

This may take time to retrieve all sources.

4. Local mirror[edit | edit source]

It can be of interest to create a local mirror of the different repositories used.

There are two possible kinds of cache:

  • REPO mirror: mirror of list of modules in repositories based on the provided manifest (for example: Android AOSP)
  • GIT mirror: mirror of one module (for example: Linux kernel)

4.1. REPO mirror[edit | edit source]

The REPO mirror is mainly used to mirror the Android AOSP sources.

1- Create and go to the cache directory

mkdir <PathToRepoCacheDir>
cd <PathToRepoCacheDir>

2- Mirror the required sources

case AOSP sources needed for the required version (recommended)

repo init -u https://android.googlesource.com/platform/manifest -b <Tag> --mirror
repo sync -q

case full AOSP sources

repo init -u https://android.googlesource.com/platform/manifest --mirror
repo sync -q

3- Create environment variable for this cache directory

export CACHE_DIR=<PathToRepoCacheDir>
Information
It is recommended to add this line in your .bashrc file available in your HOME directory

4- Use the cache directory

Add --reference=$CACHE_DIR option to your repo init command.

repo init --reference=$CACHE_DIR -u https://github.com/STMicroelectronics/android-manifest  -b refs/tags/<Tag> -m stm32mp2droid.xml

4.2. GIT mirror[edit | edit source]

While the distribution has been installed, a helper script cachesetup is available for this purpose, which creates / updates the mirrors based on the configuration file device/stm/<STM32Series>/scripts/cache/android_cache.config.

Make sure that if you change the environment variable name, you also update the associated load_xxxx scripts available in device/stm/<STM32Series>-xxxx/source directory.

Create the mirrors by executing the following commands:

source build/envsetup.sh
cachesetup --new

Regular updating of your mirror is recommended by executing:

cachesetup

For more information on how to use this command, refer to the cache setup usage (execute cachesetup -h).

Information
It is possible to update the AOSP or the Android REPO mirror using the command cachesetup aosp or cachesetup android

5. Building the OpenSTDroid distribution[edit | edit source]

When the installation is complete, refer to the How to build OpenSTDroid distribution page to learn how to build it.

6. Flashing the built image[edit | edit source]

When the distribution has been built, refer to the How to populate boards for Android page to learn how to flash your device.

7. References[edit | edit source]