Last edited 11 months ago

How to use the LVDS PRBS Generator for signal quality measurements

Applicable for STM32MP23x lines, STM32MP25x lines

A LVDS panel displaying a PRBS signal (channel 3, link 1) thanks to the LVDS PRBS generator on a STM32MP257F-EV1 Evaluation board

1. Article purpose[edit | edit source]

This article provides the basic information needed to enable LVDS PRBS[1] generator for signal quality measurements (eye pattern[2]) on OpenSTLinux distribution.

2. Introduction[edit | edit source]

The LVDS PRBS generator is capable of four sequences common in measuring and testing equipment. The polynomials are defined in ITU-T standard O.150: PRBS7, PRBS15, PRBS23 and PRBS31.

The LVDS PRBS polynomial is selected using the LVDS channel distribution link 2 configuration register LVDS_CDL2CR.PRBS (address 0x2C). Note: It is advised to use the most complex PRBS31 polynomial which provides a longer random sequence because a longer period generally produces a greater variety of data patterns that more thoroughly check the transmission system's performance.

The PRBS is transmitted outside by selecting it as a Channel, in the channel distribution operator, by selecting LVDS_CDLxCR.DISTRy = 0xA, for any Lane y of Link x.

Refer to the STM32 MPU reference manuals for the complete LVDS PRBS feature and register descriptions.

To sum up:

  1. Identify LVDS lanes on the board and connect them to the measurement equipment.
  2. Thanks to the board device tree, identify LVDS links (only link 1, only link 2 or both links 1 and 2) and related LVDS channels / distribution channels (jeida, vesa, ...). Please refer to LVDS device tree configuration for more details.
  3. Power up the board and be sure the LVDS is running.
  4. Select the PRBS polynomial type by writing in the LVDS channel distribution link 2 configuration register LVDS_CDL2CR.PRBS (address 0x2C).
  5. Enable PRBS by writing in the LVDS channel distribution link 1&2 configuration registers LVDS_CDLxCR.DISTRy (address 0x2C/0x30) the value 0xa, for any Lane y of Link x.
  6. Use the measurement equipments.

3. Installing Devmem or GDB on the target board[edit | edit source]

The simplest ways for enabling the LVDS PRBS are:

  • using the command line devmem2 tool: please refer to How to read or write peripheral registers article for its installation and usage.
  • using the debug and trace gdb tool: please refer to GDB article for its installation and usage.

4. Getting started[edit | edit source]

Once both the board under test and the measurement equipment are ready, follow the below procedure based on the devmem2 tool (Note: a similar procedure can be done with gdb tool too):

1. Boot the board and read the two related registers running values:

devmem2 0x4806002c # LVDS_CDL1CR for link 1
/dev/mem opened.
Memory mapped at address 0xffffa051e000.
Read at address  0x4806002C (0xffffa051e02c): 0x00004321
devmem2 0x48060030 # LVDS_CDL2CR for link 2 and PRBS polynomial type
/dev/mem opened.
Memory mapped at address 0xffff9e169000.
Read at address  0x48060030 (0xffff9e169030): 0x00000000

2. Configure the PRBS polynomial type (3 for the longest sequence) in LVDS_CDL2CR register:

devmem2 0x48060030 w 0x03000000 # LVDS_CDL2CR.PRBS=3
/dev/mem opened.
Memory mapped at address 0xffffa60fb000.
Read at address  0x48060030 (0xffffa60fb030): 0x00000000
Write at address 0x48060030 (0xffffa60fb030): 0x03000000, readback 0x03000000

3. Enable the PRBS by writing 0xa on a given distribution lane of a given link, here below distribution channel 3 (set to channel 4) of link 1:

devmem2 0x4806002c w 0x0a321 # LVDS_CDL1CR = 0x0a321 ie. enable prbs on DISTR3 (channel 4) of link 1
/dev/mem opened.
Memory mapped at address 0xffff8bb00000.
Read at address  0x4806002C (0xffff8bb0002c): 0x00004321
Write at address 0x4806002C (0xffff8bb0002c): 0x0000A321, readback 0x0000A321

4. Perform the eye pattern test with the measurement equipment. When done, continue with other lanes and links.


Information
Before making any measurements, it may be useful to test the procedure on a real LVDS panel, keeping in mind that enabling PRBS on the channels carrying the clock or blankings will cause the screen to become desynchronized and therefore display nothing.

5. Alternatives[edit | edit source]

It is also possible to use STM32CubeMP2 instead of OpenSTLinux distribution

6. References[edit | edit source]