Last edited 7 months ago

How to cross-compile with the Developer Package

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Article purpose[edit | edit source]

This article provides simple examples for the Developer Package of the OpenSTLinux distribution, that illustrate cross-compilation with the SDK:

  • modification of software elements delivered as source code (for example the Linux kernel)
  • addition of software (for example the Linux kernel module or user-space applications)

These examples also show how to deploy the results of the cross-compilation on the target, through a network connection to the host machine.

Information
There are many ways to achieve the same result; this article aims to provide at least one solution per example. You are free to explore other methods that are better adapted to your development constraints.

2. Prerequisites[edit | edit source]

The prerequisites from the Cross-compile with OpenSTLinux SDK article must be executed, and the cross-compilation and deployment of any piece of software, as explained in that article, is known.

The board and the host machine are connected through an Ethernet link, and a remote terminal program is started on the host machine: see How to get Terminal.

The target is started, and its IP address (<board ip address>) is known.

Information
If you encounter a problem with any of the commands in this article, remember that the README.HOW_TO.<board flavor>.txt helper files, from the Linux kernel, OP-TEE OS, TF-A and U-Boot installation directories, are the build references.
Information
Regarding the Linux kernel examples, it is considered that the Linux kernel has been setup, configured and built a first time in a dedicated build directory (<Linux kernel build directory> later in this page) different from the source code directory (<Linux kernel source directory> later in this document).

3. Modifying the Linux kernel configuration[edit | edit source]

3.1. Preamble[edit | edit source]

Warning
Please read carefully and pay attention to the following point before modifying the Linux kernel configuration

The Linux kernel configuration option that you want to modify might be used by external out-of-tree Linux kernel modules (for example the GPU kernel driver), and these should then be recompiled. These modules are, by definition, outside the kernel tree structure, and are not delivered in the Developer Package source code; it is not possible to recompile them with the Developer Package. Consequently, if the Linux kernel is reconfigured and recompiled with this option then deployed on the board, the external out-of-tree Linux kernel modules might no longer be loaded.

There are two possible situations:

  • This is not a problem for the use cases on which you are currently working. In this case you can use the Developer Package to modify and recompile the Linux kernel.
  • This is a problem for the use cases on which you are currently working. In this case you need to switch on the STM32MPU Distribution Package, and after having modified the Linux kernel configuration, use it to rebuild the whole image (that is, not only the Linux kernel but also the external out-of-tree Linux kernel modules).

Example:

  • Let's assume that the FUNCTION_TRACER and FUNCTION_GRAPH_TRACER options are activated to install the ftrace Linux kernel feature
  • This feature is used to add tracers in the whole kernel, including the external out-of-tree Linux kernel modules
  1. The Developer Package is used to reconfigure and recompile the Linux kernel, and to deploy it on the board
    1. The external out-of-tree Linux kernel modules are not recompiled. This is the case for the GPU kernel driver
    2. Consequently, the Linux kernel fails to load the GPU kernel driver module. However, even if the display no longer works, the Linux kernel boot succeeds, and the setup is sufficient, for example, to debug use cases involving an Ethernet or USB connection
  2. The Distribution Package is used to reconfigure the Linux kernel, and to rebuild and deploy the whole image on the board
    1. The external out-of-tree Linux kernel modules are recompiled, including the GPU kernel driver
    2. Consequently, the Linux kernel succeeds in loading the GPU kernel driver module. The display is available.

3.2. Simple example[edit | edit source]

This simple example modifies the value defined for the contiguous memory area (CMA) size.

  • Get the current value of the CMA size through the analysis of the target boot log
dmesg | grep -i cma
STM32MP135F-DK
[    0.000000] cma: Reserved 64 MiB at 0xd8800000
STM32MP157F-EV1
[    0.000000] Reserved memory: created CMA memory pool at 0xf5800000, size 128 MiB
STM32MP157F-DK2
[    0.000000] cma: Reserved 64 MiB at 0xd9800000
STM32MP215F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
STM32MP257F-DK for STM32MP23x lines evaluation
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB
STM32MP257F-EV1
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB
STM32MP257F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB

Note that dmesg information provides indication regarding CMA size configuration:

- With cma: Reserved message: the CMA size configuration is made via the kernel configuration
- With Reserved memory: created CMA memory pool message: the CMA size configuration is declared on kernel devicetree

Thus, in our example for modifying the Linux kernel configuration, we will only consider the STM32MP135F-DK and STM32MP157F-DK2 boards.

  • Go to the Linux kernel build directory
cd <Linux kernel build directory>
  • Navigate to "Device Drivers - Generic Driver Options"
    • select "Size in Megabytes"
    • modify its value to 256
    • exit and save the new configuration
  • Check that the configuration file (.config) has been modified
grep -i CONFIG_CMA_SIZE_MBYTES .config
CONFIG_CMA_SIZE_MBYTES=256
  • Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
dmesg | grep -i cma
STM32MP135F-DK
[    0.000000] cma: Reserved 256 MiB at 0xd8800000
STM32MP157F-DK2
[    0.000000] cma: Reserved 256 MiB at 0xd9800000

4. Modifying the Linux kernel device tree[edit | edit source]

4.1. STM32MP135F-DK and STM32MP157F-DK2 simple example[edit | edit source]

This simple example modifies the default status of a user LED.

  • With the board started; check that the user green LED (LD4 for STM32MP135F-DK , LD5 for STM32MP157F-DK2 ) is disabled
  • Go to the Linux kernel source directory
cd <Linux kernel source directory>
  • Edit the device tree source file to add the lines highlighted below
STM32MP135F-DK arch/arm/boot/dts/stm32mp135f-dk.dts
	leds {
		compatible = "gpio-leds";
		led-blue {
			function = LED_FUNCTION_HEARTBEAT;
			color = <LED_COLOR_ID_BLUE>;
			gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
			linux,default-trigger = "heartbeat";
			default-state = "off";
		};
		led-red {
			label = "stm32mp:red:user";
			gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
			default-state = "on";
		};
	};
STM32MP157F-DK2 arch/arm/boot/dts/stm32mp15xx-dkx.dtsi
	led {
		compatible = "gpio-leds";
		led-blue {
			label = "heartbeat";
			gpios = <&gpiod 11 GPIO_ACTIVE_HIGH>;
			linux,default-trigger = "heartbeat";
			default-state = "off";
		};
 		led-green {
 			label = "stm32mp:green:user";
 			gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
 			default-state = "on";
  		};
	};
  • Go to the Linux kernel build directory
cd <Linux kernel build directory>
  • Generate the device tree blobs (*.dtb) from Linux repository tree repository usage.
make dtbs

or see STM32MP257F-EV1 Evaluation board with external device tree to generate the dtb from external device
then

cp arch/<arm architecture>/boot/dts/stm32mp*.dtb install_artifact/boot/
  • Update the device tree blobs on the board
scp install_artifact/boot/stm32mp*.dtb root@<board ip address>:/boot/
  • Reboot the board
reboot
  • Check that the user green LED (LD4 for STM32MP135F-DK , LD5 for STM32MP157F-DK2 ) is enabled (green)

4.2. STM32MP2 series simple example[edit | edit source]

This simple example modifies the value defined for the contiguous memory area (CMA) size.

  • Get the current value of the CMA size through the analysis of the target boot log
dmesg | grep -i cma
STM32MP215F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 128 MiB
STM32MP257F-DK for STM32MP23x lines evaluation
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB
STM32MP257F-EV1
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB
STM32MP257F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 128 MiB

Note that dmesg information provides indication regarding CMA size configuration:

- With cma: Reserved message: the CMA size configuration is made via the kernel configuration
- With Reserved memory: created CMA memory pool message: the CMA size configuration is declared on kernel devicetree

Thus, in our example for modifying the Linux kernel device tree, we will only consider the STM32MP257F-EV1 boards.

  • Go to the Linux kernel source directory
cd <Linux kernel source directory>
  • Edit the device tree source file to modify the highlighted CMA size value below
STM32MP215F-DK arch/arm64/boot/dts/st/stm32mp215f-dk-ca35tdcid-resmem.dtsi
		linux,cma {
			compatible = "shared-dma-pool";
			reusable;
			alloc-ranges = <0 0x80000000 0 0x80000000>;
			size = <0x0 0x0x8000000>;
			alignment = <0x0 0x2000>;
			linux,cma-default;
		};
STM32MP257F-DK for STM32MP23x lines evaluation arch/arm64/boot/dts/st/stm32mp235f-dk-ca35tdcid-resmem.dtsi
		linux,cma {
			compatible = "shared-dma-pool";
			reusable;
			alloc-ranges = <0 0x80000000 0 0x80000000>;
			size = <0x0 0x0x8000000>;
			alignment = <0x0 0x2000>;
			linux,cma-default;
		};
STM32MP257F-EV1 arch/arm64/boot/dts/st/stm32mp257f-ev1-ca35tdcid-resmem.dtsi
		linux,cma {
			compatible = "shared-dma-pool";
			reusable;
			alloc-ranges = <0 0x80000000 0 0x80000000>;
			size = <0x0 0x0x8000000>;
			alignment = <0x0 0x2000>;
			linux,cma-default;
		};
STM32MP257F-DK arch/arm64/boot/dts/st/stm32mp257f-dk-ca35tdcid-resmem.dtsi
		linux,cma {
			compatible = "shared-dma-pool";
			reusable;
			alloc-ranges = <0 0x80000000 0 0x80000000>;
			size = <0x0 0x0x8000000>;
			alignment = <0x0 0x2000>;
			linux,cma-default;
		};
  • Modify the current 128MB size to match with 256MB one: 256MB = 0x10000000
  • Go to the Linux kernel build directory
cd <Linux kernel build directory>
  • Generate the device tree blobs (*.dtb)
make dtbs
  • Copy the generated device tree blobs to a dedicated install folder:
cp arch/<arm architecture>/boot/dts/stm32mp*.dtb install_artifact/boot/
  • Update the device tree blobs on the board
scp install_artifact/boot/stm32mp*.dtb root@<board ip address>:/boot/
  • Reboot the board
reboot
  • Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
dmesg | grep -i cma
STM32MP215F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f7600000, size 256 MiB
STM32MP257F-DK for STM32MP23x lines evaluation
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 256 MiB
STM32MP257F-EV1
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 256 MiB
STM32MP257F-DK
[    0.000000] Reserved memory: created CMA memory pool at 0x00000000f2200000, size 256 MiB

4.3. Using external device tree with KBUILD_EXTDTS[edit | edit source]

For compilation of external device tree (aka OSTL device tree) in the external git, you can add this git outside Linux® kernel tree.

 git clone  https://github.com/STMicroelectronics/dt-stm32mp.git <External device tree directory>

4.3.1. External git outside Linux® kernel tree with KBUILD_EXTDTS for the STM32MP1 series[edit | edit source]

Go to the Linux kernel build directory and build:

 cd <Linux kernel build directory>
 make dtbs KBUILD_EXTDTS=<External device tree directory>/stm32mp1/linux
 or you can also build directly one of the available target by simply calling, for example:
 make stm32mp135f-dk-pmic1ld-ostl.dtb KBUILD_EXTDTS=<External device tree directory>/stm32mp1/linux

4.3.2. External git outside Linux® kernel tree with KBUILD_EXTDTS for the STM32MP2 series[edit | edit source]

Go to the Linux kernel build directory and build:

 cd <Linux kernel build directory>
4.3.2.1. Example for A35-TD flavor [edit | edit source]
 make dtbs KBUILD_EXTDTS=<External device tree directory>/stm32mp2/a35-td/linux
 or you can also build directly one of the available target by simply calling, for example:
 make stm32mp257f-ev1-ca35tdcid-ostl.dtb KBUILD_EXTDTS=<External device tree directory>/stm32mp2/a35-td/linux
4.3.2.2. Example for M33-TD flavor [edit | edit source]
 make dtbs KBUILD_EXTDTS=<External device tree directory>/stm32mp2/m33-td/linux
 or you can also build directly one of the available target by simply calling, for example:
 make stm32mp257f-ev1-cm33tdcid-ostl.dtb KBUILD_EXTDTS=<External device tree directory>/stm32mp2/m33-td/linux

5. Modifying a built-in Linux kernel device driver[edit | edit source]

This simple example adds unconditional log information when the display driver is probed.

  • Check that there's no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe

  • Go to the Linux kernel source directory
cd <Linux kernel source directory>
  • Edit the ./drivers/gpu/drm/stm/drv.c source file
  • Add a log information in the stm_drm_platform_probe function
static int stm_drm_platform_probe(struct platform_device *pdev)
{
	struct device *dev = &pdev->dev;
	struct drm_device *ddev;
	int ret;
	[...]

	DRM_INFO("Simple example - %s\n", __func__);

	return 0;
	[...]
}
  • Go to the Linux kernel build directory
cd <Linux kernel build directory>
  • Cross-compile the Linux kernel (please select the expected target)
- For STM32MP1 series
[ "${ARCH}" = "arm" ] && imgtarget="uImage" || imgtarget="Image.gz"
make ${imgtarget} LOADADDR=0xC2000040
cp arch/<arm architecture>/boot/${imgtarget} install_artifact/boot/
- For STM32MP2 series
[ "${ARCH}" = "arm" ] && imgtarget="uImage" || imgtarget="Image.gz"
make ${imgtarget} LOADADDR=0x88008000
cp arch/<arm architecture>/boot/${imgtarget} install_artifact/boot/
  • Update the Linux kernel image on board
scp -r install_artifact/boot/* root@<board ip address>:/boot/
  • Reboot the board
reboot
  • Check that there is now log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
[    2.995125] [drm] Simple example - stm_drm_platform_probe

6. Modifying/adding an external Linux kernel module[edit | edit source]

Most device drivers (modules) in the Linux kernel can be compiled either into the kernel itself (built-in/internal module) or as Loadable Kernel Modules (LKM/external module) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).

6.1. Modifying an external in-tree Linux kernel module[edit | edit source]

This simple example adds an unconditional log information when the virtual video test driver (vivid) kernel module is probed or removed.

  • Go to the Linux kernel source directory
cd <Linux kernel source directory>
  • Edit the ./drivers/media/test-drivers/vivid/vivid-core.c source file
  • Add log information in the vivid_probe and vivid_remove functions
static int vivid_probe(struct platform_device *pdev)
{
	const struct font_desc *font = find_font("VGA8x16");
	int ret = 0, i;
	[...]

	/* n_devs will reflect the actual number of allocated devices */
	n_devs = i;

	pr_info("Simple example - %s\n", __func__);

	return ret;
}
static void vivid_remove(struct platform_device *pdev)
{
	struct vivid_dev *dev;
	unsigned int i, j;
	[...]

	pr_info("Simple example - %s\n", __func__);
}
  • Go to the Linux kernel build directory
cd <Linux kernel build directory>

  • Cross-compile the Linux kernel modules
make modules
make INSTALL_MOD_PATH="./install_artifact" modules_install
  • Remove the link on install_artifact/lib/modules/<kernel version>/
rm install_artifact/lib/modules/<kernel version>/build
rm install_artifact/lib/modules/<kernel version>/source
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
  • Update the vivid kernel module on the board (please check the kernel version <kernel version>)
scp install_artifact/lib/modules/"<kernel version>"/kernel/drivers/media/test-drivers/vivid/vivid.ko root@<board ip address>:/lib/modules/<kernel version>/kernel/drivers/media/test-drivers/vivid/

OR

scp -r install_artifact/lib/modules/* root@<board ip address>:/lib/modules/
  • Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
  • Insert the vivid kernel module into the Linux kernel
modprobe vivid                   
[...]
[ 3412.784638] Simple example - vivid_probe
  • Remove the vivid kernel module from the Linux kernel
rmmod vivid
[...]
[ 3423.708517] Simple example - vivid_remove

6.2. Adding an external out-of-tree Linux kernel module[edit | edit source]

This simple example adds a "Hello World" external out-of-tree Linux kernel module to the Linux kernel.

  • Prerequisite: the Linux source code is installed, and the Linux kernel has been cross-compiled
  • Go to the working directory that contains all the source code (that is, the directory that contains the Linux kernel, OP-TEE OS, TF-A and U-Boot source code directories)
cd <tag>/sources/<arm architecture>-<distro>-linux*
  • Export to KERNEL_SRC_PATH the path to the Linux kernel build directory that contains both the Linux kernel source code and the configuration file (.config)
export KERNEL_SRC_PATH=$PWD/<Linux kernel build directory>/
  • Create a directory for this kernel module example
mkdir kernel_module_example
cd kernel_module_example
  • Create the source code file for this kernel module example: kernel_module_example.c
// SPDX-identifier: GPL-2.0
/*
 * Copyright (C) STMicroelectronics SA 2018
 *
 * Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
 *
 */

#include <linux/module.h>    /* for all kernel modules */
#include <linux/kernel.h>    /* for KERN_INFO */
#include <linux/init.h>      /* for __init and __exit macros */

static int __init kernel_module_example_init(void)
{
	printk(KERN_INFO "Kernel module example: hello world from STMicroelectronics\n");
	return 0;
}

static void __exit kernel_module_example_exit(void)
{
	printk(KERN_INFO "Kernel module example: goodbye from STMicroelectronics\n");
}

module_init(kernel_module_example_init);
module_exit(kernel_module_example_exit);

MODULE_DESCRIPTION("STMicroelectronics simple external out-of-tree Linux kernel module example");
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>");
MODULE_LICENSE("GPL v2");
  • Create the makefile for this kernel module example: Makefile
Information
All the indentations in a makefile are tabulations
# Makefile for simple external out-of-tree Linux kernel module example

# Object file(s) to be built
obj-m:= kernel_module_example.o

# Path to the directory that contains the Linux kernel source code
# and the configuration file (.config)
KERNEL_DIR ?=  $(KERNEL_SRC_PATH)

# Path to the directory that contains the generated objects
DESTDIR?= $(KERNEL_DIR)/install_artifact

# Path to the directory that contains the source file(s) to compile
PWD:= $(shell pwd) 
  
default:
	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules

install:
	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install

clean:
	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean
  • Cross-compile the kernel module example
make clean
make
make install
  • Go to the Linux kernel build directory
cd <Linux kernel build directory>
  • The generated kernel module example is in: install_artifact/lib/modules/"<kernel version>"/extra/kernel_module_example.ko
  • Remove the link on "install_artifact/lib/modules/<kernel version>/"
rm install_artifact/lib/modules/<kernel version>/build
rm install_artifact/lib/modules/<kernel version>/source
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
  • Push this kernel module example on board (please check the kernel version "<kernel version>")
ssh root@<board ip address> mkdir -p /lib/modules/"<kernel version>"/extra
scp install_artifact/lib/modules/<kernel version>/extra/kernel_module_example.ko root@<board ip address>:/lib/modules/<kernel version>/extra

OR

scp -r install_artifact/lib/modules/* root@<board ip address>:/lib/modules/
  • Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
  • Insert the kernel module example into the Linux kernel
modprobe kernel_module_example
[18167.821725] Kernel module example: hello world from STMicroelectronics
  • Remove the kernel module example from the Linux kernel
rmmod kernel_module_example
[18180.086722] Kernel module example: goodbye from STMicroelectronics

7. Modifying the U-Boot[edit | edit source]

This simple example adds unconditional log information when U-Boot starts. Within the scope of the OpenSTLinux boot chain, U-Boot is used as second stage boot loader (SSBL).

  • Have a look at the U-Boot log information when the board reboots
reboot
STM32MP1 series' boards
U-Boot <U-Boot version> (<U-Boot build time flag>)
CPU: <CPU tag marking>
Model: STMicroelectronics <board model details>
Board: stm32mp1 in <boot chain mode> mode (st,<device tree>)
STM32MP2 series' boards
U-Boot <U-Boot version> (<U-Boot build time flag>)
CPU: <CPU tag marking>
Model: STMicroelectronics <board model details>
Board: stm32mp2 (st,<device tree>)
  • Go to the U-Boot source directory
cd <U-Boot source directory>
  • Edit the source file to add the lines highlighted below in the checkboard function
STM32MP1 series' boards board/st/stm32mp1/stm32mp1.c
int checkboard(void)
{
	int ret;
	char *mode;
	[...]

	log_info("Board: stm32mp1 in %s mode (%s)\n", mode,
		 fdt_compat && fdt_compat_len ? fdt_compat : "");
	log_info("U-Boot simple example\n");
	[...]

	return 0;
}
STM32MP2 series' boards board/st/stm32mp2/stm32mp2.c
int checkboard(void)
{
	int ret;
	u32 otp;
	[...]

	log_info("Board: stm32mp2 (%s)\n", fdt_compat && fdt_compat_len ? fdt_compat : "");
	log_info("U-Boot simple example\n");
	[...]

	return 0;
}
  • Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk.<board flavor> help
  • FIP image case building

The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new U-Boot binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" variable should be set as below:

export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts

Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" variable should be set as below:

export FIP_DEPLOYDIR_FIP=$PWD/../deploy/fip
  • Cross-compile the U-Boot to generate FIP binary update:
- E.g. for optee boot scheme for STM32MP157F-EV1 and STM32MP157F-DK2
make -f $PWD/../Makefile.sdk.stm32mp1 all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp15_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp157f-ev1 stm32mp157f-dk2"
- E.g. for optee boot scheme for STM32MP135F-DK
make -f $PWD/../Makefile.sdk.stm32mp1 all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp13_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp135f-dk"
- E.g. for optee boot scheme for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp21_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp215f-dk"
- E.g. for optee boot scheme for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2 all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp23_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp235f-dk"
- E.g. for optee boot scheme for STM32MP257F-EV1 and STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 all UBOOT_CONFIG=default UBOOT_DEFCONFIG=stm32mp25_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE="stm32mp257f-ev1 stm32mp257f-dk"
  • Go to the directory where the compilation results are stored
cd $FIP_DEPLOYDIR_FIP
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
ls -l /dev/disk/by-partlabel/ | grep 'fip-a'
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fip-a -> ../../sdb5
  • Copy the FIP binary to the dedicated partition
dd if=fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
  • Reset the U-Boot shell: in the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
  • Have a look at the new U-Boot log information when the board reboots
STM32MP1 series' boards
U-Boot <U-Boot version> (<U-Boot build time flag>)
CPU: <CPU tag marking>
Model: STMicroelectronics <board model details>
Board: stm32mp1 in <boot chain mode> mode (st,<device tree>)
U-Boot simple example
STM32MP2 series' boards
U-Boot <U-Boot version> (<U-Boot build time flag>)
CPU: <CPU tag marking>
Model: STMicroelectronics <board model details>
Board: stm32mp2 (st,<device tree>)
U-Boot simple example

8. Modifying the TF-A[edit | edit source]

8.1. TF-A modification example[edit | edit source]

This simple example adds unconditional log information when the TF-A starts. Within the scope of the OpenSTLinux boot chain, TF-A is used as first stage boot loader (FSBL).

  • Have a look at the TF-A log information when the board reboots
reboot
STM32MP1 series' boards
INFO:    PMIC version = <PMIC version>
NOTICE:  Reset reason (<Reset id number>):
INFO:      Power-on Reset (rst_por)
STM32MP2 series' boards
INFO:    Reset reason (<Reset id number>):
INFO:      Power-on Reset (rst_por)
INFO:    PMIC2 version = <PMIC version>
  • Go to the TF-A source directory
cd <TF-A source directory>
  • Edit the source file to add the lines highlighted below in the print_reset_reason function
STM32MP1 series' boards plat/st/stm32mp1/bl2_plat_setup.c
static void print_reset_reason(void)
{
	[...]
	NOTICE("Reset reason (0x%x):\n", rstsr);
	INFO("TF-A simple example\n");
	[...]
}
STM32MP2 series' boards plat/st/stm32mp2/bl2_plat_setup.c
static void print_reset_reason(void)
{
	[...]
	NOTICE("Reset reason (0x%x):\n", rstsr);
	INFO("TF-A simple example\n");
	[...]
}
  • Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk.<board flavor> help
Information
According to the modification done on TF-A source code, both TF-A FSBL and FIP binaries may need to be updated. You will find below the steps to follow for both update

8.2. TF-A image case building[edit | edit source]

  • Cross-compile the TF-A:
- E.g. for microSD card boot and optee boot scheme for STM32MP157F-EV1 and STM32MP157F-DK2
make -f $PWD/../Makefile.sdk.stm32mp1 TF_A_DEVICETREE="stm32mp157f-ev1 stm32mp157f-dk2" TF_A_CONFIG="optee-sdcard" stm32
- E.g. for microSD card boot and optee boot scheme for STM32MP135F-DK
make -f $PWD/../Makefile.sdk.stm32mp1 TF_A_DEVICETREE="stm32mp135f-dk" TF_A_CONFIG="optee-sdcard" stm32
- E.g. for microSD card boot and optee boot scheme for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp215f-dk" TF_A_CONFIG="optee-sdcard" stm32
- E.g. for microSD card boot and optee boot scheme for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp235f-dk" TF_A_CONFIG="optee-sdcard" stm32
- E.g. for microSD card boot and optee boot scheme for STM32MP257F-EV1 and STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp257f-ev1 stm32mp257f-dk" TF_A_CONFIG="optee-sdcard" stm32
  • Go to the directory in which the compilation results are stored
cd ../deploy
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the FSBL partition associated with the first stage boot loader
ls -l /dev/disk/by-partlabel/ | grep fsbl
STM32MP1 series' boards
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsbl1 -> ../../sdb1
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsbl2 -> ../../sdb2
STM32MP2 series' boards
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsbla1 -> ../../sdb1
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsbla2 -> ../../sdb2

Note that there are two FSBL partitions to ensure first stage boot loader binary backup.

  • Copy the TF-A binary to the dedicated partition; to test the new TF-A binary, it might be useful to keep the old TF-A binary in the backup FSBL (fsbl2 or fsbla2)
dd if=tf-a-<device tree>-sdcard.stm32 of=/dev/sdb1 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb1 :
sudo chmod 777 /dev/sdb1
  • Reset the U-Boot shell: in the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset

8.3. FIP image case building[edit | edit source]

The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new TF-A binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" var should be set as below:

export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts

Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" var should be set as below:

export FIP_DEPLOYDIR_FIP=$PWD/../deploy/fip
  • Cross-compile the TF-A to generate FIP binary update:
- E.g. for microSD card boot and optee boot scheme for STM32MP157F-EV1 and STM32MP157F-DK2 :
make -f $PWD/../Makefile.sdk.stm32mp1 TF_A_DEVICETREE="stm32mp157f-ev1 stm32mp157f-dk2" TF_A_CONFIG="optee-sdcard" fip
- E.g. for microSD card boot and optee boot scheme for STM32MP135F-DK
make -f $PWD/../Makefile.sdk.stm32mp1 TF_A_DEVICETREE="stm32mp135f-dk" TF_A_CONFIG="optee-sdcard" fip
- E.g. for microSD card boot and optee boot scheme for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp215f-dk" TF_A_CONFIG="optee-sdcard" fip
- E.g. for microSD card boot and optee boot scheme for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp235f-dk" TF_A_CONFIG="optee-sdcard" fip
- E.g. for microSD card boot and optee boot scheme for STM32MP257F-EV1 and STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 TF_A_DEVICETREE="stm32mp257f-ev1 stm32mp257f-dk" TF_A_CONFIG="optee-sdcard" fip
  • Go to the directory in which the compilation results are stored
cd $FIP_DEPLOYDIR_FIP
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
ls -l /dev/disk/by-partlabel/ | grep 'fip-a'
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fip-a -> ../../sdb5
  • Copy the FIP binary to the dedicated partition
dd if=fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
  • Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset

8.4. TF-A modification results[edit | edit source]

  • Have a look at the new TF-A log information when the board reboots
STM32MP1 series' boards
INFO:    PMIC version = <PMIC version>
NOTICE:  Reset reason (<Reset id number>):
INFO:      Power-on Reset (rst_por)
INFO:    TF-A simple example
STM32MP2 series' boards
INFO:    Reset reason (<Reset id number>):
INFO:      Power-on Reset (rst_por)
INFO:    TF-A simple example
INFO:    PMIC2 version = <PMIC version>

9. Modifying the OP-TEE OS[edit | edit source]

This simple example adds unconditional log information when the OP-TEE OS starts.

  • Have a look at the OP-TEE OS log information when the board reboots
reboot
[...]
I/TC: Embedded DTB found
I/TC: OP-TEE version: <OP-TEE OS version> (gcc version <GCC version>) [...]
I/TC: WARNING: This OP-TEE configuration might be insecure!
[...]
  • Go to the OP-TEE OS source directory
cd <OP-TEE OS source directory>
  • Edit the ./core/arch/arm/kernel/boot.c source file to add the lines highlighted below in the __weak boot_init_primary_late function
void __weak boot_init_primary_late(unsigned long fdt,
                   unsigned long manifest)
{
	init_external_dt(fdt);
	[...]

	IMSG("OP-TEE version: %s", core_v_str);
	IMSG("OP-TEE OS simple example");
 	[...]
}
  • Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk.<board flavor> help
  • FIP images case building

The "FIP_artifacts" folder should be specified to allow to update the FIP binary with the new OP-TEE OS binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "FIP_DEPLOYDIR_ROOT" var should be set as below:

export FIP_DEPLOYDIR_ROOT=$PWD/../../FIP_artifacts

Note that to keep the original FIP binary, the "FIP_DEPLOYDIR_FIP" var should be set as below:

export FIP_DEPLOYDIR_FIP=$PWD/../deploy/fip
  • Cross-compile the OP-TEE OS to generate FIP binary update:
- E.g. for optee boot scheme for STM32MP157F-EV1 and STM32MP157F-DK2
make -f $PWD/../Makefile.sdk.stm32mp1 all OPTEE_CONFIG=optee CFG_EMBED_DTB_SOURCE_FILE="stm32mp157F-ev1 stm32mp157f-dk2"
- E.g. for optee boot scheme for STM32MP135F-DK
make -f $PWD/../Makefile.sdk.stm32mp1 all OPTEE_CONFIG=optee CFG_EMBED_DTB_SOURCE_FILE="stm32mp135f-dk"
- E.g. for optee boot scheme for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 all OPTEE_CONFIG=optee CFG_EMBED_DTB_SOURCE_FILE="stm32mp215f-dk"
- E.g. for optee boot scheme for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2 all OPTEE_CONFIG=optee CFG_EMBED_DTB_SOURCE_FILE="stm32mp235f-dk"
- E.g. for optee boot scheme for STM32MP257F-EV1 and STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2 all OPTEE_CONFIG=optee CFG_EMBED_DTB_SOURCE_FILE="stm32mp257f-ev1 stm32mp257f-dk"
  • Go to the directory where the compilation results are stored
cd $FIP_DEPLOYDIR_FIP
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the secondary stage boot loader that contains the FIP binary: fip-a
ls -l /dev/disk/by-partlabel/ | grep 'fip-a'
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fip-a -> ../../sdb5
  • Copy the FIP binary to the dedicated partition
dd if=fip-<device tree>-<boot chain mode>.bin of=/dev/sdb5 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb5:
sudo chmod 777 /dev/sdb5
  • Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset
  • Have a look at the new OP-TEE OS log information when the board reboots
[...]
I/TC: Embedded DTB found
I/TC: OP-TEE version: <OP-TEE OS version> (gcc version <GCC version>) [...]
I/TC: OP-TEE OS simple example
I/TC: WARNING: This OP-TEE configuration might be insecure!
[...]

10. Modifying the TF-M[edit | edit source]

  • Go to the TF-M source directory
cd <TF-M source directory>
  • Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk.stm32mp2-m33td help
  • TF-M firmware case building

The "M33FW_artifacts" folder should be specified to allow to update the M33 firmware with the new TF-M binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "M33FW_DEPLOYDIR_ROOT" var should be set as below:

export M33FW_DEPLOYDIR_ROOT=$PWD/../../M33FW_artifacts
  • Cross-compile the TF-M to generate TF-M binary update:
- E.g. for sdcard boot device for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp215f_dk M33FW_DEVICETREE=stm32mp215f-dk-cm33tdcid-ostl tfm
- E.g. for sdcard boot device for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp235f_dk M33FW_DEVICETREE=stm32mp235f-dk-cm33tdcid-ostl tfm
- E.g. for sdcard boot device for STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp257f_dk M33FW_DEVICETREE=stm32mp257f-dk-cm33tdcid-ostl tfm
- E.g. for nor-sdcard boot device for STM32MP257F-EV1
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_nor-sdcard TF_M_PLATFORM=stm/stm32mp257f_ev1 M33FW_DEVICETREE=stm32mp257f-ev1-cm33tdcid-ostl tfm
  • Go to the directory where the compilation results are stored
cd $M33FW_DEPLOYDIR_ROOT/arm-trusted-firmware-m/bl2
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the first stage boot loader that contains the BL2 binary: fsblm1 and fsblm2
ls -l /dev/disk/by-partlabel/ | grep fsblm
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsblm1 -> ../../sdb5
lrwxrwxrwx 1 root root 10 Feb  8 08:57 fsblm2 -> ../../sdb6
  • Copy the TF-M binary to the dedicated partition
dd if=bl2-<device tree>-<m33 boot device>.stm32 of=/dev/sdb5 bs=1M conv=fdatasync
dd if=bl2-<device tree>-<m33 boot device>.stm32 of=/dev/sdb6 bs=1M conv=fdatasync

{{Info|In case you get a permission denied you can set more permission on /dev/sdb5 or /dev/sdb6:

sudo chmod 777 /dev/sdb5
sudo chmod 777 /dev/sdb6
  • M33 firmware case building
  • Cross-compile the TF-M to generate M33 firmwares update:

The m33tdprojects Starter binary should be available in ${M33FW_DEPLOYDIR_ROOT}/m33-projects folder

- E.g. for sdcard boot device for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp215f_dk M33FW_DEVICETREE=stm32mp215f-dk-cm33tdcid-ostl m33fw
- E.g. for sdcard boot device for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp235f_dk M33FW_DEVICETREE=stm32mp235f-dk-cm33tdcid-ostl m33fw
- E.g. for sdcard boot device for STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_sdcard TF_M_PLATFORM=stm/stm32mp257f_dk M33FW_DEVICETREE=stm32mp257f-dk-cm33tdcid-ostl m33fw
- E.g. for nor-sdcard boot device for STM32MP257F-EV1
make -f $PWD/../Makefile.sdk.stm32mp2-m33td TF_M_CONFIG=m33td_nor-sdcard TF_M_PLATFORM=stm/stm32mp257f_ev1 M33FW_DEVICETREE=stm32mp257f-ev1-cm33tdcid-ostl m33fw
  • Go to the directory where the compilation results are stored
cd $M33FW_DEPLOYDIR_ROOT
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the secondary stage boot loader that contains the m33 firmware: m33ddr-a and m33fw-a
ls -l /dev/disk/by-partlabel/ | grep 'm33.*-a'
lrwxrwxrwx 1 root root 10 Feb  8 08:57 m33ddr-a -> ../../sdb7
lrwxrwxrwx 1 root root 10 Feb  8 08:57 m33fw-a -> ../../sdb9
  • Copy the m33 firmware to the dedicated partition
dd if=ddr_phy-<device tree>-<m33 boot device>_Signed.bin of=/dev/sdb7 bs=1M conv=fdatasync
dd if=tfm-starterapp-<device tree>-<m33 boot device>-<a35 boot device>_s_ns_Signed.bin of=/dev/sdb9 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb7 or /dev/sdb9:
sudo chmod 777 /dev/sdb5
  • Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset

11. Modifying the m33tdprojects Starter[edit | edit source]

  • Go to the m33tdprojects Starter source directory
cd <m33tdprojects Starter source directory>
  • Get the list of supported configurations with the following command
make -f $PWD/../Makefile.sdk.stm32mp2-m33td help
  • m33tdprojects Starter firmware case building

The "M33FW_artifacts" folder should be specified to allow to update the M33 firmware with the new m33tdprojects Starter binary. When using the "SOURCES-xxxx.tar.gz" from Developer package the "M33FW_DEPLOYDIR_ROOT" var should be set as below:

export M33FW_DEPLOYDIR_ROOT=$PWD/../../M33FW_artifacts

Make sure to configure then the TF_M_BUILD_PATH path to point to TF-M build folder:

export TF_M_BUILD_PATH=<tf-m-stm32mp build dir>
  • Cross-compile the m33tdprojects Starter to generate m33tdprojects Starter binary update:
- E.g. for sdcard boot device for STM32MP215F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp215f-dk-cm33tdcid-ostl m33td
- E.g. for sdcard boot device for STM32MP257F-DK for STM32MP23x lines evaluation
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp235f-dk-cm33tdcid-ostl m33td
- E.g. for sdcard boot device for STM32MP257F-DK
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp257f-dk-cm33tdcid-ostl m33td
- E.g. for nor-sdcard boot device for STM32MP257F-EV1
make -f $PWD/../Makefile.sdk.stm32mp2-m33td clean
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_nor-sdcard M33FW_DEVICETREE=stm32mp257f-ev1-cm33tdcid-ostl m33td
  • To check build results, go to the directory where the compilation results are stored
cd $M33FW_DEPLOYDIR_ROOT/m33-projects
  • M33 firmware case building
  • Cross-compile the m33tdprojects Starter to generate M33 firmwares update:

The TF-M binary should be available in ${M33FW_DEPLOYDIR_ROOT}/arm-trusted-firmware-m folder

- E.g. for sdcard boot device for STM32MP215F-DK
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp215f-dk-cm33tdcid-ostl m33fw
- E.g. for sdcard boot device for STM32MP257F-DK for STM32MP23x lines evaluation
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp235f-dk-cm33tdcid-ostl m33fw
- E.g. for sdcard boot device for STM32MP257F-DK
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_sdcard M33FW_DEVICETREE=stm32mp257f-dk-cm33tdcid-ostl m33fw
- E.g. for nor-sdcard boot device for STM32MP257F-EV1
make -j1 -f $PWD/../Makefile.sdk.stm32mp2-m33td DEPLOYDIR=$PWD/../deploy M33FW_CONFIG=m33td_nor-sdcard M33FW_DEVICETREE=stm32mp257f-ev1-cm33tdcid-ostl m33fw
  • Go to the directory where the compilation results are stored
cd $M33FW_DEPLOYDIR_ROOT
  • Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot:  0 
STM32MP> 
  • Connect a USB cable between the host machine and the board via the USB OTG ports
  • In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
Information
For more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot
  • On the host machine, check the partition associated with the secondary stage boot loader that contains the m33 firmware: m33ddr-a and m33fw-a
ls -l /dev/disk/by-partlabel/ | grep 'm33.*-a'
lrwxrwxrwx 1 root root 10 Feb  8 08:57 m33ddr-a -> ../../sdb7
lrwxrwxrwx 1 root root 10 Feb  8 08:57 m33fw-a -> ../../sdb9
  • Copy the m33 firmware to the dedicated partition
dd if=ddr_phy-<device tree>-<m33 boot device>_Signed.bin of=/dev/sdb7 bs=1M conv=fdatasync
dd if=tfm-starterapp-<device tree>-<m33 boot device>-<a35 boot device>_s_ns_Signed.bin of=/dev/sdb9 bs=1M conv=fdatasync
Information
In case you get a permission denied you can set more permission on /dev/sdb7 or /dev/sdb9:
sudo chmod 777 /dev/sdb5
  • Reset the U-Boot shell: In the U-Boot shell, press Ctrl+C prior to get hand back.
STM32MP> reset

12. Adding a "hello world" user space example[edit | edit source]

Thanks to the OpenSTLinux SDK, it is easy to develop a project outside of the OpenEmbedded build system. This chapter shows how to compile and execute a simple "hello world" example.

12.1. Source code file[edit | edit source]

  • Go to the working directory that contains all the source codes (i.e. directory that contains the Linux kernel, OP-TEE OS, TF-A and U-Boot source code directories)
cd <tag>/sources/<arm architecture>-<distro>-linux*
  • Create a directory for this user space example
mkdir hello_world_example
cd hello_world_example
  • Create the source code file for this user space example: hello_world_example.c
// SPDX-identifier: GPL-2.0
/*
 * Copyright (C) STMicroelectronics SA 2018
 *
 * Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
 *
 */

#include <stdio.h>
#include <unistd.h>

int main(int argc, char **argv)
{
	int i =11;

	printf("\nUser space example: hello world from STMicroelectronics\n");
	setbuf(stdout,NULL);
	while (i--) {
		printf("%i ", i);
		sleep(1);
	}
	printf("\nUser space example: goodbye from STMicroelectronics\n");

	return(0);
}

12.2. Cross-compilation[edit | edit source]

Three ways to use the OpenSTLinux SDK to cross-compile this user space example are proposed below: (1) command line (2) makefile-based project (3) autotools-based project.

12.2.1. Command line[edit | edit source]

This method allows quick cross-compilation of a single-source code file. It applies if the project has only one file.
The cross-development toolchain is associated with the sysroot that contains the header files and libraries needed for generating binaries that run on the target architecture (see SDK for OpenSTLinux distribution#Native and target sysroots).
The sysroot location is specified with the --sysroot option.

The sysroot location must be specified using the --sysroot option. The CC environment variable created by the SDK already includes the --sysroot option that points to the SDK sysroot location.

echo $CC
arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
  • Create the directory in which the generated binary is to be stored
mkdir -p install_artifact install_artifact/usr install_artifact/usr/local install_artifact/usr/local/bin
  • Cross-compile the single source code file for the user space example
$CC hello_world_example.c -o ./install_artifact/usr/local/bin/hello_world_example

12.2.2. Makefile-based project[edit | edit source]

For this method, the cross-toolchain environment variables established by running the cross-toolchain environment setup script are subject to general make rules.
For example, see the following environment variables:

echo $CC
arm-ostl-linux-gnueabi-gcc -march=armv7ve -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
echo $CFLAGS
-O2 -pipe -g -feliminate-unused-debug-types
echo $LDFLAGS
-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed
echo $LD
arm-ostl-linux-gnueabi-ld --sysroot=<SDK installation directory>/SDK/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
  • Create the makefile for this user space example: Makefile
Information
All the indentations in a makefile are tabulations
PROG = hello_world_example
SRCS = hello_world_example.c
OBJS = $(SRCS:.c=.o)

CLEANFILES = $(PROG)
INSTALL_DIR = ./install_artifact/usr/local/bin

# Add / change option in CFLAGS if needed
# CFLAGS += <new option>

$(PROG):  $(OBJS)
	$(CC) $(CFLAGS) -o $(PROG) $(OBJS)

.c.o:
	$(CC) $(CFLAGS) -c $< -o $@

all: $(PROG)
 
 
clean:
	rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS)) *~

install: $(PROG)
	mkdir -p $(INSTALL_DIR)
	install $(PROG) $(INSTALL_DIR)
  • Cross-compile the project
make
make install

12.2.3. Autotools-based project[edit | edit source]

This method creates a project based on GNU autotools.

  • Create the makefile for this user space example: Makefile.am
bin_PROGRAMS = hello_world_example
hello_world_example_SOURCES = hello_world_example.c
  • Create the configuration file for this user space example: configure.ac
AC_INIT(hello_world_example,0.1)
AM_INIT_AUTOMAKE([foreign])
AC_PROG_CC
AC_PROG_INSTALL
AC_OUTPUT(Makefile)
  • Generate the local aclocal.m4 files and create the configure script
aclocal
autoconf
  • Generate the files needed by GNU coding standards (for compliance)
touch NEWS README AUTHORS ChangeLog
  • Generate the links towards SDK scripts
automake -a
                       
  • Cross-compile the project
./configure ${CONFIGURE_FLAGS}
make
make install DESTDIR=./install_artifact

12.3. Deploy and execute on board[edit | edit source]

  • Check that the generated binary for this user space example is in: ./install_artifact/usr/local/bin/hello_world_example
  • Push this binary onto the board
scp -r install_artifact/* root@<board ip address>:/
  • Execute this user space example
cd /usr/local/bin
./hello_world_example 

User space example: hello world from STMicroelectronics
10 9 8 7 6 5 4 3 2 1 0 
User space example: goodbye from STMicroelectronics