Last edited 4 weeks ago

OpenSTLinux expansion packages

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

OpenSTLinux expansion packages can be combined with STM32 MPU Yocto-based OpenSTLinux embedded software to enable the use of additional components for a specific feature such as AI-based computer vision, real-time Linux, or GNSS applications. X-LINUX components can be used as software add-ons only or may be combined with hardware shields, such as NFC expansion boards.
The X-LINUX part numbers are offered and maintained by ST, and I-LINUX part numbers are developed and maintained by partners and third parties.


OpenSTLinux_expansion_packages


Part number Supplier Supported devices Supported boards Latest supported ecosystem release[1]
X-LINUX-AI
to demonstrate AI-based computer vision applications
ST STM32MP1 series
STM32MP2 series
STM32MP1 series' boards
STM32MP2 series' boards
ecosystem release v6.2.0
X-LINUX-AWS
to enable the development of your IoT solution by bringing AWS IoT Greengrass[2] software in the Linux® kernel
ST STM32MP13x lines 
STM32MP25x lines 
STM32MP135F-DK
STM32MP257F-EV1
ecosystem release v6.0.0
X-LINUX-AZURE
to enable the development of your IoT solution by bringing Microsoft® Azure® IoT Edge[3] software in the Linux® kernel
ST STM32MP13x lines 
STM32MP25x lines 
STM32MP135F-DK
STM32MP257F-EV1
ecosystem release v6.0.0
X-LINUX-GNSS1
to demonstrate GNSS-based applications
ST STM32MP13x lines 
STM32MP15x lines 
STM32MP135F-DK
STM32MP157F-DK2
ecosystem release v4.0.0
X-LINUX-IOT01E/A
to demonstrate SPIRIT1 and LSM6DSOX-based applications
ST STM32MP13x lines 
STM32MP15x lines 
STM32MP135F-DK
STM32MP157F-DK2
ecosystem release v3.1.0
X-LINUX-ISP
to demonstrate a free-of-charge open-source software package providing Image Signal Processing (ISP) image quality software in the Linux® kernel
ST STM32MP25x lines  STM32MP257F-EV1 ecosystem release v6.2.1
X-LINUX-MEMS1
to demonstrate MEMS sensor fusion-based applications
ST STM32MP13x lines 
STM32MP15x lines 
STM32MP135F-DK
STM32MP157F-DK2
ecosystem release v4.1.0
X-LINUX-NFC5
to demonstrate RFAL-based NFC applications
ST STM32MP15x lines  STM32MP157F-DK2 ecosystem release v3.0.0
X-LINUX-NFC6
to demonstrate RFAL-based NFC applications
ST STM32MP15x lines  STM32MP157F-DK2 ecosystem release v3.0.0
X-LINUX-PREDMNT
to demonstrate predictive maintenance applications
ST STM32MP15x lines  STM32MP157F-DK2 ecosystem release v2.1.0
I-LINUX-Qt
90-day evaluation of Qt Design Studio and Qt Device Creation Enterprise licenses

(Qt commercial trial offer to test it on the STM32MP25 product).

Qt STM32MP25 STM32MP257F-DK
STM32MP257F-EV1
ecosystem release v6.2.0
X-LINUX-QT
to demonstrate Qt framework feature in the Linux® kernel

(Limited to the Qt open-source framework, this offer provides the possibility to develop Qt applications under GPL or LGPL terms. Please refer to Qt for Open Source Development for details.)

ST STM32MP257 line 
STM32MP255 line 
STM32MP157F-DK2 STM32MP135F-DK STM32MP257F-DK STM32MP257F-EV1 ecosystem release v6.2.0
X-LINUX-RT
to demonstrate the real-time (RT) feature in the Linux® kernel
ST STM32MP13x lines 
STM32MP15x lines 
STM32MP25x lines 
STM32MP1 series' boards
STM32MP257F-EV1
ecosystem release v6.2.0
X-LINUX-TPM
to demonstrate TPM feature in the Linux® kernel
ST STM32MP1 series
STM32MP257 line 
STM32MP157F-DK2
STM32MP135F-DK
STM32MP257F-DK
STM32MP257F-EV1
ecosystem release v6.2.0
X-LINUX-TSNSWCH
to demonstrate the real-time (RT) feature in the Linux® kernel
ST STM32MP257 line  STM32MP257F-EV1 ecosystem release v6.2.1
  1. ↑ If the latest supported ecosystem release for the expansion package (e.g., ecosystem release v4.0.0 ) is not the latest delivered ecosystem release (ecosystem release v6.2.1 ), then adaptations might be needed for this expansion package be built and executed on this latest delivered release.
  2. ↑ AWS IoT Greengrass
  3. ↑ Microsoft® Azure® IoT Edge