Last edited 5 months ago

STM32MP2 PWR internal peripheral

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


1. Article purpose[edit | edit source]

The purpose of this article is to:

  • briefly introduce the PWR peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit | edit source]

The power control (PWR) peripheral is used to control the device power supply configuration, and the control of the supply configuration.

PWR controls, according the the operating mode, and monitors the main supply (VDD, VDDCPU, VDDCORE, ...) and the independent voltage supplies, including the I/O supply (VDDIO) for peripherals eMMC and SD-Card.

It has 6 input pins (named wakeup pins) which can be programmed to wake the system up from low power. The wakeup pins are listed with WKUP prefix in the STM32 MPU Datasheets.

PWR is a RIF-aware peripheral. Each PWR feature could be assigned to the different execution context of the platform following firewall rules described in Resource Isolation Framework overview.

In the case a wakeup pin shall be used by the Cortex®-A35 non secure, it should be assigned to Cortex®-A35 that will forward wake-up event via secure services.

In addition the PWR peripheral drives 3 output hardware lines named PWR_ON, PWR_LP and PWR_CPU_ON according to platform low power mode:

  • with STPMIC (STPMIC25 or STPMIC2L), all 3 lines are used and may control regulators state depending on STPMIC configuration.
  • in the power discrete solution they drive VDDcore which feeds the peripherals. They also control the DDR power supplies (VDD_DDR, VREF_DDR, VTT_DDR) and VDDCpu that feeds the processor.

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit | edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the FwST-M Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit | edit source]

3.1.1. On STM32MP2 series[edit | edit source]

3.1.1.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the PWR instance on STM32MP2 series for A35-TD flavor .

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Voltage monitoring
RAM & low power
CPU1 power control ✓
CPU2 power control
CPU3 power control Only on STM32MP25x lines 
VDDIO eMMC ☐ ⬚
VDDIO SD ☐ ⬚
Wake up 1
Wake up 2
Wake up 3
Wake up 4
Wake up 5
Wake up 6
3.1.1.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the PWR instance on STM32MP2 series for M33-TD flavor ..

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
Voltage monitoring
RAM & low power
CPU1 power control ✓
CPU2 power control ✓
CPU3 power control Only on STM32MP25x lines 
VDDIO eMMC ☐ ⬚ ☐
VDDIO SD ☐ ⬚ ☐
Wake up 1
Wake up 2
Wake up 3
Wake up 4
Wake up 5
Wake up 6

3.2. Runtime assignment[edit | edit source]

3.2.1. On STM32MP21x lines [edit | edit source]

3.2.1.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP21 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP21 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP21x lines  for A35-TD flavor .

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Voltage monitoring ☑OP-TEE ⬚ ⬚ ⬚
RAM & low power ☑TF-A BL31 ⬚ ⬚ ⬚
CPU1 power control ☑TF-A BL31 ⬚
CPU2 power control ☐TFA BL31 ☐ if TZ_EN ☐ if TZ_DIS Managed by TF-A when CPU2 (Cortex-M33) is in reset
VDDIO eMMC ☑OP-TEE ⬚ ⬚ ⬚
VDDIO SD ☑OP-TEE ⬚ ⬚ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☐OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐
3.2.1.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP21 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP21 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP21x lines  for M33-TD flavor .

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Voltage monitoring ⬚OP-TEE ⬚ ☐ ⬚
RAM & low power ⬚TF-A BL31 ⬚ ☑ ⬚
CPU1 power control ☑TF-A BL31 ⬚ ☐ Managed by TF-M when CPU1 (Cortex-A35) is in reset
CPU2 power control ☑ ⬚
VDDIO eMMC ⬚OP-TEE ⬚ ☑ ⬚
VDDIO SD ⬚OP-TEE ⬚ ☑ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☐OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐

3.2.2. On STM32MP23x lines [edit | edit source]

3.2.2.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP23 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP23 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP23x lines  for A35-TD flavor .

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Voltage monitoring ☑OP-TEE ⬚ ⬚ ⬚
RAM & low power ☑TF-A BL31 ⬚ ⬚ ⬚
CPU1 power control ☑TF-A BL31 ⬚
CPU2 power control ☐TF-A BL31 ☐ if TZ_EN ☐ if TZ_DIS Managed by TF-A when CPU2 (Cortex-M33) is in reset
VDDIO eMMC ☑OP-TEE ⬚ ⬚ ⬚
VDDIO SD ☑OP-TEE ⬚ ⬚ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☐OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐
3.2.2.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP23 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP23 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP23x lines  for M33-TD flavor .

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Voltage monitoring ⬚OP-TEE ⬚ ☐ ⬚
RAM & low power ⬚TF-A BL31 ⬚ ☑ ⬚
CPU1 power control ☑TF-A BL31 ⬚ ☐ Managed by TF-M when CPU1 (Cortex-A35) is in reset
CPU2 power control ☑ ☐
VDDIO eMMC ⬚OP-TEE ⬚ ☑ ⬚
VDDIO SD ⬚OP-TEE ⬚ ☑ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☑OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐

3.2.3. On STM32MP25x lines [edit | edit source]

3.2.3.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP25x lines  for A35-TD flavor ..

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Voltage monitoring ☑OP-TEE ⬚ ⬚ ⬚
RAM & low power ☑TF-A BL31 ⬚ ⬚ ⬚
CPU1 power control ☑TF-A BL31 ⬚
CPU2 power control ☐TF-A BL31 ☐ if TZ_EN ☐ if TZ_DIS Managed by TF-A when CPU2 (Cortex-M33) is in reset
CPU3 power control ☐TF-A BL31 ⬚ ☐ ☐
VDDIO eMMC ☑OP-TEE ⬚ ⬚ ⬚
VDDIO SD ☑OP-TEE ⬚ ⬚ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☐OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐
3.2.3.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Power & Thermal PWR PWR Shareable at internal peripheral level thanks to the RIF:
see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the PWR instance on STM32MP25x lines  for M33-TD flavor ..

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Voltage monitoring ⬚OP-TEE ⬚ ☐ ⬚
RAM & low power ⬚TF-A BL31 ⬚ ☑ ⬚
CPU1 power control ☑TF-A BL31 ⬚ ☐ Managed by TF-M when CPU1 (Cortex-A35) is in reset
CPU2 power control ☑ ☐
CPU3 power control ☐TF-A BL31 ⬚ ☐ ☐
VDDIO eMMC ⬚OP-TEE ⬚ ☑ ⬚
VDDIO SD ⬚OP-TEE ⬚ ☑ ⬚
Wake up 1 ☐OP-TEE ⬚ ☐ ☐
Wake up 2 ☐OP-TEE ⬚ ☐ ☐
Wake up 3 ☐OP-TEE ⬚ ☐ ☐
Wake up 4 ☐OP-TEE ⬚ ☐ ☐
Wake up 5 ☐OP-TEE ⬚ ☐ ☐
Wake up 6 ☐OP-TEE ⬚ ☐ ☐

4. Software frameworks and drivers[edit | edit source]

Below are listed the software frameworks and drivers managing the PWR peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit | edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:

  • partial device trees (pin control and clock tree) for the OpenSTLinux software components,
  • HAL initialization code for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

6. How to go further[edit | edit source]

STM32MP2 power overview shows the usage of PWR drivers in OpenSTlinux power management.

7. References[edit | edit source]