Last edited 2 years ago

Dpkg

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


1. Article purpose[edit | edit source]

This article aims to give information required to start with the Linux tool: dpkg[1]

2. Introduction[edit | edit source]

dpkg is the basic tool to deal with this package manager. A package manager is helpful for installing, removing and updating package in the rootfs.

A package is an archive with .deb extension that contains a set of files but also a set of installing/removing scripts.

Any package provides two kind of artifacts:

  • metadata: collection of scripts and configs needs to correctly install data of the package
  • data: applications, libraries, and any files to copy to the rootfs


3. Getting Started[edit | edit source]

dpkg can be very helpful to know which file of the rootfs belongs to which package.

Keep in mind that the OpenSTLinux distribution has been generated with OpenEmbedded. There is a direct parity between 'recipes' and 'packages'.

Indeed an OpenEmbedded recipe describes how to get sources code, how to compile it, where to install built artifacts on filesystem and also which 'dpkg' packages to create and which files to put in.

That is why it can be very interesting to list the files that belong to a package or to find a package that belongs to a file.

Here a short list of useful commands with 'dpkg':

  • How to list the currently installed packages
dpkg -l
  • How to install a package:
dpkg -i <packageName>.deb
  • How to remove/uninstalling a package
dpkg -r <packageName>
  • How to list files of a package
dpkg -L <packageName>
  • How to find a package that belongs to a file
dpkg -S </absolute/path/to/a/file/of/target>

4. References[edit | edit source]