Last edited 4 months ago

STM32DDRFW-UTIL

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. STM32DDRFW-UTIL overview[edit | edit source]

This article describes STM32DDRFW-UTIL, an official STMicroelectronics firmware package for DDR configuration and test on STM32 Arm® Cortex® MPUs .

1.1. Package overview[edit | edit source]

STM32DDRFW-UTIL firmware is a software package containing multiple STM32CubeIDE projects applicable for all STM32 MPU products, with a DDR which includes:

  • BSP, CMSIS and HAL drivers for all applicable STM32 Arm® Cortex® MPUs 
  • DDR_Tool full source code with:
    • "Common directory" with general purpose content,
    • "Tool directory" with tool core and tests,
    • STM32CubeIDE Projects for all supported ST boards,
  • Binaries for all supported ST boards with STM32 header for binary files to be programmed directly into microSDTM card or loaded via STM32CubeProgrammer without using STM32CubeIDE tool.
  • README.md document for help
Warning
Dependency with STM32CubeIDE release notified inside the delivery package for the projects ( possible compilation issues with other versions).

1.2. README.md[edit | edit source]

The README.md , included in the package, describes:

  • the software architecture and design of STM32DDRFW-UTIL.
  • how to use the STM32DDRFW-UTIL firmware package for DDR configuration and test on STM32 Arm® Cortex® MPUs .

2. How to get STM32DDRFW-UTIL[edit | edit source]

Refer to the following link "STM32DDRFW-UTIL" directory to find STM32DDRFW-UTIL firmware package.

STM32DDRFW-UTIL for Linux® and Windows® host PC
Download

Version v1.7.0

  • STM32DDRFW-UTIL firmware package is available: here .
Installing the STM32DDRFW-UTIL
  • To use STM32DDRFW-UTIL, unzip the package on computer..
  • Then refer to README.md , to use this tool .
Detailed release note
  • Full details about the content of this tool release are available here: Release_Notes.md .