Last edited one month ago

OpenBMC-based Linux ecosystem release note

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Ecosystem content[edit | edit source]

The OpenBMC-based Linux ecosystem releases aim at:

  • providing a full ecosystem for the STM32MP1 series and STM32MP2 series
  • working efficiently with STM32 MPU boards , using OpenBMC-based Linux embedded software provided by STMicroelectronics' partner.

This ecosystem release consists of:

  • Development tools
    • STM32CubeIDE
    • STM32CubeMX
    • Programming tools
      • STM32CubeProgrammer
        • Keygen tool
        • Signing tool
        • Trusted package creator tool
      • STM32PRG-TOOLBOX
        • STM32PRG-TOOLBOX-DFU
        • STM32PRG-TOOLBOX-FB

2. Scope of OpenBMC version based on OpenSTLinux BSP v6.2.0[edit | edit source]

The OpenBMC-based Linux-ecosystem OSTL-6.2.0_OBMC-2.18 release is dedicated to the STM32MP2 series.

2.1. Main changes[edit | edit source]

OpenBMC-based Linux ecosystem is provided by ST as example.

The main changes provided by the release are:

Visit the README.md#features-of-openbmc to discover main features coming with this release and foreseen for next releases.

2.2. Main restrictions[edit | edit source]

Visit the OpenBMC Bug Reporting to discover main restrictions coming with this release.

3. Intended audience[edit | edit source]

The targeted audience is STM32MP2 series customers and partners.

4. Licensing[edit | edit source]

All licenses corresponding to this OpenBMC-based Linux ecosystem are available here

5. Supported development boards[edit | edit source]

Two ST boards are included in the OpenBMC distribution as examples:

  • STM32MP257F-EV1 [1] that supports both eMMC and SNOR flash memories.
  • STM32MP257F-DK [2] that supports eMMC flash memory.

Supported ST boards are listed here

6. Embedded software[edit | edit source]

In the table below, for each STM32 MPU device, you can find on which Cortex® the embedded software are running.

Embedded software STM32MP21x lines  STM32MP23x lines  STM32MP25x lines 
OpenBMC for Arm® Cortex®-A Yes Cortex®-A35 Yes Cortex®-A35 Yes Cortex®-A35
FwST-M for Arm® Cortex®-M Yes Cortex®-M33 Yes Cortex®-M33 Yes Cortex®-M33
Yes Cortex®-M0
STM32DDRFW-UTIL for Arm® Cortex®-A Yes Cortex®-A35 Yes Cortex®-A35 Yes Cortex®-A35
STM32PRGFW-UTIL for Arm® Cortex®-A Yes Cortex®-A35 Yes Cortex®-A35 Yes Cortex®-A35
STM32MPUSSP-UTIL for Arm® Cortex®-A Yes Cortex®-A35 Yes Cortex®-A35 Yes Cortex®-A35

6.1. OpenBMC-based Linux embedded software[edit | edit source]

The OpenBMC-based Linux® embedded software is part of the STM32 MPU embedded software offer.
It is a set of software (see architecture overview) created to ease the integration of our STM32 MPU devices inside the OpenBMC[3] project.

It is made up of:

  • an open-source Linux® distribution, based on the OpenBMC community project, running on the Arm® Cortex®-A processor(s).
  • firmwares, running on the Arm® Cortex®-M processor: FwST-M Packages

OpenBMC[3] is a Linux operating system targeting embedded devices.OpenBMC includes a collection of applications and services that address BMC functional requirements. It is most commonly deployed on a companion chip paired with a server processor, where it provides a management interface between the administrator and the server. The BMC is also responsible for managing the chassis, firmware updates, sensor management, and access control.

The Linux® distribution relies on the OpenSTLinux board support package (U-Boot, TF-A, OP-TEE, Linux kernel) complemented with a user-space with a features set brought by OpenBMC.

The OpenBMC forked repository[4] is delivered on the official STMicroelectronics GitHub[5].


OpenBMC forked repositoryFwST-M PackagesLinux OpenBMC-based embedded software


6.1.1. OpenBMC-based Linux Distribution for Arm® Cortex®-A[edit | edit source]

Updated OpenBMC v2.18.0 is the version delivered with the OpenBMC-based Linux-ecosystem OSTL-6.2.0_OBMC-2.18.

The release note and readme files give information and details about the features / content / restrictions of the OpenBMC-based Linux Distribution.


Firmware Release note Version
OpenBMC Linux Distribution Readme file and ST readme.md OSTL-6.2.0_OBMC-2.18

6.1.2. FwST-M packages for Arm® Cortex®-M[edit | edit source]

The release notes give information and details about the features / content / restrictions of the Packages.

Since OpenBMC-based Linux ecosystem-v6.1.0, the TF-M is no more supported.

They do not explain how to download the software. For that, refer to How to download the software and start with this release chapter.

Firmware Release note Version
STM32CubeMP2 Package STM32CubeMP2 Package release note - v1.3.0 STM32CubeMP2 Package v1.3.0


7. Development tools[edit | edit source]

The tools version has to match the version of the ST BSP components, aka Yocto-based OpenSTLinux BSP v6.2.0, available in Yocto-based OpenSTLinux ecosystem release note - v6.2.0#Development tools.

8. Documentation[edit | edit source]

To discover the detailed explanation on this release content and to learn how to use it, refer to the OpenBMC "Docs" repository

You can also find visit this page Category:STM32 MPU technical literature ; and selecting the relevant STM32 MPU documentation set, you will have access to all information related to the full ecosystem.

9. How to download the software and start with this release[edit | edit source]

Refer to OpenBMC-based Linux embedded software article.


10. References[edit | edit source]