An STM32 MPU ecosystem is composed of:
- embedded software (distributions and packages),
- STM32 MPU boards,
- set of developments tools,
- set of documents.
This category regroups all release notes constituting the different STM32 MPU ecosystems provided in this wiki (for the v6 flow - v6.y.z ecosystem releases).
There are 2 STM32 MPU ecosystem flagships:
- the Yocto-based OpenSTLinux ecosystem, whose embedded software running on Arm® Cortex®-A processor(s) is a Linux® distribution. The other Linux-based ecosystems align their embedded software on the BSP of this Yocto-based OpenSTLinux ecosystem.
- the bare metal - RTOS ecosystem, whose embedded software running on Arm® Cortex®-A processor(s) is a STM32Cube MPU package (similar to the well-known the STM32 MCU packages for STM32 MCU series) with a RTOS or without (bare metal).
Below are listed all STM32 MPU ecosytems provided in this wiki and pointing on their associated release notes
| STM32 MPU ecosystems | Suppliers | Supported devices | Last ecosystem release note | For Linux-based ecosystems, version of the last ported OSTL BSP | |
|---|---|---|---|---|---|
| ST | STM32MP1 series STM32MP2 series |
Yocto-based OpenSTLinux ecosystem release note | v6.2.1 | ||
| ST | STM32MP13x lines |
STM32CubeMP13 bare metal - RTOS ecosystem release note | Not applicable | ||
| ST | STM32MP25x lines |
Android-based OpenSTDroid ecosystem release note | v6.2.1 | ||
| ST | STM32MP25x lines |
OpenBMC-based Linux ecosystem release note | v6.2.0 | ||
| via partner | STM32MP1 series STM32MP2 series |
Buildroot-based Linux ecosystem release note | v6.2.0 | ||
| via partner | STM32MP1 series STM32MP2 series |
OpenWrt-based Linux ecosystem release note | v6.1.0 | ||
The former release notes of the STM32 MPU ecosystems are stored in the STM32 MPU ecosystems release notes archives category.
Subcategories
This category has only the following subcategory.
Pages in category "STM32 MPU ecosystems release notes"
The following 6 pages are in this category, out of 6 total.