OpenSTLinux developer packages

This category groups together all articles related to the developer packages proposed to add your own developments on top of the Yocto-based OpenSTLinux embedded software (whatever the microprocessor device). These developer packages provide the software development kit (SDK), and the source code of the OpenSTLinux board support packages (BSPs), for the different STM32 MPU series.

"OpenSTLinux" is used here as a shortcut for "Yocto-based OpenSTLinux embedded software". However, it is important to note that, for STM32MP15x lines  and STM32MP2 series, the developer packages also provide the STM32Cube MPU package source code.


Pages in category "OpenSTLinux developer packages"

This category contains only the following page.