Last edited 10 months ago

STM32CubeMP13 Package - Getting started

Applicable for STM32MP13x lines


1. Step by step approach[edit | edit source]

The STM32CubeMP13 package is part of the STM32 MPU embedded software offer. It runs on the Arm® Cortex®-A7 core.

This article shows how to start up a STM32MP135x-DK Discovery kit (flexible and complete development platform for the STM32MP13x lines ) with the STM32CubeMP13 package. It is valid for STM32MP135F-DK Discovery kit : the part numbers are specified in the STM32MP13 microprocessor part numbers article.

It lists the required material, points to the board features description, and gives the step-by-step process to set up the system.

Finally, it explains how to develop, build and run existing or new examples to discover some of the board capabilities.

The steps to get the STM32MP135x-DK Discovery kit up and running, are:
☐ Checking the material
☐ Assembling the board
☐ Installing tools : Installing the components to develop software running Arm® Cortex®-A7 with STM32CubeMPU Package

• Installing STM32CubeIDE (mandatory for any development on Arm® Cortex®-A7)
• Installing the STM32CubeMX (optional only if you plan to use graphical user interface that guides you through the initial configuration of a firmware project.)
• Installing the STM32CubeMPU Package (mandatory)

Once the board is assembled and the required tools and software are installed on the host PC, there are different ways (Boot switch configuration) to load the firmware into the Arm® Cortex®-A7 core:

  • the serial boot mode (forced USB or UART boot for programming firmware on a virgin device through a serial interface)
  • the developer boot mode (the firmware is loaded from the IDE).
  • the microSD™ card boot mode (the firmware is loaded from a programmed microSD™ card)

Different boot modes are to be used depending on the development or production phase. The developer boot mode is used during development to connect to the debugger and to use the IDE.

Other boot modes are used during production phase for programming images into target or boot from external memory.

2. Checking the material[edit | edit source]

Mandatory

PC Linux® or Windows® operating systems. See PC prerequisites for more details on the required configurations.
STM32MP135x-DK Discovery kit Flexible and complete development platform for the STM32MP135 microprocessor device including:
  • an MB1635 mother board
Power supply Including:
  • a USB Type-C® cable (included in the packaging)
  • a USB Type-C® charger (5 V, 3 A) (not included in the packaging)
microSD™ card

Populated with STM32CubeMPU firmware, the microSD™ card can be used as external memory to populate firmware into board

USB Micro-B cable To connect the STM32MP135x-DK Discovery kit to the PC through the USB Micro-B (ST-LINK/V2-1) connector.
USB Type-C® cable To connect the STM32MP135x-DK Discovery kit to a USB OTG device through the USB Type-C® connector.


Optional

USB keyboard and mouse Through its USB Type-A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse.
Ethernet cable To connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector.

Optional: It is possible to plug more devices and extension boards to the STM32MP135x-DK Discovery kit by means of its expansion connectors such as the GPIO expansion connector.


The following figure shows the optional material (not included in STM32MP135x-DK Discovery kit package).

Recommended material for this Starter Package

3. Assembling the board[edit | edit source]

The STM32MP135F-DK Discovery kit package is composed of the items listed below.

Position Description
1 MB1635 mother board
2 MB1897 camera module (GalaxyCore GC2145 camera sensor)
3 Camera module flat cable
4 microSD™ card

Note that the STM32MP135F-DK Discovery kit delivery does not contain a USB cable or a USB charger.


STM32MP135F-DK Discovery kit assembled.
(picture is not contractual)




4. Installing tools[edit | edit source]

This section is for installing the components required to develop software running on Arm® Cortex®-A7 with STM32CubeMPU package.

4.1. Installing STM32CubeIDE[edit | edit source]

It is needed if you want to run existing examples or modify or add software running on Arm® Cortex®-A7.

The table below explains how to download and install STM32CubeIDE which addresses STM32 MCU, and also provides support for Cortex-A7 inside STM32 MPU.

STM32 MPU support, inside STM32CubeIDE, is available on Linux® and Windows® host PCs, but it is NOT on macOS®.

STM32CubeIDE for Linux® host PC STM32CubeIDE for Windows® host PC
Download

Version v2.2.0

  • Download the preferred all-in-one Linux installer from st.com
    • Generic Linux Installer - STM32CubeIDE-Lnx
    • RPM Linux Installer - STM32CubeIDE-RPM
    • Debian Linux Installer - STM32CubeIDE-DEB

Version v2.2.0

  • Download the all-in-one Windows installer from st.com
    • Windows Installer - STM32CubeIDE-Win
Installation guide
  • Refer to STM32CubeIDE installation guide (UM2563) available on st.com.
User manual
  • When the installation is completed, see additional information about STM32CubeIDE in st.com:
    • STM32CubeIDE quick start guide (UM2553)
Detailed release note
  • Details about the content of this tool version are available in the STM32CubeIDE release v2.2.0 release note from st.com
Restrictions Main restrictions are identified in this chapter
  • STM32CubeIDE errata( This page is hosted in the STM32 MCU wiki. Selecting the link opens a new tab. Be aware that visiting this page leaves the STM32 MPU wiki)

Minor releases may be available from the update site. Check chapter 10 in (UM2609) for more information on how to update STM32CubeIDE.


4.2. Installing STM32CubeMX[edit | edit source]

Optional step: This is required only if developer wants to use STM32CubeMX for initial configuration of firmware project. Refer to STM32CubeMX release note for more details.

5. Installing the STM32CubeMPU Package[edit | edit source]

Prerequisite: the STM32CubeIDE is installed.


  • The STM32CubeMP13 Package is delivered through an archive file named en.stm32cubemp13-v1-2-0.zip.

  • Download and install the STM32CubeMP13 Package

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32CubeMP13 Package - v1.2.0 release
From st.com From github
Download
  • Go on st.com to download the en.stm32cubemp13-v1-2-0.zip file.
Installation
  • Go to the host PC directory in which you want to install the Package
  • Uncompress the archive file to get the STM32CubeMP13 Package
  • Installation of package can be done in two ways:
    • Download ZIP (en.stm32cubemp13-v1-2-0.zip)
    • Clone the git repo
Release note Details about the content of the STM32CubeMP13 Package are available in STM32CubeMP13 Package content article and in the Release_Notes.html file.
STM32Cube_FW_MP13_V1.2.0		STM32CubeMP13 Package: details in STM32CubeMP13 Package content article
├── Drivers
│   ├── BSP				BSP drivers for the supported STM32MP13 boards
│   │   └── [...]
│   ├── CMSIS
│   │   └── [...]
│   └── STM32MP13xx_HAL_Driver		HAL drivers for the supported STM32MP13 devices
│       └── [...]
├── _htmresc
│   └── [...]
├── License.md
├── Middlewares
│   └── [...]
├── package.xml
├── Projects
│   ├── STM32CubeProjectsList.html	List of examples and applications for STM32CubeMP13 Package
│   ├── STM32MP135C-DK			Set of examples and applications → STM32MP13 Discovery kits
│   │   └── [...]
│   └── STM32MP13XX_CUSTOM_HW		Set of examples and applications → STM32MP13 Custom boards
│       └── [...]
├── Readme.md
├── Release_Notes.html			Release note for STM32CubeMP13 Package
└── Utilities
    └── [...]


The STM32CubeMPU Package is now installed: let's develop software running on Arm® Cortex®-A7.

6. Playing with STM32CubeMPU Package[edit | edit source]

All examples and applications, explained below, have been designed to run on a STM32MP135F-DK Discovery kit integrating an STM32MP135C line .

Prerequisites

  • STM32CubeMP13 Package and the STM32CubeIDE are installed on your host PC
  • ST-Link cable is connected between your host PC and your board.

It is recommended to use the developer boot mode when developing or debugging an application running on the Arm® Cortex®-A7 core. Selection of developer boot mode is described in Select boot mode chapter.

This chapter and its sub-chapters explain all steps needed to run an existing example or application using STM32CubeIDE. Once done, you can jump to the chapter How to go further to enhance your experience with the STM32CubeMP13 package.


6.1. How to run existing examples on Arm Cortex-A7[edit | edit source]

This section explains how to build and execute examples using STM32CubeIDE.

Information
  • You can also find lot of additional useful information in STM32CubeIDE article

6.1.1. As bare metal[edit | edit source]

Bare metal means that the hardware resources are managed by the user application itself without an intervening operating system, such as Azure RTOS.

6.1.1.1. Select the example to run[edit | edit source]

First select the example to be run from the package below.

├── Projects
│   ├── STM32MP135C-DK			->Set of examples → STM32MP13 Discovery kits
│   ├── [Applications]
│   ├── [Examples]
│   ├── [External_Loader]
│   ├── [Templates]
Important
  • STM32MP135C-DK,used above and here after, means finally STM32MP135F-DK Discovery kit
6.1.1.2. Build the example[edit | edit source]
  • Open the folder containing the example and double-click on file .project to open STM32CubeIDE:

  • The directory layout of project containing the example appears like this, in STM32CubeIDE:

  • Click on "Hammer" button to build the example:

6.1.1.3. Select boot mode[edit | edit source]

For flashing images onto your board with STM32CubeIDE, developer boot mode is required. For that, boot switches must be set in a specific configuration, defined here.

6.1.1.4. Read the README file carefully[edit | edit source]

A readme file exists for any example and is available in the folder associated with the example. It provides all the information about the example setup and verdict.

6.1.1.5. Download and run an example from SYSRAM[edit | edit source]
  • Open the Debug Configurations panel:

  • Configure the Main panel to add the firmware binary:

  • Configure the Debugger & Startup panel to load and run the firmware in the target:

  • Expected verdict of an example is given in associated Readme file.

6.1.2. Integrating middleware's[edit | edit source]

Below is the approach to build and run middleware applications, for example, Azure RTOS, FreeRTOS™, and LwIP.

6.1.2.1. Select the application to run[edit | edit source]

First, select the application to run from the package below.

├── Projects
│   ├── STM32MP135C-DK			->Set of applications → STM32MP13 Discovery kits
│   ├── [Applications]
│   ├── [Examples]
│   ├── [External_Loader]
│   ├── [Templates]
Important
  • STM32MP135C-DK,used above and here after, means finally STM32MP135F-DK Discovery kit .
6.1.2.2. Build the application[edit | edit source]
  • Open the folder containing the application and double-click on file .project:

  • The directory layout of project containing the example appears like this, in STM32CubeIDE:

Important
  • It is recommended to switch to DDR in case application size exceeds SYSRAM size.
  • All delivered applications are built to be run from DDR. To execute from DDR , add USE_DDR flag in .cproject file. This flag is already set in the delivered STM32CubeMP13 package.
  • Click on "Hammer" button to build the application:

6.1.2.3. Select boot mode[edit | edit source]

For flashing images onto your board with STM32CubeIDE, developer boot mode is required. For that, boot switches must be set in a specific configuration, defined here.

6.1.2.4. Read the README file carefully[edit | edit source]

A readme file exists for any application and is available in the folder associated with the application. It provides all the information about the application setup and verdict.

6.1.2.5. Initialize the DDR[edit | edit source]

DDR Initialization is a prerequisite to download and run applications from DDR memory. Effectively, DDR needs to be initialized first with the DDR_Init project.

  • Open the folder containing the DDR_Init example and double-click on the .project file to open STM32CubeIDE:

  • Follow the same steps mentioned in the Build the application section to build, download, and run the DDR_Init example.
  • After executing the example, DDR is successfully initialized. This can be validated by referring to the 'Readme' of DDR_Init example.
6.1.2.6. Download and run an application from DDR[edit | edit source]

Prerequisite: DDR must be initialized (refer to Initialize the DDR chapter if not already done). The project should be compiled and linked for DDR (refer to Build application for DDR). After successful completion of DDR initialization, follow the steps mentioned below:

  • Open the Debug Configurations panel:

  • Configure the Main panel to add the firmware binary:

  • Configure the Debugger panel:

  • Configure the Startup' panel and remove monitor reset or mon reset command. This is done to avoid reset of DDR clock, initialized by DDR_Init example.

  • Download and run the firmware in the target:

  • Readme should be checked for expected verdict of the application.

6.2. How to go further[edit | edit source]

6.2.1. How to develop and run your examples or applications[edit | edit source]

6.2.1.1. Create your project for your board[edit | edit source]

A project is board and application specific. To create a new project, you start either from the template project or any available project from examples or applications.

Information
Information
The Template project provides empty main loop function. It is also a good starting point to get familiar with the STM32CubeMP13 project settings.

The template project has the following characteristics:

  • It contains the source code of HAL, CMSIS, and BSP drivers, which are the minimum components required to develop code for a given board.
  • CMSIS contains separate system and startup files for AzureRTOS and bare-metal use cases. For example:
    • system_stm32mp13xx_A7_azurertos.c and system_stm32mp13xx_A7.c
    • startup_stm32mp135cxx_ca7.c and startup_stm32mp135c_ca7_azurertos.c
  • It contains the include paths for all the firmware components.
  • It defines the STM32MP13 supported device, which defines the CMSIS and HAL driver configuration settings.
  • It provides pre-configured user files that are ready to use, as shown below:
    • HAL is initialized with the default time base with Arm® Core SysTick.
    • SysTick ISR is implemented for delay management purposes (HAL_Delay()).
  • It contains the linker script stm32mp13xx_a7_sysram.ld by default to execute from SYSRAM. If code needs to be executed from DDR, do the following changes in the linker file:
/*REGION_ALIAS("RAM", DDR_BASE);*/
REGION_ALIAS("RAM", SYSRAM_BASE);   Code is placed and executed from SYSRAM) 

REGION_ALIAS("RAM", DDR_BASE);    Code is placed and executed from DDR) 
/*REGION_ALIAS("RAM", SYSRAM_BASE); */
Warning
  • Make sure to update the include paths when copying an existing project to another location


6.2.1.2. Build application for DDR (optional)[edit | edit source]

In case the application size exceeds the SYSRAM size, it must be executed from DDR. The developer needs to follow the steps below in order:

  1. Add USE_DDR in the .cproject file.
  2. Find the reference DDR linker script in Drivers\CMSIS\Device\ST\STM32MP13xx\Source\Templates\gcc\linker\stm32mp13xx_a7_ddr.ld inside the STM32CubeMPU package.
  3. Build the application or example using STM32CubeIDE.
  4. To execute the example or application, the first step is to initialize the DDR, and then the example/application can be run from DDR. For details on this step, see the DDR Initialization and Download and run an application from DDR chapters.
6.2.1.3. Enabling Cache and MMU in application (optional)[edit | edit source]

To enable the cache and MMU in an application or example, follow the steps defined below:

  1. Add MMU_USE and CACHE_USE in the .c project file.
  2. Build the application or example using STM32CubeIDE.
Warning
  • To utilize the cache within an application, it is essential to enable both, the cache and the MMU. Effectively, the cache cannot function without the MMU being active.

Refer to the How to ensure data coherency when cache and MMU used in STM32CubeMP13 articles to know more about data coherency management.

6.2.1.4. Create signed application (optional)[edit | edit source]

This section explains how to create a signed binary for your application.

If the application needs to be booted by ROM code, then the application binary needs to be signed or prepended with the STM32 header. The STM32 header includes mandatory and optional information.

For example, FSBLA_Sdmmc1_A7_Signed.bin or MP13_BSP_TemplatesA7_DISCO_Signed.bin, delivered as part of the external loader package available in the directory Firmware/Projects/STM32MP135C-DK/External_Loader/SD_Ext_Loader. This signed binary can be created by adding a post-build option in STM32CubeIDE build steps as shown below.


Post build script (postbuild_STM32MP13.sh) is delivered as part of MP13 package and available in directory Utilities/ImageHeader.

6.2.1.5. Add middleware to your project (optional)[edit | edit source]

Your project may need to support additional middleware. This support is available from these middleware stacks: AzureRTOS.
If you have the experience, it is also possible to look in the application source code to find out which source files and which include paths must be added.

6.2.1.6. Configure the firmware components[edit | edit source]

The HAL and middleware components offer a set of build-time configuration options using macros #define, declared in a header file.
A template configuration file is provided for each component. It must be copied to the project folder (usually the configuration file is named xxx_conf_template.h, and the word _template needs to be removed when copying it to the project folder).

The configuration file provides enough information to understand the impact of each configuration option. More detailed information is available in the documentation provided with each component.

6.2.1.7. Start the HAL Library[edit | edit source]

After jumping to the main program, the application code must call the function HAL_Init() to initialize the HAL library. It includes the following tasks:
a) Configuration of the SysTick to generate an interrupt every 1 millisecond with the SysTick interrupt priority TICK_INT_PRIORITY defined in the file stm32mp13xx_hal_conf.h.
b) Configure GIC interrupts.
c) Call the HAL_MspInit() function defined in the stm32mp13xx_hal_msp.c user file to perform global low-level hardware initializations like HSEM clock enable.

6.2.1.8. Configure the system clock[edit | edit source]

The system clock configuration is done by calling the two APIs described below:
a) HAL_RCC_OscConfig(): This API configures the internal or external oscillators, as well as the PLL source and factors. The user chooses to configure either one oscillator or all oscillators. The PLL configuration can be skipped if there is no need to run the system at a high frequency.
b) HAL_RCC_ClockConfig(): This API configures the system clock source and bus prescalers.

6.2.1.9. Initialize the peripheral[edit | edit source]

a) Edit the file stm32mp13xx_hal_msp.c to write to the peripheral HAL_MspInit() function. Proceed as follows:

  1. Enable the peripheral clock.
  2. Configure the peripheral GPIOs.
  3. Configure the DMA channel and enable the DMA interrupt (if needed).
  4. Enable the peripheral interrupt (if needed).

b) Edit the stm32mp13xx_it.c file to call the required interrupt handlers (peripheral and DMA), if needed.
c) Write process complete callback functions if you plan to use the peripheral interrupt or DMA.
d) In the main.c file, initialize the peripheral handler structure, then call the function HAL_Init() to initialize your peripheral.

6.2.1.10. Develop your application[edit | edit source]

At this stage, your system is ready, and you can start developing your application code.

  • The HAL provides intuitive and ready-to-use APIs to configure the peripheral. It supports polling, interrupts, and a DMA programming model to accommodate any application requirement.
  • For more details on how to use each peripheral and manage real-time constraints, refer to the full set of examples and applications provided in the STM32CubeMP13 package (List of available projects).


6.2.2. How to debug your STM32CubeMP13 package with STM32CubeIDE[edit | edit source]

6.2.3. How to develop application with TouchGFX[edit | edit source]

To develop application using TouchGFX tool, you need to Install the X-CUBE-TOUCHGFX and the X-TouchGFX MPU addon.


6.3. How to configure the STM32CubeMP13 package for your board[edit | edit source]

6.3.1. How to initialize your new driver with STM32CubeMX[edit | edit source]

Refer to STM32CubeMX user manual UM1718.

6.3.2. How to configure the Bootloader for execution from DDR[edit | edit source]

The ROM code starts the processor in secure mode and reads the boot mode configuration. When booting from a microSD™ card, the ROM code loads and runs the FSBLA firmware from the microSD™ card inside the SYSRAM. FSBLA then loads the STM32Cube example into DDR external RAM and jumps to it. Refer to STM32CubeMP13 boot architecture for more information.

The first stage boot loader, FSBLA_Sdmmc1, is the code used as FSBLA on STM32CubeMP13 as described below.

├── Projects
│   ├── STM32MP135C-DK
│   │   ├── Applications
│   │   └── FSBLA
│   │   │   └── FSBLA_Sdmmc1	-> FSBLA code for SDMMC1

To use STM32Cube example loading by FSBLA into DDR, external loader utility should be used. Refer to section How to load and boot from external memory

6.3.3. How to load and boot from external memory[edit | edit source]

During the production phase, to flash images onto your board without using STM32CubeIDE, follow these steps:

  1. Change the boot mode to serial mode. Refer to Set boot switches to know the appropriate boot switch configuration.
  2. Issue a reset.
  3. Using the external loader utility, load the images into external memory (microSD™ card in this case) using STM32CubeProgrammer through the serial interface (UART).
  4. Once done, change the boot mode to microSD™ card boot. Refer to Set boot switches.
  5. Issue a reset.
  6. The application in the microSD™ card is loaded using FSBLA into DDR and executes from there.

External loader utility is supported for :

  1. Boot from MicroSD™ card on the STM32MP135F-DK board. Refer to Loading application into SD and boot from SD
  2. Boot from SNOR Flash on custom hardware. Refer to Loading application into SNOR and boot from SNOR
  3. Boot from eMMC on custom hardware. Refer to Loading application into eMMC and boot from eMMC