Last edited 8 months ago

STM32MP21 memory mapping

Applicable for STM32MP21x lines

This article describes how the STM32 MPU Embedded Software distribution maps the various software memory needs in internal and external volatile memories.


1. Overview[edit | edit source]

This article shows the default memory mapping defined by STMicroelectronics in STM32MPU Embedded Software. It uses a subset of all memory regions that are exposed at hardware level: customers may use other memory regions or aliases that are not shown here but are described in the STM32MP25 reference manuals.
The objective of the default STM32MPU Embedded Software memory mapping is to propose a generic memory mapping that:

  • allows demonstrating all the features proposed by the hardware platform and associated software.
  • is compliant with the official ST boards.

2. Memory mapping[edit | edit source]

2.1. Overall memory mapping[edit | edit source]

The following figure shows assignment of the different memories to the different execution contexts.
The different memory aliases required by Cortex-M33 Armv8-M architecture to differentiate secure and nonsecure memories are not represented in below figure.


ROM codeSYSRAMSRAM1RETRAMBKPSRAMDDR
STM32MP21 memory mapping

3. Internal RAM mapping[edit | edit source]

SYSRAM, SRAM1 and RETRAM internal RAMs are mapped several times at different aliases in the memory map. Possible aliases are: 0x0A000000, 0x0E000000, 0x20000000 and 0x30000000.

3.1. Overview[edit | edit source]

The SYSRAM, SRAM1 (if Video decoder and Video encoder are not used) and RETRAM can be assigned to different execution contexts of the platform by configuring the RISAB memory firewall.

The STM32MPU Embedded Software is based on a default internal RAM memory mapping which can be modified by customer to fit with its product requirements. The next chapters describe the constraints per type of RAM and memory region.

3.1.1. SYSRAM[edit | edit source]

The SYSRAM is mainly dedicated to the Cortex-A35. As it is used by the ROM code during the cold boot and the D1Standby exit, it is not recommended to dedicate a region of the SYSRAM to the Cortex-M33. Anyway, it could be could as shared memory between Cortex-A35 and Cortex-M33 to exchange some data.

At runtime, the SYSRAM is split in two regions:

  • 128kB Cortex-A35 Secure region dedicated to TF-A BL31 secure monitor.
  • 128kB Cortex-A35 nonsecure region dedicated to HPDMA linked lists management.

See SYSRAM internal memory for more information.

The following figure shows the evolution of the SYSRAM mapping during boot flow.

3.1.2. SRAM1[edit | edit source]
3.1.2.1. A35-TD flavor [edit | edit source]

At boot time, the SRAM1 is used by FSBL TF-A BL2 to store DDR controller firmware and to prepare BSEC mirror, used at runtime to share the BSEC non secret OTP.

At runtime, the SRAM1 is used to manage exchanges between both cores:

  • A dedicated BSEC mirror is used to share the BSEC non secret OTP that are necessary for both cores to configure the platform. The area is shared between Cortex-A35 OP-TEE secure OS and Cortex-M33 TF-M secure OS.
  • SCMI CID2 buffers to exchange messages between the CID2 clients (secure, non-secure) and the server (ecosystem release ≥ v6.1.0 ).
  • CM33_SRAM1 as reserved area for default M33 usage (rest of the memory).

The following figure shows the evolution of SRAM mapping during boot flow:

3.1.2.2. M33-TD flavor [edit | edit source]

During MCUboot execution, the SRAM1 is used to host the MCUboot memory stack (~46KB).

At runtime, the SRAM1 is used to manage exchanges between both cores:

  • A dedicated BSEC mirror is used to share the BSEC non secret OTP that are necessary for both cores to configure the platform. The area is a non-secure area that can be accessible by all cores but limited as read only partition.
  • SCMI CID1 buffers to exchange messages between the CID1 clients (secure, non-secure) and the server.
  • PSA buffer to exchange between client and the CID2 server.
  • A TFM_SHARED_DATA area to exchange data between MCUboot and TF-M.
  • CM33_SRAM1 as reserved area for default M33 usage (rest of the memory).
3.1.3. RETRAM[edit | edit source]
3.1.3.1. A35-TD flavor [edit | edit source]

In STM32MPU Embedded Software, RETRAM is used for:

  • DDR parameters saving to restore DDR access on low power modes exit.
  • Cortex-M33 firmware that must be preserved in low power Standby mode. It is mainly the low power entry and exit functions executed by the Cortex-M33 secure context.
3.1.3.2. M33-TD flavor [edit | edit source]

In STM32MPU Embedded Software, RETRAM is used for:

  • MPU ROM code loads MCUboot from storage device to RETRAM for his execution.
  • During MCUboot execution, the RETRAM is also used to host DDR buffer needed to load the DDR PHY firmware from the mass storage (~35KB).
  • After MCUboot execution, RETRAM is used to manage the low power restoration firmware (including RIF and DDR parameters).
3.1.4. BKPSRAM[edit | edit source]

In the STM32MPU Embedded Software architecture, the BKPSRAM is used during a cold boot or a wake-up from Standby with DDR OFF:

  • 4 kB are reserved for TF-A low power context with the DDR in Self-Refresh mode. In this case, the BKPSRAM internal memory contains the secure context initialized by TF-A BL31 that must be restored by TF-A BL2 before resuming execution of OP-TEE secure OS and Linux in DDR.
  • 4 kB are reserved for TF-M Internal Trusted Storage (ITS).

4. DDR mapping[edit | edit source]

STM32MPU Embedded Software proposes a generic DDR mapping compliant with DDR from 256MB to 4GB, allowing to demonstrate all STM32MPU Embedded Software features.

The first 64MB are reserved to firmware:

  • Cortex-M33 secure software (TF-M code and data)
  • Cortex-M33 nonsecure application (Cube code and data)
  • Cortex-A35 secure software (OP-TEE)
  • Shared memory IPC between Cortex-A35 and Cortex-M33
  • Cortex-M33 LTDC layer (only for M33-TD flavor )

Rest of the DDR is allocated to the Linux kernel and applications.
All bus master peripherals can access only to the lower 2GB of DDR as they are 32bit capable. Linux CMA and reserved memories used for contiguous buffers allocation must be defined in the first 2GB of DDR.
In case of generic memory allocation done in the higher 2GB of DDR, Linux kernel offers SWIOTLB mechanism to recopy data in a bounce buffer located in the lower 2GB of DDR compliant with 32bit bus master peripherals.

The following figure shows the evolution of the DDR mapping during the boot sequence.

  • A35-TD flavor :
  • M33-TD flavor :
Information
Note:
U-Boot supports a maximum size of 2GB DDR.

It is customer responsibility to adapt DDR mapping to its product configuration (DDR size and SW components)

4.1. How to configure RAM mapping[edit | edit source]

The memory mapping is defined in each SW component device tree file using Reserved_memory bindings. Customer can change name, based address, size, and access rights of each region according to its product needs.

To ensure the consistency of the system, memory declarations of each SW component have to be updated according to the expected configuration.

ST recommends using STM32CubeMX tools to generate coherent memory mapping with associated access rights.