Approved version. Approved on: 09:08, 12 December 2019
- Last edited 3 years ago ago
Hardware components
Subcategories
This category has the following 6 subcategories, out of 6 total.
Expert | Approved |
Technical writer | Approved |
Maintainer | Approved |
This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.
A hardware component is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board). A hardware component is natively managed by the STM32MPU Embedded Software distributions. Be careful not to confuse a hardware component with an internal peripheral (a.k.a. hardware block ) which is embedded inside a STM32 MPU microprocessor device. |
![]() |
Microprocessor unit
This category has the following 6 subcategories, out of 6 total.