1. Article purpose[edit | edit source]
The purpose of this article is to:
- briefly introduce the CSI peripheral and its main features,
- indicate the peripheral instances assignment at boot time, and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral, and to
- explain how to configure the peripheral.
2. Peripheral overview[edit | edit source]
The CSI2-Host (camera serial interface) internal peripheral is used to receive video data from an external MIPI® CSI camera sensor device, or from any other digital video equipment supporting a CSI interface. Received data are internally transferred to the DCMIPP[1] internal peripheral for further processing.
The MIPI® CSI is part of a group of communication protocols defined by the MIPI® Alliance [2]. The CSI2-Host peripheral supports MIPI® CSI2 v1.3 standard, and can receive various frame data formats using two data lanes @ 2.5 Gbps/lane.
For information on the complete list of features, refer to the STM32 MPU reference manuals. For further information on the implemented features, refer to the introduction of software frameworks and drivers below.
3. Peripheral usage[edit | edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the FwST-M Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit | edit source]
The CSI internal peripheral is not used at boot time.
3.2. Runtime assignment[edit | edit source]
3.2.1. On STM32MP21x lines
[edit | edit source]
The table below is applicable to any TD flavor (A35-TD or M33-TD)
.
Click on
to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP21 reference manuals.
| Domain | Peripheral | Runtime allocation | Comment | ||||
|---|---|---|---|---|---|---|---|
| Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 nonsecure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 nonsecure (STM32Cube) | |||
| Visual | CSI | CSI | ⬚OP-TEE | ☐ | ⬚ | ☐ | |
3.2.2. On STM32MP23x lines
[edit | edit source]
The table below is applicable to any TD flavor (A35-TD or M33-TD)
.
Click on
to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP23 reference manuals.
| Domain | Peripheral | Runtime allocation | Comment | ||||
|---|---|---|---|---|---|---|---|
| Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 nonsecure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 nonsecure (STM32Cube) | |||
| Visual | CSI | CSI | ⬚OP-TEE | ☐ | ⬚ | ☐ | |
3.2.3. On STM32MP25x lines
[edit | edit source]
The table below is applicable to any TD flavor (A35-TD or M33-TD)
.
Click on
to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
| Domain | Peripheral | Runtime allocation | Comment | |||||
|---|---|---|---|---|---|---|---|---|
| Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 nonsecure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 nonsecure (STM32Cube) |
Cortex-M0+ (STM32Cube) | |||
| Visual | CSI | CSI | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
4. Software frameworks and drivers[edit | edit source]
Below are listed the software frameworks and drivers managing the CSI peripheral for the embedded software components listed in the above tables.
- Linux®:
- V4L2 framework
- Linux kernel: drivers/media/platform/st/stm32/stm32-csi.c
- STM32Cube:
- CSI HAL driver
- Unsupported domain!
5. How to assign and configure the peripheral[edit | edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:
- partial device trees (pin control and clock tree) for the OpenSTLinux software components, and
- HAL initialization code for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
For additional information, refer to the CSI device tree configuration article for Linux®.
6. References[edit | edit source]
- ↑ DCMIPP internal peripheral
- ↑ https://www.mipi.org MIPI® Alliance