OpenSTLinux expansion packages can be combined with STM32 MPU Yocto-based OpenSTLinux embedded software to enable the use of additional components for a specific feature such as AI-based computer vision, real-time Linux, or GNSS applications. X-LINUX components can be used as software add-ons only or may be combined with hardware shields, such as NFC expansion boards.
The X-LINUX part numbers are offered and maintained by ST, and I-LINUX part numbers are developed and maintained by partners and third parties.
| Part number | Supplier | Supported devices | Supported boards | Latest supported ecosystem release[1] |
|---|---|---|---|---|
| X-LINUX-AI to demonstrate AI-based computer vision applications |
ST | STM32MP1 series STM32MP2 series |
STM32MP1 series' boards STM32MP2 series' boards |
ecosystem release v6.2.0 |
| X-LINUX-AWS to enable the development of your IoT solution by bringing AWS IoT Greengrass[2] software in the Linux® kernel |
ST | STM32MP13x lines STM32MP25x lines |
STM32MP135F-DK STM32MP257F-EV1 |
ecosystem release v6.0.0 |
| X-LINUX-AZURE to enable the development of your IoT solution by bringing Microsoft® Azure® IoT Edge[3] software in the Linux® kernel |
ST | STM32MP13x lines STM32MP25x lines |
STM32MP135F-DK STM32MP257F-EV1 |
ecosystem release v6.0.0 |
| X-LINUX-GNSS1 to demonstrate GNSS-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v4.0.0 |
| X-LINUX-IOT01E/A to demonstrate SPIRIT1 and LSM6DSOX-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v3.1.0 |
| X-LINUX-ISP to demonstrate a free-of-charge open-source software package providing Image Signal Processing (ISP) image quality software in the Linux® kernel |
ST | STM32MP25x lines |
STM32MP257F-EV1 |
ecosystem release v6.2.1 |
| X-LINUX-MEMS1 to demonstrate MEMS sensor fusion-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v4.1.0 |
| X-LINUX-NFC5 to demonstrate RFAL-based NFC applications |
ST | STM32MP15x lines |
STM32MP157F-DK2 |
ecosystem release v3.0.0 |
| X-LINUX-NFC6 to demonstrate RFAL-based NFC applications |
ST | STM32MP15x lines |
STM32MP157F-DK2 |
ecosystem release v3.0.0 |
| X-LINUX-PREDMNT to demonstrate predictive maintenance applications |
ST | STM32MP15x lines |
STM32MP157F-DK2 |
ecosystem release v2.1.0 |
| I-LINUX-Qt 90-day evaluation of Qt Design Studio and Qt Device Creation Enterprise licenses (Qt commercial trial offer to test it on the STM32MP25 product). |
Qt | STM32MP25 | STM32MP257F-DK STM32MP257F-EV1 |
ecosystem release v6.2.0 |
| X-LINUX-QT to demonstrate Qt framework feature in the Linux® kernel (Limited to the Qt open-source framework, this offer provides the possibility to develop Qt applications under GPL or LGPL terms. Please refer to Qt for Open Source Development for details.) |
ST | STM32MP257 line STM32MP255 line |
STM32MP157F-DK2 |
ecosystem release v6.2.0 |
| X-LINUX-RT to demonstrate the real-time (RT) feature in the Linux® kernel |
ST | STM32MP13x lines STM32MP15x lines STM32MP25x lines |
STM32MP1 series' boards STM32MP257F-EV1 |
ecosystem release v6.2.0 |
| X-LINUX-TPM to demonstrate TPM feature in the Linux® kernel |
ST | STM32MP1 series STM32MP257 line |
STM32MP157F-DK2 STM32MP135F-DK STM32MP257F-DK STM32MP257F-EV1 |
ecosystem release v6.2.0 |
| X-LINUX-TSNSWCH to demonstrate the real-time (RT) feature in the Linux® kernel |
ST | STM32MP257 line |
STM32MP257F-EV1 |
ecosystem release v6.2.1 |
- ↑ If the latest supported ecosystem release for the expansion package (e.g., ecosystem release v4.0.0 ) is not the latest delivered ecosystem release (ecosystem release v6.2.1
), then adaptations might be needed for this expansion package be built and executed on this latest delivered release.
- ↑ AWS IoT Greengrass
- ↑ Microsoft® Azure® IoT Edge
Subcategories
This category has the following 9 subcategories, out of 9 total.