Last edited 2 years ago

GPU troubleshooting grid

Applicable for STM32MP15x lines, STM32MP23x lines, STM32MP25x lines

Some typical issues related to the GPU framework are listed below. Solutions or debugging methods are proposed for these issues.

If your issue is not listed, try also looking in the articles available in the GPU or troubleshooting grids categories.


Symptom Resolution
[ 45.679109] Unhandled fault: imprecise external abort (0xc06) at 0xae1a0000
[ 45.684628] pgd = d1e98000
[ 45.687334] [ae1a0000] *pgd=d1e9f835, *pte=f8000747, *ppte=f8000c37
[ 45.693842] Unhandled fault: imprecise external abort (0xc06) at 0xae1a0000
[ 45.700480] pgd = d1dc0000
[ 45.703156] [ae1a0000] *pgd=00000000

Maybe the GPU reserved memory area in the kernel device tree is not aligned with the board DDR memory size. Have a look at the "gpu_reserved" entry in the kernel device tree, and update it if necessary.