Last edited 4 months ago

STM32MP2 clock tree

Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


All the peripherals receive one or several clocks that are generated via RCC internal peripheral. RCC relies on several clock sources (LSI, LSE, HSI, HSE, MSI), eight PLL, and sixty-four FLEXGEN in order to provide adequate input frequencies to all the peripherals. The clock tree covers all the system clock distribution aspects, from the clock sources to the consumer peripherals (internal and external), except clock gating management that is locally controlled by each peripheral driver.

1. Overview[edit | edit source]

In OpenSTLinux, the clock tree is configured at different steps and is managed by RCC driver in several software components:

  • When the device is reset, all RCC registers take their reset values: the eight PLL are disabled and most of the clock source selectors are pointing to the HSI.
  • The ROM Code configures the minimum clock tree needed to boot on the selected boot device.
  • The OpenSTLinux clock tree is configured by the STM32MPU software components of the boot chain with the configuration given in the device tree:
    • For A35-TD flavor it is configured by the Cortex-A35 boot chain:
      • TF-A BL2 (FSBL) has the same strategy as the ROM code, configuring the minimum clock tree needed for its execution.
      • OP-TEE (Secure OS) completely configures the clock tree as expected, all the way up to Linux.
    • For M33-TD flavor it is configured by the Cortex-M33 boot chain:
      • MCUboot (FSBL-M) has the same strategy as the ROM code, configuring the minimum clock tree needed for its execution.
      • TF-M (Secure OS) completely configures the clock tree as expected, all the way up to Linux and FwST-M_Packages.
      • Some clocks are still configured by the Cortex-A35 boot chain, when these clocks are assigned to the D1 domain (as PLL1 for Cortex-A35 frequency)
  • Linux may partly modify clock tree at runtime thanks to SCMI clock services provided by OP-TEE secure OS.
    Information related to SCMI are taken from the device tree:

2. How to build a clock tree[edit | edit source]

Building a clock tree is quite complex as it needs to take into account the constraints set by each internal and external peripheral, including external clock sources.

We encourage the use of STM32CubeMX to build the clock tree, and avoid having to know all internal peripherals details: the tool allows the selection of the peripherals that will be present on the board, fix the clock sources frequencies and automatically find an optimized clock tree. It is then able to generate the device tree that is directly consumed by the boot chain and the secure OS. Linux kernel will be able to modify clock tree at runtime thanks to SCMI clock services provided by OP-TEE.

3. ST boards clock tree for A35-TD flavor [edit | edit source]

This chapter ensures that all peripherals receive clocks with characteristics compatible with the specification (frequency, duty cycle, precision) on each ST board for A35-TD flavor .

Information
See How to change the CPU frequency article for more information about the CPU frequency setting (PLL1), including dynamic voltage and frequency scaling (DVFS) configuration.

3.1. STM32MP257F-EV1 Evaluation board case[edit | edit source]

This chapter shows the result of the boot time clock tree set by the FSBL, overlaid by the runtime clock tree set by the Secure OS on STM32MP257F-EV1 Evaluation board .

Linux eventual runtime modifications are not covered here.

3.1.1. Clock tree[edit | edit source]

The following table shows what STM32MP257F-EV1 Evaluation board clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX.

                                                       hardware
   clock                                         rate     enable
----------------------------------------------------------------
 hsi_ck                                      64000000          Y
    ck_flexgen_08                            64000000          Y
       ck_ker_usart2                         64000000          Y
       ck_ker_uart4                          64000000          N
    ck_flexgen_09                            64000000          Y
       ck_ker_usart3                         64000000          N
       ck_ker_uart5                          64000000          Y
    ck_flexgen_19                            16000000          Y
       ck_ker_usart1                         16000000          N
    ck_flexgen_20                            64000000          Y
       ck_ker_usart6                         64000000          N
    ck_flexgen_21                            64000000          Y
       ck_ker_uart7                          64000000          N
       ck_ker_uart8                          64000000          N
    ck_flexgen_22                            64000000          Y
       ck_ker_uart9                          64000000          N
    ck_flexgen_35                            16000000          Y
       ck_ker_usbtc                          16000000          Y
    ck_flexgen_50                            64000000          Y
       ck_ker_fmc                            64000000          Y
 lsi_ck                                         32000          Y
 msi_ck                                      16000000          Y
    ck_flexgen_39                            16000000          Y
       ck_ker_lpuart1                        16000000          N
 hse_ck                                      40000000          Y
    hse_div2_ck                              20000000          Y
       ck_ker_usb3pciephy                    20000000          Y
    ck_hse_rtc                               40000000          Y
    ck_pll2                                 600000000          Y
    ck_pll3                                  40000000          N
       ck_ker_gpu                            40000000          N
    ck_pll4                                1200000000          Y
       ck_icn_hs_mcu                        400000000          Y
          ck_icn_ls_mcu                     200000000          Y
             ck_icn_apb1                    200000000          Y
                ck_timg1                    200000000          Y
                   ck_ker_tim2              200000000          Y
                   ck_ker_tim3              200000000          N
                   ck_ker_tim4              200000000          N
                   ck_ker_tim5              200000000          N
                   ck_ker_tim6              200000000          Y
                   ck_ker_tim7              200000000          N
                   ck_ker_tim10             200000000          N
                   ck_ker_tim11             200000000          N
                   ck_ker_tim12             200000000          N
                   ck_ker_tim13             200000000          N
                   ck_ker_tim14             200000000          N
                ck_icn_p_tim2               200000000          Y
                ck_icn_p_tim3               200000000          N
                ck_icn_p_tim4               200000000          N
                ck_icn_p_tim5               200000000          N
                ck_icn_p_tim6               200000000          Y
                ck_icn_p_tim7               200000000          N
                ck_icn_p_tim10              200000000          N
                ck_icn_p_tim11              200000000          N
                ck_icn_p_tim12              200000000          N
                ck_icn_p_tim13              200000000          N
                ck_icn_p_tim14              200000000          N
                ck_icn_p_lptim1             200000000          N
                ck_icn_p_lptim2             200000000          N
                ck_icn_p_spi2               200000000          N
                ck_icn_p_spi3               200000000          N
                ck_icn_p_spdifrx            200000000          N
                ck_icn_p_usart2             200000000          Y
                ck_icn_p_usart3             200000000          N
                ck_icn_p_uart4              200000000          N
                ck_icn_p_uart5              200000000          Y
                ck_icn_p_i2c1               200000000          Y
                ck_icn_p_i2c2               200000000          N
                ck_icn_p_i2c3               200000000          N
                ck_icn_p_i2c4               200000000          N
                ck_icn_p_i2c5               200000000          N
                ck_icn_p_i2c6               200000000          N
                ck_icn_p_i2c7               200000000          N
                ck_icn_p_i3c1               200000000          N
                ck_icn_p_i3c2               200000000          N
                ck_icn_p_i3c3               200000000          N
             ck_icn_apb2                    200000000          Y
                ck_timg2                    200000000          Y
                   ck_ker_tim1              200000000          N
                   ck_ker_tim8              200000000          N
                   ck_ker_tim15             200000000          N
                   ck_ker_tim16             200000000          N
                   ck_ker_tim17             200000000          N
                   ck_ker_tim20             200000000          N
                ck_icn_p_tim1               200000000          N
                ck_icn_p_tim8               200000000          N
                ck_icn_p_tim15              200000000          N
                ck_icn_p_tim16              200000000          N
                ck_icn_p_tim17              200000000          N
                ck_icn_p_tim20              200000000          N
                ck_icn_p_sai1               200000000          N
                ck_icn_p_sai2               200000000          N
                ck_icn_p_sai3               200000000          N
                ck_icn_p_sai4               200000000          N
                ck_icn_p_usart1             200000000          N
                ck_icn_p_usart6             200000000          N
                ck_icn_p_uart7              200000000          N
                ck_icn_p_uart8              200000000          N
                ck_icn_p_uart9              200000000          N
                ck_icn_p_fdcan              200000000          N
                ck_icn_p_spi1               200000000          N
                ck_icn_p_spi4               200000000          N
                ck_icn_p_spi5               200000000          N
                ck_icn_p_spi6               200000000          N
                ck_icn_p_spi7               200000000          N
             ck_icn_apb3                    200000000          Y
                ck_icn_p_bsec               200000000          Y
                ck_icn_p_iwdg1              200000000          Y
                ck_icn_p_iwdg2              200000000          N
                ck_icn_p_iwdg3              200000000          N
                ck_icn_p_iwdg4              200000000          N
                ck_icn_p_wwdg1              200000000          N
                ck_icn_p_vref               200000000          N
                ck_icn_p_dts                200000000          Y
                ck_icn_p_serc               200000000          Y
                ck_icn_p_hdp                200000000          N
                ck_icn_p_is2m               200000000          N
             ck_icn_apb4                    200000000          Y
                ck_icn_p_dsi                200000000          N
                ck_icn_p_ltdc               200000000          N
                ck_icn_p_csi2               200000000          N
                ck_icn_p_dcmipp             200000000          N
                ck_icn_p_ddrc               200000000          Y
                ck_icn_p_ddrcfg             200000000          Y
                ck_icn_p_lvds               200000000          N
                ck_icn_p_gicv2m             200000000          Y
                ck_icn_p_usbtc              200000000          Y
                ck_icn_p_busperfm           200000000          N
                ck_icn_p_usb3pciephy        200000000          Y
                ck_icn_p_stgen              200000000          Y
                ck_icn_p_vdec               200000000          N
                ck_icn_p_venc               200000000          N
             ck_icn_apbdbg                  200000000          Y
                ck_sys_dbg                  200000000          Y
                ck_icn_p_stm                200000000          N
                ck_icn_p_etr                200000000          N
             ck_icn_s_bkpsram               200000000          Y
             ck_icn_p_ddrphyc               200000000          Y
             ck_icn_p_syscpu1               200000000          Y
             ck_icn_p_hpdma1                200000000          Y
             ck_icn_p_hpdma2                200000000          Y
             ck_icn_p_hpdma3                200000000          Y
             ck_icn_p_ipcc1                 200000000          Y
             ck_icn_p_ipcc2                 200000000          Y
             ck_icn_p_cci                   200000000          N
             ck_icn_p_crc                   200000000          N
             ck_icn_p_ospiiom               200000000          N
             ck_icn_p_hash                  200000000          N
             ck_icn_p_rng                   200000000          Y
             ck_icn_p_cryp1                 200000000          N
             ck_icn_p_cryp2                 200000000          N
             ck_icn_p_saes                  200000000          Y
             ck_icn_p_pka                   200000000          Y
             ck_icn_p_gpioa                 200000000          Y
             ck_icn_p_gpiob                 200000000          Y
             ck_icn_p_gpioc                 200000000          Y
             ck_icn_p_gpiod                 200000000          Y
             ck_icn_p_gpioe                 200000000          Y
             ck_icn_p_gpiof                 200000000          Y
             ck_icn_p_gpiog                 200000000          Y
             ck_icn_p_gpioh                 200000000          Y
             ck_icn_p_gpioi                 200000000          Y
             ck_icn_p_gpioj                 200000000          Y
             ck_icn_p_gpiok                 200000000          Y
             ck_icn_s_lpsram1               200000000          Y
             ck_icn_s_lpsram2               200000000          Y
             ck_icn_s_lpsram3               200000000          Y
             ck_icn_p_gpioz                 200000000          Y
             ck_icn_p_lpdma                 200000000          N
             ck_icn_p_adf1                  200000000          N
             ck_icn_p_hsem                  200000000          N
             ck_icn_p_rtc                   200000000          Y
             ck_icn_p_iwdg5                 200000000          N
             ck_icn_p_wwdg2                 200000000          N
             ck_icn_s_stm                   200000000          N
             ck_icn_p_fmc                   200000000          Y
             ck_icn_p_eth1                  200000000          N
             ck_icn_p_ethsw                 200000000          N
             ck_icn_p_eth2                  200000000          Y
             ck_icn_p_pcie                  200000000          Y
             ck_icn_p_adc12                 200000000          N
             ck_icn_p_adc3                  200000000          Y
             ck_icn_p_mdf1                  200000000          N
             ck_icn_p_spi8                  200000000          N
             ck_icn_p_lpuart1               200000000          N
             ck_icn_p_i2c8                  200000000          N
             ck_icn_p_lptim3                200000000          Y
             ck_icn_p_lptim4                200000000          N
             ck_icn_p_lptim5                200000000          N
             ck_icn_p_risaf4                200000000          Y
             ck_icn_p_i3c4                  200000000          N
             ck_ker_eth1stp                 200000000          N
             ck_ker_eth2stp                 200000000          N
          ck_icn_s_sysram                   400000000          Y
          ck_icn_s_vderam                   400000000          Y
          ck_icn_s_retram                   400000000          Y
          ck_icn_s_sram1                    400000000          Y
          ck_icn_s_sram2                    400000000          Y
          ck_icn_s_ospi1                    400000000          Y
          ck_icn_s_ospi2                    400000000          Y
          ck_icn_p_otfd1                    400000000          Y
          ck_icn_p_otfd2                    400000000          Y
       ck_icn_sdmmc                         200000000          Y
          ck_icn_m_sdmmc1                   200000000          N
          ck_icn_m_sdmmc2                   200000000          N
          ck_icn_m_sdmmc3                   200000000          N
       ck_icn_ddr                           600000000          Y
          ck_icn_s_ddr                      600000000          Y
       ck_icn_display                       400000000          Y
       ck_icn_hsl                           300000000          Y
          ck_icn_m_usb2ohci                 300000000          Y
          ck_icn_m_usb2ehci                 300000000          Y
          ck_icn_m_usb3dr                   300000000          Y
       ck_icn_nic                           400000000          Y
       ck_icn_vid                           600000000          Y
       ck_flexgen_07                        100000000          Y
          ck_ker_lptim1                     100000000          N
          ck_ker_lptim2                     100000000          N
       ck_flexgen_11                        200000000          Y
          ck_ker_spdifrx                    200000000          N
       ck_flexgen_12                        100000000          Y
          ck_ker_i2c1                       100000000          Y
          ck_ker_i2c2                       100000000          N
          ck_ker_i3c1                       100000000          N
          ck_ker_i3c2                       100000000          N
       ck_flexgen_13                        100000000          Y
          ck_ker_i2c3                       100000000          N
          ck_ker_i2c5                       100000000          N
          ck_ker_i3c3                       100000000          N
       ck_flexgen_14                        100000000          Y
          ck_ker_i2c4                       100000000          N
          ck_ker_i2c6                       100000000          N
       ck_flexgen_15                        100000000          Y
          ck_ker_i2c7                       100000000          N
       ck_flexgen_16                         50000000          Y
          ck_ker_spi1                        50000000          N
       ck_flexgen_26                        100000000          Y
          ck_ker_fdcan                      100000000          N
       ck_flexgen_34                         20000000          Y
       ck_flexgen_41                        100000000          Y
          ck_ker_lptim4                     100000000          N
          ck_ker_lptim5                     100000000          N
       ck_flexgen_43                         50000000          Y
          ck_ker_tsdbg                       50000000          Y
       ck_flexgen_44                        200000000          Y
          ck_ker_tpiu                       200000000          N
       ck_flexgen_45                        400000000          Y
          ck_icn_m_etr                      400000000          N
          ck_sys_atb                        400000000          Y
       ck_flexgen_51                        200000000          Y
          ck_ker_sdmmc1                     200000000          N
       ck_flexgen_52                        200000000          Y
          ck_ker_sdmmc2                     200000000          N
       ck_flexgen_53                        200000000          Y
          ck_ker_sdmmc3                     200000000          N
       ck_flexgen_56                        200000000          Y
          ck_ker_eth1ptp                    200000000          N
          ck_ker_eth2ptp                    200000000          Y
       ck_flexgen_59                        600000000          Y
          ck_icn_m_gpu                      600000000          N
       ck_flexgen_60                         50000000          Y
          ck_ker_ethswref                    50000000          N
       ck_flexgen_61                        150000000          Y
          ck_mco1                           150000000          N
       ck_flexgen_62                        150000000          Y
          ck_mco2                           150000000          N
       ck_flexgen_63                        400000000          Y
    ck_pll5                                 532000000          Y
       ck_flexgen_17                        133000000          Y
          ck_ker_spi4                       133000000          N
          ck_ker_spi5                       133000000          N
       ck_flexgen_18                        133000000          Y
          ck_ker_spi6                       133000000          N
          ck_ker_spi7                       133000000          N
       ck_flexgen_29                        266000000          Y
          ck_ker_csi2                       266000000          N
       ck_flexgen_31                         26600000          Y
          ck_ker_csi2phy                     26600000          N
       ck_flexgen_32                         26600000          Y
          ck_ker_lvdsphy                     26600000          N
       ck_flexgen_36                        133000000          Y
          ck_ker_i3c4                       133000000          N
       ck_flexgen_37                        133000000          Y
          ck_ker_spi8                       133000000          N
       ck_flexgen_38                        133000000          Y
          ck_ker_i2c8                       133000000          N
       ck_flexgen_46                        133000000          Y
          ck_ker_adc12                      133000000          N
       ck_flexgen_47                        133000000          Y
          ck_ker_adc3                       133000000          Y
       ck_flexgen_48                        133000000          Y
          ck_ker_ospi1                      133000000          Y
       ck_flexgen_49                        133000000          Y
          ck_ker_ospi2                      133000000          Y
    ck_pll6                                 125000000          Y
       ck_flexgen_54                         62500000          Y
          ck_ker_eth1                        62500000          N
          ck_ker_ethsw                       62500000          N
       ck_flexgen_55                        125000000          Y
          ck_ker_eth2                       125000000          Y
    ck_pll7                                 835511719          Y
       ck_flexgen_10                         49147748          Y
          ck_ker_spi2                        49147748          N
          ck_ker_spi3                        49147748          N
       ck_flexgen_23                         49147748          Y
          ck_ker_mdf1                        49147748          N
          ck_ker_sai1                        49147748          N
       ck_flexgen_24                         49147748          Y
          ck_ker_sai2                        49147748          N
       ck_flexgen_25                         49147748          Y
          ck_ker_sai3                        49147748          N
          ck_ker_sai4                        49147748          N
       ck_flexgen_42                         49147748          Y
          ck_ker_adf1                        49147748          N
    ck_pll8                                 594000000          Y
       ck_flexgen_27                        148500000          Y
          ck_ker_ltdc                       148500000          N
       ck_flexgen_28                         27000000          Y
          clk_phy_dsi                        27000000          N
    ck_flexgen_30                            20000000          Y
       ck_ker_csi2txesc                      20000000          N
    ck_flexgen_33                            40000000          Y
       ck_ker_stgen                          40000000          Y
    ck_flexgen_57                            20000000          Y
       ck_ker_usb2phy1                       20000000          Y
    ck_flexgen_58                            20000000          Y
       ck_ker_usb2phy2                       20000000          Y
       ck_ker_usb2phy2_en                    20000000          Y
    ck_ker_dts                               40000000          Y
 lse_ck                                         32768          Y
    ck_flexgen_40                               32768          Y
       ck_ker_lptim3                            32768          Y
    ck_rtc                                      32768          Y
 spdifsymb                                          0          Y
 i2sckin                                            0          Y
 txbyteclk                                          0          Y
    clk_lanebyte                                    0          N
 ck_cpu1                                   1500000000          Y
 ck_obs0                                            0          Y
 ck_obs1                                            0          Y

3.1.2. Device tree[edit | edit source]

As mentioned in previous chapters, RCC configuration is done in two steps, first by the first stage boot loader (FSBL: TF-A BL2) and then by the secure OS (OP-TEE).

Here are the corresponding device tree rcc sub node properties in fdts/stm32mp257f-ev1-ca35tdcid-rcc.dtsi consumed by the first stage boot loader (FSBL: TF-A BL2) to configure the clock tree required to boot on STM32MP257F-EV1 Evaluation board :

&rcc {
	st,busclk = <
		DIV_CFG(DIV_LSMCU, 1)
		DIV_CFG(DIV_APB1, 0)
		DIV_CFG(DIV_APB2, 0)
		DIV_CFG(DIV_APB3, 0)
		DIV_CFG(DIV_APB4, 0)
		DIV_CFG(DIV_APBDBG, 0)
	>;

	st,flexgen = <
		FLEXGEN_CFG(0, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(1, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(2, XBAR_SRC_PLL4, 0, 1)
		FLEXGEN_CFG(4, XBAR_SRC_PLL4, 0, 3)
		FLEXGEN_CFG(5, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(8, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(48, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(51, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(52, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(58, XBAR_SRC_HSE_KER, 0, 1)
		FLEXGEN_CFG(63, XBAR_SRC_PLL4, 0, 2)
	>;

	st,kerclk = <
		MUX_CFG(MUX_USB2PHY1, MUX_USB2PHY1_FLEX57)
		MUX_CFG(MUX_USB2PHY2, MUX_USB2PHY2_FLEX58)
	>;

	pll1: st,pll-1 {
		st,pll = <&pll1_cfg_1200Mhz>;

		pll1_cfg_1200Mhz: pll1-cfg-1200Mhz {
			cfg = <30 1 1 1>;
			src = <MUX_CFG(MUX_MUXSEL5, MUXSEL_HSE)>;
		};
	};

	pll2: st,pll-2 {
		st,pll = <&pll2_cfg_600Mhz>;

		pll2_cfg_600Mhz: pll2-cfg-600Mhz {
			cfg = <30 1 1 2>;
			src = <MUX_CFG(MUX_MUXSEL6, MUXSEL_HSE)>;
		};
	};

	pll4: st,pll-4 {
		st,pll = <&pll4_cfg_1200Mhz>;

		pll4_cfg_1200Mhz: pll4-cfg-1200Mhz {
			cfg = <30 1 1 1>;
			src = <MUX_CFG(MUX_MUXSEL0, MUXSEL_HSE)>;
		};
	};

	pll5: st,pll-5 {
		st,pll = <&pll5_cfg_532Mhz>;

		pll5_cfg_532Mhz: pll5-cfg-532Mhz {
			cfg = <133 5 1 2>;
			src = <MUX_CFG(MUX_MUXSEL1, MUXSEL_HSE)>;
		};
	};
};

Here are the corresponding device tree rcc sub node properties in core/arch/arm/dts/stm32mp257f-ev1-ca35tdcid-rcc.dtsi consumed by the secure OS (OP-TEE) to configure the clock tree above:

&rcc {
	st,busclk = <
		DIV_CFG(DIV_LSMCU, 1)
		DIV_CFG(DIV_APB1, 0)
		DIV_CFG(DIV_APB2, 0)
		DIV_CFG(DIV_APB3, 0)
		DIV_CFG(DIV_APB4, 0)
		DIV_CFG(DIV_APBDBG, 0)
	>;

	st,flexgen = <
		FLEXGEN_CFG(0, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(1, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(2, XBAR_SRC_PLL4, 0, 1)
		FLEXGEN_CFG(3, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(4, XBAR_SRC_PLL4, 0, 3)
		FLEXGEN_CFG(5, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(6, XBAR_SRC_PLL4, 0, 1)
		FLEXGEN_CFG(7, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(8, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(9, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(10, XBAR_SRC_PLL7, 0, 16)
		FLEXGEN_CFG(11, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(12, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(13, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(14, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(15, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(16, XBAR_SRC_PLL4, 0, 23)
		FLEXGEN_CFG(17, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(18, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(19, XBAR_SRC_HSI_KER, 0, 3)
		FLEXGEN_CFG(20, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(21, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(22, XBAR_SRC_HSI_KER, 0, 0)
		FLEXGEN_CFG(23, XBAR_SRC_PLL7, 0, 16)
		FLEXGEN_CFG(24, XBAR_SRC_PLL7, 0, 16)
		FLEXGEN_CFG(25, XBAR_SRC_PLL7, 0, 16)
		FLEXGEN_CFG(26, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(27, XBAR_SRC_PLL8, 0, 3)
		FLEXGEN_CFG(28, XBAR_SRC_PLL8, 0, 21)
		FLEXGEN_CFG(29, XBAR_SRC_PLL5, 0, 1)
		FLEXGEN_CFG(30, XBAR_SRC_HSE_KER, 0, 1)
		FLEXGEN_CFG(31, XBAR_SRC_PLL5, 0, 19)
		FLEXGEN_CFG(32, XBAR_SRC_PLL5, 0, 19)
		FLEXGEN_CFG(33, XBAR_SRC_PLL4, 0, 23)
		FLEXGEN_CFG(34, XBAR_SRC_PLL4, 0, 59)
		FLEXGEN_CFG(35, XBAR_SRC_HSI_KER, 0, 3)
		FLEXGEN_CFG(36, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(37, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(38, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(39, XBAR_SRC_MSI_KER, 0, 0)
		FLEXGEN_CFG(40, XBAR_SRC_LSE, 0, 0)
		FLEXGEN_CFG(41, XBAR_SRC_PLL4, 0, 11)
		FLEXGEN_CFG(42, XBAR_SRC_PLL7, 0, 16)
		FLEXGEN_CFG(43, XBAR_SRC_PLL4, 0, 23)
		FLEXGEN_CFG(44, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(45, XBAR_SRC_PLL4, 0, 2)
		FLEXGEN_CFG(46, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(47, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(48, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(49, XBAR_SRC_PLL5, 0, 3)
		FLEXGEN_CFG(51, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(52, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(53, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(54, XBAR_SRC_PLL6, 0, 3)
		FLEXGEN_CFG(55, XBAR_SRC_PLL6, 0, 3)
		FLEXGEN_CFG(56, XBAR_SRC_PLL4, 0, 5)
		FLEXGEN_CFG(57, XBAR_SRC_HSE_KER, 0, 1)
		FLEXGEN_CFG(58, XBAR_SRC_HSE_KER, 0, 1)
		FLEXGEN_CFG(59, XBAR_SRC_PLL4, 0, 1)
		FLEXGEN_CFG(60, XBAR_SRC_PLL4, 0, 23)
		FLEXGEN_CFG(61, XBAR_SRC_PLL4, 0, 7)
		FLEXGEN_CFG(62, XBAR_SRC_PLL4, 0, 7)
		FLEXGEN_CFG(63, XBAR_SRC_PLL4, 0, 2)
	>;

	st,kerclk = <
		MUX_CFG(MUX_ADC12, MUX_ADC12_FLEX46)
		MUX_CFG(MUX_USB2PHY1, MUX_USB2PHY1_FLEX57)
		MUX_CFG(MUX_USB2PHY2, MUX_USB2PHY2_FLEX58)
		MUX_CFG(MUX_USB3PCIEPHY, MUX_USB3PCIEPHY_HSE)
		MUX_CFG(MUX_DSIPHY, MUX_DSIPHY_FLEX28)
		MUX_CFG(MUX_DSIBLANE, MUX_DSIBLANE_DSIPHY)
		MUX_CFG(MUX_LVDSPHY, MUX_LVDSPHY_FLEX32)
		MUX_CFG(MUX_DTS, MUX_DTS_HSE)
		MUX_CFG(MUX_RTC, MUX_RTC_LSE)
		MUX_CFG(MUX_D3PER, MUX_D3PER_MSI)
		MCO_CFG(MCO1, MUX_MCO1_FLEX61, MCO_OFF)
		MCO_CFG(MCO2, MUX_MCO2_FLEX62, MCO_OFF)
	>;

	pll1: st,pll-1 {
		st,pll = <&pll1_cfg_1200Mhz>;

		pll1_cfg_1200Mhz: pll1-cfg-1200Mhz {
			cfg = <30 1 1 1>;
			src = <MUX_CFG(MUX_MUXSEL5, MUXSEL_HSE)>;
		};

		pll1_cfg_1500Mhz: pll1-cfg-1500Mhz {
			cfg = <75 2 1 1>;
			src = <MUX_CFG(MUX_MUXSEL5, MUXSEL_HSE)>;
		};
	};

	pll2: st,pll-2 {
		st,pll = <&pll2_cfg_600Mhz>;

		pll2_cfg_600Mhz: pll2-cfg-600Mhz {
			cfg = <30 1 1 2>;
			src = <MUX_CFG(MUX_MUXSEL6, MUXSEL_HSE)>;
		};
	};

	pll3: st,pll-3 {
		st,pll = <&pll3_cfg_800Mhz>;

		pll3_cfg_800Mhz: pll3-cfg-800Mhz {
			cfg = <20 1 1 1>;
			src = <MUX_CFG(MUX_MUXSEL7, MUXSEL_HSE)>;
		};

		pll3_cfg_900Mhz: pll3-cfg-900Mhz {
			cfg = <45 2 1 1>;
			src = <MUX_CFG(MUX_MUXSEL7, MUXSEL_HSE)>;
		};
	};

	pll4: st,pll-4 {
		st,pll = <&pll4_cfg_1200Mhz>;

		pll4_cfg_1200Mhz: pll4-cfg-1200Mhz {
			cfg = <30 1 1 1>;
			src = <MUX_CFG(MUX_MUXSEL0, MUXSEL_HSE)>;
		};
	};

	pll5: st,pll-5 {
		st,pll = <&pll5_cfg_532Mhz>;

		pll5_cfg_532Mhz: pll5-cfg-532Mhz {
			cfg = <133 5 1 2>;
			src = <MUX_CFG(MUX_MUXSEL1, MUXSEL_HSE)>;
		};
	};
As mentioned in previous chapters, RCC configuration is done in two steps, first by the first stage boot loader (FSBL: TF-A BL2) and then by the secure OS (OP-TEE), configured by 

	pll6: st,pll-6 {
		st,pll = <&pll6_cfg_500Mhz>;

		pll6_cfg_500Mhz: pll6-cfg-500Mhz {
			cfg = <25 1 1 2>;
			src = <MUX_CFG(MUX_MUXSEL2, MUXSEL_HSE)>;
		};
	};

	pll7: st,pll-7 {
		st,pll = <&pll7_cfg_835_51172Mhz>;

		pll7_cfg_835_51172Mhz: pll7-cfg-835-51172Mhz {
			cfg = <167 4 1 2>;
			src = <MUX_CFG(MUX_MUXSEL3, MUXSEL_HSE)>;
			frac = < 0x1A3337 >;
		};
	};

	pll8: st,pll-8 {
		st,pll = <&pll8_cfg_594Mhz>;

		pll8_cfg_594Mhz: pll8-cfg-594Mhz {
			cfg = <297 5 1 4>;
			src = <MUX_CFG(MUX_MUXSEL4, MUXSEL_HSE)>;
		};
	};
};

3.2. STM32MP257F-DK Discovery kit case[edit | edit source]

This chapter shows the result of the boot time clock tree set by the FSBL, overlaid by the runtime clock tree set by the Secure OS on STM32MP257F-DK Discovery kit .

3.2.1. Clock tree[edit | edit source]

The STM32MP257F-DK Discovery kit clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX can be displayed with the next command:

cat /sys/kernel/debug/clk/stm32_clk_summary

3.2.2. Device tree[edit | edit source]

As mentioned in previous chapters, RCC configuration is done in two steps, first by the first stage boot loader (FSBL: TF-A BL2) and then by the secure OS (OP-TEE), configured by

3.3. STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation case[edit | edit source]

The same clock tree is used in STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation device tree files:

3.4. STM32MP215F-DK Discovery kit case[edit | edit source]

This chapter shows the result of the boot time clock tree set by the FSBL, overlaid by the runtime clock tree set by the Secure OS on STM32MP215F-DK Discovery kit .

3.4.1. Clock tree[edit | edit source]

The STM32MP215F-DK Discovery kit clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX can be displayed with the next command:

cat /sys/kernel/debug/clk/stm32_clk_summary

3.4.2. Device tree[edit | edit source]

As mentioned in previous chapters, RCC configuration is done in two steps, first by the first stage boot loader (FSBL: TF-A BL2) and then by the secure OS (OP-TEE), configured by

4. ST boards clock tree for M33-TD flavor [edit | edit source]

As mentioned in previous chapters, RCC configuration is done in several steps:

  • first by the Cortex-M33 boot chain for system resources and clocks assigned to D2 domain
    • the first stage boot loader (FSBL-M: MCUBoot)
    • the secure OS (TF-M)
  • then by the Cortex-A35 boot chain but only for clock assigned to D1 domain (see RCC resource allocation per feature; this protection is defined by RIF-aware RCC features or is inherited for internal peripherals from RIFSC configuration)
    • the first stage boot loader (FSBL-A: TF-A BL2)
    • the secure OS (OP-TEE)

The clock tree for on each ST board ensures that all peripherals receive clocks with characteristics compatible with the specification (frequency, duty cycle, precision) .

Information
See How to change the CPU frequency article for more information about the CPU frequency setting (PLL1), including dynamic voltage and frequency scaling (DVFS) configuration.

4.1. STM32MP215F-DK Discovery kit for M33-TD flavor [edit | edit source]

RCC configuration is configured by the rcc sub node properties in device tree:

  1. MCUBoot in stm32mp2/m33-td/mcuboot/stm32mp215f-dk-cm33tdcid-ostl-sdcard-bl2-rcc.dtsi
  2. TF-M in stm32mp2/m33-td/tfm/stm32mp215f-dk-cm33tdcid-ostl-rcc.dtsi
  3. TF-A in stm32mp2/m33-td/tf-a/stm32mp215f-dk-cm33tdcid-ostl-rcc.dtsi
  4. OP-TEE in stm32mp2/m33-td/optee/stm32mp215f-dk-cm33tdcid-ostl-rcc.dtsi

4.2. STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation for M33-TD flavor [edit | edit source]

RCC configuration is configured by the rcc sub node properties in device tree:

  1. MCUBoot in stm32mp2/m33-td/mcuboot/stm32mp235f-dk-cm33tdcid-ostl-sdcard-bl2-rcc.dtsi
  2. TF-M in stm32mp2/m33-td/tfm/stm32mp235f-dk-cm33tdcid-ostl-rcc.dtsi
  3. TF-A in stm32mp2/m33-td/tf-a/stm32mp235f-dk-cm33tdcid-ostl-rcc.dtsi
  4. OP-TEE in stm32mp2/m33-td/optee/stm32mp235f-dk-cm33tdcid-ostl-rcc.dtsi


4.3. STM32MP257F-DK Discovery kit for M33-TD flavor [edit | edit source]

RCC configuration is configured by the rcc sub node properties in device tree:

  1. MCUBoot in stm32mp2/m33-td/mcuboot/stm32mp257f-dk-cm33tdcid-ostl-sdcard-bl2-rcc.dtsi
  2. TF-M in stm32mp2/m33-td/tfm/stm32mp257f-dk-cm33tdcid-ostl-rcc.dtsi
  3. TF-A in stm32mp2/m33-td/tf-a/stm32mp257f-dk-cm33tdcid-ostl-rcc.dtsi
  4. OP-TEE in stm32mp2/m33-td/optee/stm32mp257f-dk-cm33tdcid-ostl-rcc.dtsi


4.4. STM32MP257F-EV1 Evaluation board for M33-TD flavor [edit | edit source]

RCC configuration is configured by the rcc sub node properties in device tree:

  1. MCUBoot in stm32mp2/m33-td/mcuboot/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-bl2-rcc.dtsi
  2. TF-M in stm32mp2/m33-td/tfm/stm32mp257f-ev1-cm33tdcid-ostl-rcc.dtsi
  3. TF-A in stm32mp2/m33-td/tf-a/stm32mp257f-ev1-cm33tdcid-ostl-rcc.dtsi
  4. OP-TEE in stm32mp2/m33-td/optee/stm32mp257f-ev1-cm33tdcid-ostl-rcc.dtsi