Last edited 8 months ago

FwST-M BSP architecture overview

Applicable for STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

The FwST-M BSP encompasses the following components:

  • The boot chain based on MCUboot (FSBL-M) running on the Arm® Cortex®-M in secure mode, for M33-TD flavor of STM32MP2 series only.
  • The TF-M secure OS running on the Arm® Cortex®-M in secure mode. It provides local secure services to STM32Cube MPU Package. For STM32MP2 series only.
  • The STM32Cube MPU Package drivers (BSP, HAL, LL) running on the Arm® Cortex®-M nonsecure mode.

The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

Zoom out to FwST-M Packages



TF-M overviewMCUboot overviewCategory:STM32Cube MPU Packages
FwST-M BSP architecture overview