OpenWrt-based Linux embedded software

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


Important
OpenWrt-based Linux distribution is validated against the ecosystem release v6.1.0 (see release note). It has not been ported yet on ecosystem release v6.2.1 .
Partner program
Bootlin has developed specific support, demonstration configurations, and documentation to help ST customers use OpenWrt on STM32 MPU platforms.

See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html

To address Bootlin technical support for OpenWrt: mailto:openwrt-st-support@bootlin.com



The OpenWrt-based Linux® embedded software is part of the STM32 MPU embedded software offer.
It is a set of software (see architecture overview), system build and development tools created to ease the development to be done on top of STM32 MPU devices.

It is made up of:

  • an open-source Linux® distribution, based on the OpenWrt framework, running on the Arm® Cortex®-A processor(s),
  • firmwares, running on the Arm® Cortex®-M processor: FwST-M Packages (not supported for STM32MP13x lines )

OpenWrt[1] is a Linux operating system targeting embedded devices. OpenWrt provides a fully writable filesystem with package management. OpenWrt is the framework to build an application without having to build a complete firmware around it; for users this means the ability for full customization, to use the device in ways never envisioned.

The Linux® distribution relies on the OpenSTLinux board support package (U-Boot, TF-A, OP-TEE, Linux kernel) complemented with a user-space with a features set.

The partner's repository[2] is "OpenWrt feed"[3] dedicated to supporting the STMicroelectronics STM32MPU platforms.

Several examples of OpenWrt configurations[4] are provided:

  • the minimal configuration relies on the OpenSTLinux BSP[5]: TF-A, U-Boot, OP-TEE, Linux
  • "demo" configurations include additional packages like a web interface to configure the device

This feed also shows how use the OpenWrt image Builder and how to run benchmarks[6].


OpenWrt Release noteFwST-M PackagesLinux OpenWrt-based embedded software

The OpenWrt-based Linux embedded software offers two development packages that let developers select the support that best meets their needs:

  • the starter package to quickly and easily start with the boards. It delivers a software image (binary), ready to flash on an SD card, that includes pre-built examples (a.k.a. firmware) of the package(s) running on the Arm® Cortex®-M processor, running as coprocessor.
  • the distribution package to create your own OpenWrt-based Linux® embedded software, as well as your own starter and developer packages. It delivers the source code of all the software components of the OpenWrt-based Linux® embedded software, and uses the OpenWrt as the underlying building and distribution generation framework.
STM32 supported device Boards Starter Package Distribution Package Ecosystem release note
STM32MP13x lines  STM32MP13 Discovery kits STM32MPU Starter Package Latest OpenWrt tag: openstlinux-6.6-openwrt-24.10.6-mpu-v25.06.11 OpenWrt-based Linux ecosystem release note
STM32MP15x lines  STM32MP15 Discovery kits
STM32MP21x lines 
STM32MP21 Discovery kits
STM32MP23x lines 
STM32MP25 Discovery kits for STM32MP23x lines evaluation
STM32MP25x lines  STM32MP25 Evaluation boards
STM32MP25 Discovery kits

1. References[edit | edit source]


Pages in category "OpenWrt-based Linux embedded software"

This category contains only the following page.