Last edited 9 months ago

Reserved memory

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Article purpose[edit | edit source]

The Reserved-memory mechanism[1] allows reserving memory regions in the kernel. This mechanism is used by drivers to allocate buffers in specific memory regions (such as internal SRAM) or to get a dedicated memory pool that will not be managed by Linux® conventionnal memory allocator (in DDR).

2. Use cases[edit | edit source]

In OpenSTLinux, the reserved-memory is used:

  • On STM32MP1 series by:
  • On STM32MP15x lines  by:
  • the remoteproc driver to reserve the regions in RETRAM and MCU SRAM where the Cortex-M4 coprocessor firmware will be loaded.
  • the RPMsg driver to reserve the region where RPMsg buffers used for interprocess communication with the Cortex-M4 coprocessor, are allocated, typically MCU SRAM.
  • the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the DDR.
  • On STM32MP2 series by:
  • the dmaengine driver to reserve the region where DMA buffers are allocated, typically in internal STM32MP2 SRAM.
  • the remoteproc driver to reserve the regions in RETRAM, SRAM and DDR, where the Cortex-M coprocessor firmware will be loaded.
  • the RPMsg driver to reserve the region where RPMsg buffers used for interprocess communication with the Cortex-M coprocessor, are allocated, typically in SRAM or DDR.
  • the SCMI to reserve the region for SCMI buffers, typically in SRAM
  • the LTDC driver, see DRM KMS overview.
  • On STM32MP23x lines  and STM32MP25x lines , the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the DDR.

3. References[edit | edit source]