Last edited 9 months ago

STM32MP13 ecosystem errata sheet

Applicable for STM32MP13x lines



1. Article purpose[edit | edit source]

The STM32MP13xx device errata sheet[1] lists the different device limitations and explains the corresponding workarounds (software and/or hardware) if any.

The objective of this article is to explain which of the workarounds, described in this errata sheet, are applicable and implemented in ecosystem release v4.1.0 .

This article lists

  • errata to be workaround by the customers,
  • errata workaround implemented in STM32MPU Ecosystem releases,
  • and errata not applicable in STM32MPU Ecosystem releases.

Errata, present in STM32MP13xx device errata sheet[1] and not listed in this article, have no workaround implemented in STM32MPU Ecosystem releases.

2. Legend[edit | edit source]

The section column refers to the number of the erratum chapter in the errata sheet document.

Rev.Y columns , present in the tables below, refer to the availability and status of a given errata workaround for the described erratum in errata sheet document:

  • A = workaround available
  • P = partial workaround available
  • N = no workaround available

OpenSTLinux and CubeMP1 columns , present in the tables below, refer to the availability of a workaround for a given STM32MP13 ecosystem release:

  • U = workaround to implement by User
  • I = workaround Implemented
  • NA= Errata Not Applicable in ST software release

Wave your mouse over a status in the table to display the corresponding legend.

3. Workarounds to implement by customer[edit | edit source]

Function Section Limitation Rev.Y Comment
Arm® Cortex®-A7 core 2.1.1 Memory locations might be accessed speculatively due to instruction fetches when HCR.VM is set A U NA OpenSTLinux distribution does not activate Arm® Cortex®-A7 Hypervisor mode and hence the Virtual Memory second stage of translation.

The customer should implement the workaround if the Hypervisor mode is used in his/her product.

System 2.2.3 SAES, RNG, PKA stuck after first stage bootloader (FSBL) decryption A U NA OpenSTLinux distribution: The enabling of SAES is handled within TF-A in OpenSTLinux.

STM32CubeMP13_Package: When another FSBL is used the SAES clock should be enabled in the customer software, even if SAES is not.

DMAMUX 2.4.4 Wrong input DMA request routed upon specific DMAMUX_CxCR register write coinciding with synchronization event A NA U STM32CubeMP13_Package: The customer should provide the right DMAMUX signal polarity configuration when calling the HAL_DMAEx_ConfigMuxSync() function provided in STM32CubeMP13_Package Src/stm32mp1xx_hal_dma_ex.c .
FMC 2.5.1 NOR Flash memory/PSRAM incorrect bus turnaround timing A U OpenSTLinux distribution: Delays to applied by customer device tree.
ADC 2.8.4 ADC_AWDy_OUT reset by non-guarded channels A U U OpenSTLinux distribution: The customer should implement this workaround by configuring only ADC channels that are guarded by a watchdog in the device tree

STM32CubeMP13_Package: The customer should implement this workaround by configuring only ADC channels that are guarded by a watchdog in the application.

LPTIM 2.14.1 Device may remain stuck in LPTIM interrupt when entering Stop mode A NA U OpenSTLinux distribution: The LPTIM interrupt is not used.

STM32CubeMP13_Package: The customer should implement this workaround in MspDeinit().

I2C 2.16.2 Spurious bus error detection in master mode A U U OpenSTLinux distribution: The LPTIM interrupt is not used.

STM32CubeMP13_Package: Issue visible only in interrupt mode, not in DMA mode. Bus Error should be handled by a Timeout at application level.).

4. Workarounds implemented in STM32MP13 ecosystem releases[edit | edit source]

Function Section Limitation Rev.Y Comment
Arm® Cortex®-A7 core 2.1.2 Cache maintenance by set/way operations can execute out of order A I NA OpenSTLinux distribution: Implementation accepted by the community since Linux® kernel v5.3 in arch/arm/Kconfig (refer to ARM_ERRATA_814220).
System 2.2.2 Incorrect reset of glitch-free kernel clock switch P I OpenSTLinux distribution: By default, STPMIC1 performs a VDDCORE reset on NRST activation.
2.2.3 SAES, RNG, PKA stuck after first stage bootloader (FSBL) decryption A U NA OpenSTLinux distribution: The enabling of SAES is handled within TF-A in OpenSTLinux.

STM32CubeMP13_Package: When another FSBL is used the SAES clock should be enabled in the customer software, even if SAES is not.

QUADSPI 2.6.1 Memory-mapped read of last memory byte fails P I
DTS 2.9.1 DTS incorrect operation with LSE as reference clock and PCLK enabled P I
LPTIM 2.14.2 MCU may remain stuck in LPTIM interrupt when clearing event flag P NA I
I2C 2.16.1 Wrong data sampling when data setup time (tSU;DAT) is shorter than one I2C kernel clock period P I I OpenSTLinux distribution: Workaround implemented in device tree with a clock tree that configures the I2C kernel clock source to a frequency higher than 20 MHz.
SPI 2.19.1 Master data transfer stall at system clock much faster than SCK A I I OpenSTLinux distribution: SPI is disabled after each EOT

STM32CubeMP13_Package: SPI is disabled after each EOT.

2.19.3 TXP interrupt occurring while SPI disabled A I I OpenSTLinux distribution: all interrupts are disabled before the SPI is disabled.
ETH 2.22.2 Rx DMA may fail to recover upon DMA restart following a bus error, with Rx timestamping enabled A I OpenSTLinux distribution: Workaround is implemented in stmmac driver. When a bus error is detected, a SW reset is done and all the descriptors are cleared (Rx and Tx), the queues and descriptors are reinitialized
2.22.6 ARP offload function not effective A I
2.22.9 DMA spurious state upon AXI DMA slave bus error P I OpenSTLinux distribution: Workaround is implemented is stmmac drive

5. Workarounds not applicable in STM32MP13 ecosystem releases[edit | edit source]

Function Section Limitation Rev.Y Comment
DMAMUX 2.4.1 SOFx not asserted when writing into DMAMUX_CFR register N NA OpenSTLinux distribution: DMA synchronization event is not used.
2.4.2 OFx not asserted for trigger event coinciding with last DMAMUX request N NA OpenSTLinux distribution: DMA Trigger event is not used.
2.4.3 OFx not asserted when writing into DMAMUX_RGCFR register N NA OpenSTLinux distribution: DMA Trigger event is not used.
2.4.4 Wrong input DMA request routed upon specific DMAMUX_CxCR register write coinciding with synchronization event A NA U OpenSTLinux distribution: DMA synchronization event is not used.
FMC 2.5.2 Incorrect FMC_CLK clock period when CLKDIV value is changed on-the-fly in continuous clock mode A NA OpenSTLinux distribution: CLKDIV can't be changed on-the-fly.
2.5.3 NAND Flash memory IREF/IFEF flags wrongly asserted just after enabling in FMC_IER A NA OpenSTLinux distribution: IREF/IFEF flags are not used.
2.5.4 Command sequencer accesses NAND Flash memory device while PBKEN bit is cleared in FMC_PCR A NA OpenSTLinux distribution: PBKEN bit is set at probe time and never cleared on the flag.
2.5.5 NAND Flash memory IREF flag wrongly asserted after reset A NA
ADC 2.8.1 New context conversion initiated without waiting for trigger when writing new context in ADC_JSQR with JQDIS = 0 and JQM = 0 A NA OpenSTLinux distribution: JQDIS = 1, this issue occurs only when JQDIS = 0.
2.8.2 Two consecutive context conversions fail when writing new context in ADC_JSQR just after previous context completion with JQDIS = 0 and JQM = 0 A NA OpenSTLinux distribution: JQDIS = 1, this issue occurs only when JQDIS = 0.
2.8.3 Unexpected regular conversion when two consecutive injected conversions are performed in Dual interleaved mode A NA OpenSTLinux distribution: Dual mode is not implemented.
2.8.5 Injected data stored in the wrong ADC_JDRx registers A NA OpenSTLinux distribution: Injected conversion not implemented.
2.8.6 ADC slave data may be shifted in Dual regular simultaneous mode A NA OpenSTLinux distribution: Dual mode is not implemented.
SDMMC 2.7.1 Command response and receive data end bits not checked N NA NA Not an issue from SW side as not visible by the SW.
LPTIM 2.14.1 Device may remain stuck in LPTIM interrupt when entering Stop mode A NA U OpenSTLinux distribution: LPTIM interrupt is not used
2.14.2 MCU may remain stuck in LPTIM interrupt when clearing event flag P NA I OpenSTLinux distribution: LPTIM interrupt is not used
RTC and TAMP 2.15.2 Binary mode: SSR is not reloaded with 0xFFFF FFFF when SSCLR = 1 A NA OpenSTLinux distribution: Binary mode is not used
USART 2.17.1 Anticipated end-of-transmission signaling in SPI slave mode A NA OpenSTLinux distribution: SPI slave mode is not implemented
2.17.3 Received data may be corrupted upon clearing the ABREN bit A NA OpenSTLinux distribution: Condition never reached in Linux OS thanks to the specific implementation (ABREN bit never cleaned up in USART_CR2 register).
2.17.4 Noise error flag set while ONEBIT is set A NA OpenSTLinux distribution: Not applicable as Linux Framework doesn't handle the Noise error indication.
SPI 2.19.2 Corrupted CRC return at non-zero UDRDET setting P NA OpenSTLinux distribution: CRC is not supported
2.19.4 Possible corruption of last-received data depending on CRCSIZE setting A NA OpenSTLinux distribution: CRC is not supported
I2C 2.16.4 Transmission stalled after first byte transfer P NA OpenSTLinux distribution: Condition never reached in Linux OS thanks to the specific implementation (TXDR always filled before transmission).
ETH 2.22.3 Spurious receive watchdog timeout interrupt A NA OpenSTLinux distribution: This bug does not affect OpenSTLinux because of the specific implementation of the driver.
2.22.10 Incorrect DMA transfer state in TEB[2:0] and REB[2:0] on bus error A NA OpenSTLinux distribution: No functional impact because only the DMA transfer state is incorrect.
2.22.12 Fatal bus error interrupt not generated when the descriptor posted write is enabled A NA OpenSTLinux distribution: No impact as the register DSPW bit if the ETH_DMAMR register is never used in dwmac driver. It remains set to 0 in any condition.

6. References[edit | edit source]