Last edited 2 years ago

SPI overview

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article gives basic information about the Linux® SPI framework and STM32 SPI driver installation. It explains how to use the SPI and more specifically:

  • how to activate the SPI interface on a Linux® BSP
  • how to access the SPI from kernel space
  • how to access the SPI from user space.

1. Framework purpose[edit | edit source]

The Linux kernel provides a specific framework for SPI[1] protocol support. The SPI (serial peripheral interface) is a synchronous serial communication interface used for short distance communications, mainly in embedded systems.
This interface was created by Motorola and has become a de facto standard. As it is not defined by a consortium such as I2C, there are different signal names and signal polarity modes.
SPI devices communicate either in Full duplex, Half duplex, or Simplex (rx/tx) mode using a master-slave architecture with a single master.

The Linux kernel SPI framework provides a complete support for SPI master (the Linux kernel initiates SPI messaging on the bus) and more recently for SPI slave (the Linux kernel answers to requests from the bus master).

See [2] for an introduction on the Linux kernel SPI framework.

2. System overview[edit | edit source]

The user can add many SPI external devices around the microprocessor device, to create a custom board. Each external device can be accessed through the SPI from the user space or the kernel space.

2.1. Component description[edit | edit source]

2.1.1. Board external SPI devices[edit | edit source]

Master/Slave devices 'X' are physical devices (connected to the STM32 microprocessor via an SPI bus) that behave as slaves or master with respect to the STM32.
The STM32 is the SPI bus controller.
A chip select signal allows selecting independently each device.

2.1.2. STM32 SPI internal peripheral controller[edit | edit source]

The STM32 SPI controller handles any external SPI devices connected to the same bus.
The STM32 microprocessor devices usually embed several instances of the SPI internal peripheral allowing to manage multiple SPI buses.
For more information about STM32 SPI internal peripherals, please refer to SPI main features

2.1.3. STM32 QSPI internal peripheral controller[edit | edit source]

The STM32 QSPI controller can handles external SPI devices connected to the same bus.
For more information about STM32 QSPI internal peripherals, please refer to QUADSPI Peripheral overview

2.1.4. spi-stm32[edit | edit source]

The STM32 SPI controller driver offers an ST SPI internal peripheral abstraction layer to the spi-core.
It defines all the SPI transfer methods to be used by the SPI core base.

2.1.5. spi-core[edit | edit source]

spi-core is the "brain of the communication": it instantiates and manages all buses and peripherals.

  • As stated by its name, this is the SPI engine. It is also in charge of parsing device tree entries both for adapter and devices. It implements the standard SPI modes: 0, 1, 2 and 3.

2.1.6. Device drivers[edit | edit source]

This layer represents all the drivers associated to physical peripherals.

2.1.7. spidev[edit | edit source]

spidev is the interface between the user and the peripheral. This is a kernel driver that offers a unified SPI bus access to the user space application using this dev-interface API. See API Description for examples.

2.1.8. Application[edit | edit source]

The application can control all peripherals thanks to the spidev interface.

2.2. API description[edit | edit source]

2.2.1. User space application[edit | edit source]

The user space application uses a kernel driver (spidev) for SPI transfers through the devfs.
Let's take the example of an SPI device connected to bus B with chip select C. The spidev driver provides the following interfaces:

  • /dev/spidevB.C: character special device created by "udev" that is used by the user space application to control and transfer data to the SPI device.

Supported system calls : open(), close(), read(), write(), ioctl(), llseek(), release().

Supported ioctls commands
Constant Description
SPI_IOC_RD_MODE, SPI_IOC_WR_MODE Gets/sets SPI transfer mode
SPI_IOC_RD_LSB_FIRST, SPI_IOC_WR_LSB_FIRST Gets/sets bit justification used to transfer SPI words.
SPI_IOC_RD_BITS_PER_WORD, SPI_IOC_WR_BITS_PER_WORD Gets/sets the number of bits in each SPI transfer word.
SPI_IOC_RD_MAX_SPEED_HZ, SPI_IOC_WR_MAX_SPEED_HZ Gets/sets the maximum SPI transfer speed in Hz.

The table above shows only the main commands. Additional commands are defined in the framework (see dev-interface API[3] for a complete list).

2.2.2. Kernel space peripheral driver[edit | edit source]

The kernel space peripheral driver communicates with SPI devices and uses the following SPI core API: [4]

3. Configuration[edit | edit source]

3.1. Kernel configuration[edit | edit source]

Enable SPI support (SPI framework and STM32 SPI driver) in the kernel configuration through the Linux Menuconfig tool: Menuconfig or how to configure kernel.

[x] Device Drivers
    [x] SPI support
        *** SPI Master Controller Drivers *** 
        [x] STMicroelectronics STM32 SPI controller
        *** SPI Protocol Masters *** 
        [x] User mode SPI device driver support
        [x] SPI slave protocol handlers

This can be done manually in your kernel:

CONFIG_SPI=y
CONFIG_SPI_MASTER=y
CONFIG_SPI_SLAVE=y
CONFIG_SPI_STM32=y
CONFIG_SPI_SPIDEV=y

Drivers (controller and peripheral) can be compiled as a kernel module (selected by the 'm' kernel configuration file) or directly into the kernel (aka built-in) (selected by the 'y' kernel configuration file).

Information
If a device is involved in the boot process, the drivers required to support it are considered as critical and must be built into the kernel

3.2. Device tree configuration[edit | edit source]

Please refer to SPI device tree configuration.

4. How to use the framework[edit | edit source]

Detailed information on how to write an SPI device driver to control an SPI device are available in the Linux kernel documentation[5].
User-space examples can be found in How to use SPI from Linux userland with spidev.

5. How to trace and debug the framework[edit | edit source]

5.1. How to trace[edit | edit source]

5.1.1. Activating SPI framework debug messages[edit | edit source]

To get verbose messages from the SPI Framework, activate "Debug support for SPI drivers" in the Linux kernel via menuconfig Menuconfig or how to configure kernel.

[x] Device Drivers
    [x] SPI support
        [x] Debug support for SPI drivers

This is done manually in your kernel .config file:

CONFIG_SPI=y
CONFIG_SPI_DEBUG=y
CONFIG_SPI_MASTER=y
...

the debug support for SPI drivers (CONFIG_SPI_DEBUG) compiles all the SPI files located in Linux kernel drivers/spi folder with DEBUG flag.

Information
Reminder: loglevel needs to be increased to 8 by using either boot arguments or the dmesg -n 8 command through the console

5.1.2. Dynamic trace[edit | edit source]

A detailed dynamic trace is available in How to use the kernel dynamic debug

 echo  "file spi* +p" > /sys/kernel/debug/dynamic_debug/control

This command enables all the traces related to the SPI core and drivers at runtime.
A finer selection can be made by choosing only the files to trace.

Information
Reminder: loglevel needs to be increased to 8 by using either boot arguments or the dmesg -n 8 command through the console

5.2. How to debug[edit | edit source]

5.2.1. Detecting SPI configuration[edit | edit source]

5.2.1.1. sysfs[edit | edit source]

When a peripheral is instantiated, the spi-core and the kernel export several files through the sysfs :

  • /sys/class/spi_master/spix shows all the instantiated SPI buses, 'x' being the SPI bus number.
Warning
'x' may not match the SPI internal peripheral index as it depends on device probing order.
  • /sys/bus/spi/devices lists all the instantiated peripherals. For example, the repository named spi0.0 corresponds to the peripheral connected to SPI bus 0 and chip select 0. Below an example representing the "TPM" device:
  • /sys/bus/spi/drivers lists all the instantiated drivers. The tpm_tis_spi/ repository is the driver of TPM 2.0. The spidev/ repository is the generic driver of SPI user mode.
/sys/bus/spi/devices/spi0.0/
            /
            /drivers/tpm_tis_spi/spi0.0/
            /drivers/spidev/...
/sys/class/spi_master/spi0/spi0.0
                     /spi1/
                     /spi2/

5.2.2. devfs[edit | edit source]

If the spidev driver is compiled into the kernel, the repository /dev contains all SPI device entries. They are numbered spix.y where:

  • 'x' is the SPI bus number
  • 'y' is the chip select index on the bus.

Unlike i2c-dev which allows full access to the I2C bus, the spidev offers direct access to the SPI device identified by its chip select signal defined in the device tree node.

Below example shows user mode SPI device on SPI bus 4, chipselect 2.

/dev/spi4.2

For more information, please refer to the spidev documentation [3].

6. Source code location[edit | edit source]

7. References[edit | edit source]