Last edited 2 weeks ago

How to configure, build and deploy TF-M

(Redirected from How to configure TF-M)
Applicable for STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Article purpose[edit | edit source]

This section details the TF-M stage (Trusted Firmware-M). It explains how to configure and build TF-M in the STM32 MPU context, describes the build process from sources, and shows how to deploy it on the target device.

2. Build with a bare environment or STM32CubeIDE[edit | edit source]

2.1. Prerequisites[edit | edit source]

2.1.1. Linux® PC[edit | edit source]

2.1.1.1. Installing the build environment[edit | edit source]

Install the dependencies:

sudo apt-get install -y git curl wget build-essential libssl-dev python3 \
           python3-pip cmake make

Then add the CMake path to the environment:

export PATH=<CMake path>/bin:$PATH
2.1.1.2. Installing a toolchain[edit | edit source]

If using STM32CubeIDE to build TF-M, installing a toolchain is not necessary, since STM32CubeIDE comes with a built-in toolchain.

If using a command-line interface, download the toolchain and add the GNU Arm toolchain path to the environment:

export PATH=$PATH:<toolchain installation directory>/sysroots/x86_64-ostl_sdk-linux/usr/share/gcc-arm-none-eabi/bin

2.1.2. Windows® PC[edit | edit source]

2.1.2.1. Installing the build environment[edit | edit source]

Install the dependencies:

Important
It is recommended to install GNU make in a path without any space characters. Avoid /c/Program Files/, for example.

Then add the CMake path to the environment:

set PATH=<CMake_Path>/bin;%PATH%
2.1.2.2. Installing a toolchain[edit | edit source]

If using STM32CubeIDE to build TF-M, installing a toolchain is not necessary, since STM32CubeIDE comes with a built-in toolchain.

If using a command-line interface, use the toolchain from STM32CubeIDE and update the path in .bashrc as follows:

PATH="/c/ST/<STM32 CubeIDE path>/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.2.202309201523/tools/bin":$PATH
Information
The plugin version may differ from one STM32CubeIDE version to another, so modify it accordingly.

2.2. Installing sources[edit | edit source]

2.2.1. Downloading source[edit | edit source]

For the full-featured software, go to the STMicroelectronics github:

 git clone https://github.com/STMicroelectronics/trusted-firmware-m.git
Warning
The STM32MP2 platform is not upstreamed.

For the record, the official Trusted Firmware-M git repository (without STM32MP2 support) can be downloaded there:

 git clone https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git/
Warning
To run TF-M application with STM32CubeMP2 package, install the TF-M source inside STM32CubeMP2 Package Middlewares/Third_Party/.

2.3. Installing Python dependencies[edit | edit source]

From the TF-M source code installed on the PC:

pip3 install --upgrade pip \
           pip3 install -r tools/requirements.txt

2.4. Build process[edit | edit source]

Important
STMicroelectronics implementation uses the medium profile by default. See TF-M profile page for more information.
Only medium and large profile are supported for M33-TD flavor . Indeed, CONFIG_TFM_SPM_BACKEND set to IPC is mandatory for IPCC mailbox used by SCMI and PSA services. And by definition, CONFIG_TFM_SPM_BACKEND set to SFN is mandatory for small profile.

2.4.1. STM32CubeIDE[edit | edit source]

There is one Cortex®-M33 nonsecure STM32Cube firmware example that uses TF-M services and builds TF-M using STM32CubeIDE.
Refer to the How to build and debug secure project on Cortex-M33 coprocessor in STM32CubeIDE wiki page for a step-by-step build-and-load example with TF-M.

2.4.2. Build command lines[edit | edit source]

You can also use TF-M-tests for the tests and non-secure software example. Starting from ecosystem release v6.1.0 , TF-M is based on official release v2.1, for which build system has changed. You will need to fetch TF-M-tests:

 git clone https://github.com/STMicroelectronics/tf-m-tests.git ${TF-M-TESTS_DIRECTORY}


See the Github pages for compilation steps and the different possible build options for STM32MP257-EV1 or STM32MP215F-DK

2.4.3. External device tree for the STM32MP2 series[edit | edit source]

STMicroelectronics provides device tree configurations for others boards in a dedicated git repository: stm32mp2/a35-td/tfm/ .

The repository can be used to store custom configurations. Use the following command to build with this external dt repository:

 git clone https://github.com/STMicroelectronics/dt-stm32mp.git ${DT_PATH}

Depending on your configuration, you will need to add build options for the external DT files.

For A35-TD flavor and M33-TD flavor , more information is also given on Github pages for STM32MP257-EV1 or STM32MP215F-DK


2.4.3.1. Example for A35-TD flavor [edit | edit source]

DT_PATH can be set to any path, but it must not be a relative path.

       -DDTS_EXT_DIR=${DT_PATH}/stm32mp2/a35-td \
       -DDTS_BOARD_S=tfm/stm32mp257f-ev1-ca35tdcid-ostl-s.dts

And optionally, the nonsecure DT

       -DDTS_BOARD_NS=tfm/stm32mp257f-ev1-ca35tdcid-ostl-ns.dts
2.4.3.2. Example for M33-TD flavor [edit | edit source]

DT_PATH can be set to any path, but it must not be a relative path.

       -DDTS_EXT_DIR=${DT_PATH}/stm32mp2/m33-td \
       -DDTS_BOARD_S=tfm/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-s.dts \
       -DDTS_BOARD_BL2=mcuboot/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-bl2.dts

And optionally, the nonsecure DT

       -DDTS_BOARD_NS=tfm/stm32mp257f-ev1-cm33tdcid-ostl-sdcard-ns.dts

3. Build with Developer package[edit | edit source]

For the A35-TD flavor , only CubeIDE is supported to build TF-M
For the M33-TD flavor , TF-M is managed by Developper package. please refer to the following article to understand how to install & develop: STM32MPU Developer Package

4. Build with Distribution package[edit | edit source]

The Linux Yocto-based distribution package (STM32MPU distribution package) integrates the TF-M components source code in a dedicated recipe in the OpenSTLinux distribution.
To generate the three required binaries for M33TD flavor — **MCUBoot**, **DDR firmware** and **M33 firmware** — use the command:

bitbake m33fw-stm32mp2

If you need to build them individually, use the following commands:

bitbake tf-m-stm32mp 
bitbake m33tdprojects-starter-stm32mp2 
bitbake m33fw-stm32mp2