Last edited 8 months ago

WLAN and Bluetooth hardware component

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines


1. Article purpose[edit | edit source]

The purpose of this article is to:

  • list the WLAN/BT hardware components that might be integrated in the different boards
  • link these components to the corresponding software framework(s)
  • point to the datasheet(s) of these components

2. Software frameworks[edit | edit source]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Networking for STM32MP13x lines  and STM32MP15x lines  : Murata 1DX, for STM32MP25x lines  and STM32MP23x lines  : Murata 1YN, for STM32MP21x lines  : Murata 2BZ WLAN framework

Bluetooth framework

3. Murata 1DX / Murata 1YN / Murata 2BZ[edit | edit source]

  • for STM32MP13x lines  and STM32MP15x lines 

The Type 1DX[1] module is an ultra-small module that includes 2.4 GHz WLAN and Bluetooth functionality. Based on the Cypress CYW4343W (previously Broadcom BCM4343W), the module provides high-efficiency RF front end circuits. The module is designed to fit into small spaces and is smaller than a dime. Minimal external circuitry is required to complete a radio design; add an antenna, a power source, clocks, processor, and associated interface hardware, and the radio hardware design is complete. To ease Wi-Fi certification, the Type 1DX module complies with IEEE 802.11b/g/n and Bluetooth Version 4.1 plus EDR, Power Class 1 (10 dBm max) + BLE.

  • for STM32MP25x lines  and STM32MP23x lines 

The Type 1YN[2] is a small and high performance module based on Infineon CYW43439 combo chipset which supports Wi-Fi® 802.11b/g/n + Bluetooth® 5.2 BR/EDR/LE up to 65Mbps PHY data rate on Wi-fi® and 3Mbps PHY data rate on Bluetooth®. The WLAN section supports SDIO v2.0 interface and the Bluetooth® section supports high-speed 4-wire UART interface and PCM for audio data. The CYW43439 implements highly sophisticated enhanced collaborative coexistence hardware mechanisms and algorithms, which ensure that WLAN and Bluetooth® collaboration is optimized for maximum performance.

  • for STM32MP21x lines 

The Type 2BZ[3] is a small and very high performance module based on Infineon CYW54590 combo chipset which supports Wi-Fi® 802.11a/b/g/n/ac 2×2 MIMO + Bluetooth® 5.2 BR/EDR/LE up to 866Mbps PHY data rate on Wi-Fi® and 3Mbps PHY data rate on Bluetooth®. The WLAN section supports SDIO v3.0 interface and the Bluetooth® section supports high-speed 4-wire UART interface and PCM for audio data. The CYW54590 implements highly sophisticated enhanced collaborative coexistence hardware mechanisms and algorithms, which ensure that WLAN and Bluetooth® collaboration is optimized for maximum performance.

3.1. Linux driver[edit | edit source]

Bindings : Documentation/devicetree/bindings/net/wireless/brcm,bcm4329-fmac.yaml
Documentation/devicetree/bindings/net/broadcom-bluetooth.yaml

Sources: drivers/net/wireless/broadcom/brcm80211/brcmfmac/of.c
drivers/bluetooth/hci_bcm.c

3.1.1. Pre requisite[edit | edit source]

1DX, 1YN and 2BZ chipsets need 2 pieces of firmware to work:

3.1.1.1. Bluetooth[edit | edit source]

The ST Yocto delivery includes the following recipe:
- meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware-bluetooth-bcm4343.bb

  • for STM32MP13x lines  and STM32MP15x lines 

that includes the CYW4343W Firmware which is needed by the driver: CYW43430A1.1DX.hcd (firmware)

  • for STM32MP25x lines  and STM32MP23x lines 

that includes the CYW4343A2 Firmware which is needed by the driver: CYW4343A2_001.003.016.0031.0000.1YN.hcd (firmware)

  • for STM32MP21x lines 

that includes the CYW54590 Firmware which is needed by the driver: BCM4359D0_004.001.016.0241.0275.2BZ.sAnt.hcd (firmware)

If the newest firmware versions are requested, they can be retrieved as described below :
Clone bluetooth firmware from the Murata git repository:

   git clone https://github.com/murata-wireless/cyw-bt-patch
  • for STM32MP13x lines  and STM32MP15x lines 

Copy/Rename CYW43430A1.1DX.hcd file in the target (rename needed to be compliant with the broadcom driver):

   cp CYW43430A1.1DX.hcd $target/rootfs/lib/firmware/brcm/BCM43430A1.hcd
  • for STM32MP25x lines  and STM32MP23x lines 

Copy/Rename CYW4343A2_001.003.016.0031.0000.1YN.hcd file in the target (rename needed to be compliant with the broadcom driver):

   cp CYW4343A2_001.003.016.0031.0000.1YN.hcd $target/rootfs/lib/firmware/brcm/BCM4343A2.hcd
  • for STM32MP21x lines 

Copy/Rename BCM4359D0_004.001.016.0241.0275.2BZ.sAnt.hcd file in the target (rename needed to be compliant with the broadcom driver):

   cp BCM4359D0_004.001.016.0241.0275.2BZ.sAnt.hcd $target/rootfs/lib/firmware/brcm/BCM.st,stm32mp215f-dk.hcd
3.1.1.2. WLAN[edit | edit source]

The ST Yocto delivery includes the following recipes:
- openembedded-core/meta/recipes-kernel/linux-firmware/linux-firmware_git.bb
- meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware_git.bbappend

  • for STM32MP13x lines  and STM32MP15x lines 

These provide the CYW4343W firmware and calibration data needed by the wlan driver: brcmfmac43430-sdio.bin (firmware), and brcmfmac43430-sdio.txt (calibration data file)

  • for STM32MP25x lines  and STM32MP23x lines 

These provide the CYW43439 firmware and calibration data needed by the wlan driver: brcmfmac43439-sdio.bin (firmware), and brcmfmac43439-sdio.txt (calibration data file)

  • for STM32MP21x lines 

These provide the CYW54590 firmware and calibration data needed by the wlan driver: cyfmac54591-sdio.bin (firmware), and cyfmac54591-sdio.3ant.2BZ.txt (calibration data file) If the newest firmware versions are requested, they can be retrieved as described below:

Clone brcm firmware from kernel.org git repository:

   git clone git://git.kernel.org/pub/scm/linux/kernel/git/firmware/linux-firmware.git

Firmware is available in the linux-firmware/brcm folder:

  • for STM32MP13x lines  and STM32MP15x lines 
   cp linux-firmware/brcm/brcmfmac43430-sdio.* $target/rootfs/lib/firmware/brcm/
  • for STM32MP25x lines  and STM32MP23x lines 
   cp linux-firmware/brcm/brcmfmac43439-sdio.* $target/rootfs/lib/firmware/brcm/
  • for STM32MP21x lines 
   cp linux-firmware/brcm/cyfmac54591-sdio.* $target/rootfs/lib/firmware/brcm/
  • for STM32MP13x lines  and STM32MP15x lines , at startup, the MURATA 1DX module is loaded and you should see the following dmesg output:
[   67.306154] brcmfmac: brcmf_c_preinit_dcmds: Firmware version = wl0: Aug  6 2017 23:19:25 version 7.45.98.30 (r666241 CY) FWID 01-f0b000
[   67.326146] brcmfmac: brcmf_c_preinit_dcmds: CLM version = API: 12.2 Data: 7.11.15 Compiler: 1.24.2 ClmImport: 1.24.1 Creation: 2014-05 
[   67.676323] brcmfmac: brcmf_cfg80211_reg_notifier: not a ISO3166 code (0x30 0x30)
  • for STM32MP25x lines  and STM32MP23x lines , at startup, the MURATA 1YN module is loaded and you should see the following dmesg output:
[   96.840123] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM43439/5 wl0: Aug 31 2023 01:16:08 version 7.95.64.1 (64b6b2d CY) FWID 01-b73af1f1
  • for STM32MP21x lines  at startup, the MURATA 2BZ module is loaded and you should see the following dmesg output:
  16.789022] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac4355-sdio for chip BCM4355/13
[   17.174514] brcmfmac: brcmf_c_process_txcap_blob: no txcap_blob available (err=-2)
[   17.177774] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4355/13 wl0: Oct 29 2024 19:35:59 version 13.35.369 (65bac01 CY) FWID 01-fa235e7e

[   17.737284] Bluetooth: hci0: BCM: chip id 143
[   17.742151] Bluetooth: hci0: BCM: features 0x0f
[   17.744083] Bluetooth: hci0: BCM4359D0
[   17.744838] Bluetooth: hci0: BCM (004.001.016) build 0000
[   17.760102] Bluetooth: hci0: BCM 'brcm/BCM.st,stm32mp215f-dk.hcd' Patch
[   19.039573] Bluetooth: hci0: BCM: features 0x0f
[   19.041473] Bluetooth: hci0: CYW54591 MURATA Type1XA sLNA 00534335 0241
[   19.045389] Bluetooth: hci0: BCM (004.001.016) build 0275
[   21.671837] Bluetooth: MGMT ver 1.22

4. References[edit | edit source]

  1. ↑ [1], 1DX
  2. ↑ [2], 1YN
  3. ↑ [3], 2BZ
  • Kernel.org wiki

https://wireless.wiki.kernel.org/en/users/drivers/brcm80211