Last edited 11 months ago

IPCC internal peripheral

Applicable for STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

1. Article purpose[edit | edit source]

The purpose of this article is to:

  • briefly introduce the IPCC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit | edit source]

The IPCC (inter-processor communication controller) peripheral is used to exchange data between two processors. It provides a non blocking signaling mechanism to post and retrieve information in an atomic way. Note that shared memory buffers are allocated in the MCU SRAM, which is not part of the IPCC block.

The IPCC peripheral provides a hardware support to manage inter-processor communication between two processor instances. Each processor owns specific register bank and interrupts.

The IPCC provides the signaling for bidirectional channels.

Each channel is divided into two subchannels that offer a unidirectional signaling from the "sender" processor to the "receiver" processor:

  • P1_TO_P2 subchannel
  • P2_TO_P1 subchannel

A subchannel consists in:

  • One flag that toggles between occupied and free: the flag is set to occupied by the "sender" processor and cleared by the "receiver" processor.
  • Two associated interrupts (shared with the other channels):
    • RXO: RX channel occupied, connected to the "receiver" processor.
    • TXF: TX channel free, connected to the "sender" processor.
  • Two associated interrupt masks multiplexing channel IRQs.



The IPCC supports the following channel operating modes:

  • Simplex communication mode:
    • Only one subchannel is used.
    • Unidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated.
  • Half-duplex communication mode:
    • Only one subchannel is used.
    • Bidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated and the response is available in shared memory.
  • Full-duplex communication mode:
    • The subchannels are used in Asynchronous mode.
    • Any processor can post asynchronously a message by setting the subchannel status flag to occupied. The "receiver" processor clears the flag when the message is treated. This mode can be considered as a combination of two simplex modes on a given channel.

Refer to the reference manuals[1][2] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit | edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the FwST-M Package running on the Arm® Cortex®-M processor.

3.1. Processor interface assignment[edit | edit source]

3.1.1. On STM32MP15x lines [edit | edit source]

STMicroelectronics distribution uses the IPCC peripheral for inter-processor communication with the following configuration:

  • The IPCC processor 1 interface (PROC1)is assigned to the Arm® Cortex®-A7, nonsecure context.
  • The IPCC processor 2 interface (PROC2) is assigned to the Arm® Cortex®-M4 context.

3.1.2. On STM32MP21x lines  and STM32MP23x lines [edit | edit source]

The IPCC1 peripheral is dedicated for the communication between the Arm® Cortex®-A35 and the Arm® Cortex®-M33. The interfaces are assigned in hardware to the Cortexes :

    • The processor 1 interface (PROC1) is assigned by hardware to the Arm® Cortex®-A35, secure and nonsecure context.
    • The processor 2 interface (PROC2) is assigned by hardware to the Arm® Cortex®-M33, secure and nonsecure context.

3.1.3. On STM32MP25x lines [edit | edit source]

  • The IPCC1 peripheral is dedicated for the communication between the Arm® Cortex®-A35 and the Arm® Cortex®-M33. The interfaces are assigned in hardware to the Cortexes :
    • The processor 1 interface (PROC1) is assigned by hardware to the Arm® Cortex®-A35, secure and nonsecure context.
    • The processor 2 interface (PROC2) is assigned by hardware to the Arm® Cortex®-M33, secure and nonsecure context.
  • The IPCC2 peripheral is dedicated for the communication between the Arm® Cortex®-A35 or the Arm® Cortex®-M33 and the Arm® Cortex®-M0+.
    • The processor 1 interface (PROC1) is assigned by hardware to the Arm® Cortex®-M0+.
    • The processor 2 interface (PROC2) is assignable to the Arm® Cortex®-A35 or the Arm® Cortex®-M33, secure and nonsecure context.

3.2. Boot time assignment[edit | edit source]

3.2.1. On STM32MP15x lines [edit | edit source]

The IPCC peripheral is not utilized during boot time in the OpenSTlinux distribution.

3.2.2. On STM32MP21x lines  and STM32MP23x lines [edit | edit source]

3.2.2.1. For A35-TD flavor [edit | edit source]

The IPCC peripheral is not utilized during boot time in the OpenSTlinux distribution.


Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the IPCC1 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
CPU1 channel 1 ⬚ ⬚
CPU1 channel 2 ⬚ ⬚
CPU1 channel 3 ⬚ ⬚
CPU1 channel 4 ⬚ ⬚
CPU1 channel 5 ⬚ ⬚
CPU1 channel 6 ⬚ ⬚
CPU1 channel 7 ⬚ ⬚
CPU1 channel 8 ⬚ ⬚
CPU1 channel 9 ⬚ ⬚
CPU1 channel 10 ⬚ ⬚
CPU1 channel 11 ⬚ ⬚
CPU1 channel 12 ⬚ ⬚
CPU1 channel 13 ⬚ ⬚
CPU1 channel 14 ⬚ ⬚
CPU1 channel 15 ⬚ ⬚
CPU1 channel 16 ⬚ ⬚
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4
CPU2 channel 5
CPU2 channel 6
CPU2 channel 7
CPU2 channel 8
CPU2 channel 9
CPU2 channel 10
CPU2 channel 11
CPU2 channel 12
CPU2 channel 13
CPU2 channel 14
CPU2 channel 15
CPU2 channel 16
3.2.2.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the IPCC1 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
CPU1 channel 1 ⬚ ⬚
CPU1 channel 2 ⬚ ⬚
CPU1 channel 3 ⬚ ⬚
CPU1 channel 4 ⬚ ⬚
CPU1 channel 5 ⬚ ⬚
CPU1 channel 6 ⬚ ⬚
CPU1 channel 7 ⬚ ⬚
CPU1 channel 8 ⬚ ⬚
CPU1 channel 9 ⬚ ⬚
CPU1 channel 10 ⬚ ⬚
CPU1 channel 11 ⬚ ⬚
CPU1 channel 12 ⬚ ⬚
CPU1 channel 13 ⬚ ⬚
CPU1 channel 14 ⬚ ⬚
CPU1 channel 15 ⬚ ⬚
CPU1 channel 16 ⬚ ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 1 ⬚
CPU2 channel 2 ⬚
CPU2 channel 3 ⬚
CPU2 channel 4 ⬚
CPU2 channel 5 ⬚
CPU2 channel 6 ⬚
CPU2 channel 7 ⬚
CPU2 channel 8 ⬚
CPU2 channel 9 ⬚
CPU2 channel 10 ⬚
CPU2 channel 11 ⬚
CPU2 channel 12 ⬚
CPU2 channel 13 ⬚
CPU2 channel 14 ⬚
CPU2 channel 15 ⬚
CPU2 channel 16 ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)

3.2.3. On STM32MP25x lines [edit | edit source]

3.2.3.1. For A35-TD flavor [edit | edit source]

The IPCC peripherals are not utilized during boot time in the OpenSTlinux distribution.


Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the IPCC1 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
CPU1 channel 1 ⬚ ⬚
CPU1 channel 2 ⬚ ⬚
CPU1 channel 3 ⬚ ⬚
CPU1 channel 4 ⬚ ⬚
CPU1 channel 5 ⬚ ⬚
CPU1 channel 6 ⬚ ⬚
CPU1 channel 7 ⬚ ⬚
CPU1 channel 8 ⬚ ⬚
CPU1 channel 9 ⬚ ⬚
CPU1 channel 10 ⬚ ⬚
CPU1 channel 11 ⬚ ⬚
CPU1 channel 12 ⬚ ⬚
CPU1 channel 13 ⬚ ⬚
CPU1 channel 14 ⬚ ⬚
CPU1 channel 15 ⬚ ⬚
CPU1 channel 16 ⬚ ⬚
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4
CPU2 channel 5
CPU2 channel 6
CPU2 channel 7
CPU2 channel 8
CPU2 channel 9
CPU2 channel 10
CPU2 channel 11
CPU2 channel 12
CPU2 channel 13
CPU2 channel 14
CPU2 channel 15
CPU2 channel 16

The below table shows the possible boot time allocations for the features of the IPCC2 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
CPU1 channel 1 ⬚ ⬚
CPU1 channel 2 ⬚ ⬚
CPU1 channel 3 ⬚ ⬚
CPU1 channel 4 ⬚ ⬚
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4
3.2.3.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given boot time context.
  • ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the IPCC1 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
CPU1 channel 1 ⬚ ⬚
CPU1 channel 2 ⬚ ⬚
CPU1 channel 3 ⬚ ⬚
CPU1 channel 4 ⬚ ⬚
CPU1 channel 5 ⬚ ⬚
CPU1 channel 6 ⬚ ⬚
CPU1 channel 7 ⬚ ⬚
CPU1 channel 8 ⬚ ⬚
CPU1 channel 9 ⬚ ⬚
CPU1 channel 10 ⬚ ⬚
CPU1 channel 11 ⬚ ⬚
CPU1 channel 12 ⬚ ⬚
CPU1 channel 13 ⬚ ⬚
CPU1 channel 14 ⬚ ⬚
CPU1 channel 15 ⬚ ⬚
CPU1 channel 16 ⬚ ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 1 ⬚
CPU2 channel 2 ⬚
CPU2 channel 3 ⬚
CPU2 channel 4 ⬚
CPU2 channel 5 ⬚
CPU2 channel 6 ⬚
CPU2 channel 7 ⬚
CPU2 channel 8 ⬚
CPU2 channel 9 ⬚
CPU2 channel 10 ⬚
CPU2 channel 11 ⬚
CPU2 channel 12 ⬚
CPU2 channel 13 ⬚
CPU2 channel 14 ⬚
CPU2 channel 15 ⬚
CPU2 channel 16 ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)

The below table shows the possible boot time allocations for the features of the IPCC2 instance.

Feature Boot time allocation Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Cortex-M33
secure
(MCUboot)
CPU1 channel 1 ⬚ ⬚ ⬚
CPU1 channel 2 ⬚ ⬚ ⬚
CPU1 channel 3 ⬚ ⬚ ⬚
CPU1 channel 4 ⬚ ⬚ ⬚
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4

3.3. Runtime assignment[edit | edit source]

It does not make sense to allocate the IPCC to a single runtime execution context. It is consequently enabled by default for both cores in the STM32CubeMX.

3.3.1. On STM32MP15x lines [edit | edit source]

Click on to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
nonsecure
(Linux)
Cortex-M4

(STM32Cube)
Coprocessor IPCC IPCC ☑ ☑ Shared (none or both)
Processor interface Context Comment
Cortex-A7 nonsecure
(Linux)
Cortex-M4
(STM32Cube)
PROC1 channel 1 ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
PROC1 channel 2 ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
PROC1 channel 3 ☑ Simplex communication used by the remote framework to request the Cortex-M4 to shutdown.
PROC1 channel 4 ☐
PROC1 channel 5 ☐
PROC1 channel 6 ☐
PROC2 channel 1 ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
PROC2 channel 2 ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
PROC2 channel 3 ☑ Simplex communication used by the remote framework to request the Cortex-M4 to shutdown.
PROC2 channel 4 ☐
PROC2 channel 5 ☐
PROC2 channel 6 ☐


3.3.2. On STM32MP21x lines  and STM32MP23x lines [edit | edit source]

3.3.2.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP21 internal peripherals
STM32MP23 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP21 reference manuals and in STM32MP23 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the IPCC1 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
CPU1 channel 2 ☐OP-TEE ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treate
CPU1 channel 3 ☐OP-TEE ☑ Simplex communication used by the remote framework to request the Cortex-M33 to shutdown.
CPU1 channel 4 ☐OP-TEE ☐
CPU1 channel 5 ☐OP-TEE ☐
CPU1 channel 6 ☐OP-TEE ☐
CPU1 channel 7 ☐OP-TEE ☐
CPU1 channel 8 ☐OP-TEE ☐
CPU1 channel 9 ☐OP-TEE ☐
CPU1 channel 10 ☐OP-TEE ☐
CPU1 channel 11 ☐OP-TEE ☐
CPU1 channel 12 ☐OP-TEE ☐
CPU1 channel 13 ☐OP-TEE ☐
CPU1 channel 14 ☐OP-TEE ☐
CPU1 channel 15 ☐OP-TEE ☐
CPU1 channel 16 ☑OP-TEE ☐ SCMI for system resource configuration controlled by the Cortex-A35 secure (OPTEE)
CPU2 channel 1 ☐ ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated|-
CPU2 channel 2 ☐ ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
CPU2 channel 3 ☐ ☑ Simplex communication used by the remote framework to request the Cortex-M4 to shutdown.
CPU2 channel 4 ☐ ☐
CPU2 channel 5 ☐ ☐
CPU2 channel 6 ☐ ☐
CPU2 channel 7 ☐ ☐
CPU2 channel 8 ☐ ☐
CPU2 channel 9 ☐ ☐
CPU2 channel 10 ☐ ☐
CPU2 channel 11 ☐ ☐
CPU2 channel 12 ☐ ☐
CPU2 channel 13 ☐ ☐
CPU2 channel 14 ☐ ☐
CPU2 channel 15 ☐ ☐
CPU2 channel 16 ☐ ☑ SCMI for system resource configuration controlled by the Cortex-A35 secure (OPTEE)
3.3.2.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP21 internal peripherals
STM32MP23 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP21 reference manuals and in STM32MP23 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the IPCC1 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
CPU1 channel 2 ☐OP-TEE ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treate
CPU1 channel 3 ☐OP-TEE ☑ Simplex communication used by the remote framework to request the Cortex-M33 to shutdown.
CPU1 channel 4 ☐OP-TEE ☐
CPU1 channel 5 ☐OP-TEE ☐
CPU1 channel 6 ☐OP-TEE ☐
CPU1 channel 7 ☐OP-TEE ☐
CPU1 channel 8 ☐OP-TEE ☐
CPU1 channel 9 ☐OP-TEE ☐
CPU1 channel 10 ☐OP-TEE ☐
CPU1 channel 11 ☐OP-TEE ☐
CPU1 channel 12 ☐OP-TEE ☐
CPU1 channel 13 ☐OP-TEE ☐
CPU1 channel 14 ☑TF-A ☐ PSA service for platform secure architecture service controlled by the Cortex-M33 secure (TF-M)
CPU1 channel 15 ☑OP-TEE ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU1 channel 16 ☐OP-TEE ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 1 ☐ ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated|-
CPU2 channel 2 ☐ ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
CPU2 channel 3 ☐ ☑ Simplex communication used by the remote framework to request the Cortex-M4 to shutdown.
CPU2 channel 4 ☐ ☐
CPU2 channel 5 ☐ ☐
CPU2 channel 6 ☐ ☐
CPU2 channel 7 ☐ ☐
CPU2 channel 8 ☐ ☐
CPU2 channel 9 ☐ ☐
CPU2 channel 10 ☐ ☐
CPU2 channel 11 ☐ ☐
CPU2 channel 12 ☐ ☐
CPU2 channel 13 ☐ ☐
CPU2 channel 14 ☑ ☐ PSA service for platform secure architecture service controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 15 ☑ ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 16 ☑ ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)

3.3.3. On STM32MP25x lines [edit | edit source]

3.3.3.1. For A35-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the IPCC1 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
CPU1 channel 2 ☐OP-TEE ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treate
CPU1 channel 3 ☐OP-TEE ☑ Simplex communication used by the remote framework to request the Cortex-M33 to shutdown.
CPU1 channel 4 ☐OP-TEE ☐
CPU1 channel 5 ☐OP-TEE ☐
CPU1 channel 6 ☐OP-TEE ☐
CPU1 channel 7 ☐OP-TEE ☐
CPU1 channel 8 ☐OP-TEE ☐
CPU1 channel 9 ☐OP-TEE ☐
CPU1 channel 10 ☐OP-TEE ☐
CPU1 channel 11 ☐OP-TEE ☐
CPU1 channel 12 ☐OP-TEE ☐
CPU1 channel 13 ☐OP-TEE ☐
CPU1 channel 14 ☐OP-TEE ☐
CPU1 channel 15 ☐OP-TEE ☐
CPU1 channel 16 ☑OP-TEE ☐ SCMI for system resource configuration controlled by the Cortex-A35 secure (OPTEE)
CPU2 channel 1 ☐ ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated|-
CPU2 channel 2 ☐ ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
CPU2 channel 3 ☐ ☑ Simplex communication used by the remote framework to request the Cortex-M33 to shutdown.
CPU2 channel 4 ☐ ☐
CPU2 channel 5 ☐ ☐
CPU2 channel 6 ☐ ☐
CPU2 channel 7 ☐ ☐
CPU2 channel 8 ☐ ☐
CPU2 channel 9 ☐ ☐
CPU2 channel 10 ☐ ☐
CPU2 channel 11 ☐ ☐
CPU2 channel 12 ☐ ☐
CPU2 channel 13 ☐ ☐
CPU2 channel 14 ☐ ☐
CPU2 channel 15 ☐ ☐
CPU2 channel 16 ☐ ☑ SCMI for system resource configuration controlled by the Cortex-A35 secure (OPTEE)

The below table shows the possible runtime allocations for the features of the IPCC2 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☑ ☐ ☐ Interprocessor communication
CPU1 channel 2 ☐OP-TEE ☑ ☐ ☐ Simplex communication used by the remote framework to request the Cortex-M0+ to shutdown.
CPU1 channel 3 ☐OP-TEE ☐ ☐ ☐
CPU1 channel 4 ☐OP-TEE ☐ ☐ ☐
CPU2 channel 1 ☑ Interprocessor communication
CPU2 channel 2 ☑ Simplex communication used by the remote framework to request the Cortex-M0+ to shutdown.
CPU2 channel 3 ☐
CPU2 channel 4 ☐
3.3.3.2. For M33-TD flavor [edit | edit source]

Click on to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by the OpenSTLinux BSP:

  • ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • ☐ means that the peripheral can be assigned to the given runtime context.
  • ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Coprocessor IPCC IPCC1 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the IPCC1 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
CPU1 channel 2 ☐OP-TEE ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treate
CPU1 channel 3 ☐OP-TEE ☑ Simplex communication used by the remote framework to request the Cortex-A to shutdown.
CPU1 channel 4 ☐OP-TEE ☐
CPU1 channel 5 ☐OP-TEE ☐
CPU1 channel 6 ☐OP-TEE ☐
CPU1 channel 7 ☐OP-TEE ☐
CPU1 channel 8 ☐OP-TEE ☐
CPU1 channel 9 ☐OP-TEE ☐
CPU1 channel 10 ☐OP-TEE ☐
CPU1 channel 11 ☐OP-TEE ☐
CPU1 channel 12 ☐OP-TEE ☐
CPU1 channel 13 ☐OP-TEE ☐
CPU1 channel 14 ☑TF-A ☐ PSA service for platform secure architecture service controlled by the Cortex-M33 secure (TF-M)
CPU1 channel 15 ☑TF-A ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU1 channel 16 ☐OP-TEE ☑ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 1 ☐ ☑ RPMsg transfer from Cortex-M to Cortex-A

Full-duplex communication:

  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
CPU2 channel 2 ☐ ☑ RPMsg transfer from Cortex-A to Cortex-M

Full-duplex communication:

  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
CPU2 channel 3 ☐ ☑ Simplex communication used by the remote framework to request the Cortex-A to shutdown.
CPU2 channel 4 ☐ ☐
CPU2 channel 5 ☐ ☐
CPU2 channel 6 ☐ ☐
CPU2 channel 7 ☐ ☐
CPU2 channel 8 ☐ ☐
CPU2 channel 9 ☐ ☐
CPU2 channel 10 ☐ ☐
CPU2 channel 11 ☐ ☐
CPU2 channel 12 ☐ ☐
CPU2 channel 13 ☐ ☐
CPU2 channel 14 ☑ ☐ PSA service for platform secure architecture service controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 15 ☑ ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)
CPU2 channel 16 ☑ ☐ SCMI for system resource configuration controlled by the Cortex-M33 secure (TF-M)

The below table shows the possible runtime allocations for the features of the IPCC2 instance.

Feature Runtime allocation Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
CPU1 channel 1 ☐OP-TEE ☐ ☐ ☐
CPU1 channel 2 ☐OP-TEE ☐ ☐ ☐
CPU1 channel 3 ☐OP-TEE ☐ ☐ ☐
CPU1 channel 4 ☐OP-TEE ☐ ☐ ☐
CPU2 channel 1 ☐
CPU2 channel 2 ☐
CPU2 channel 3 ☐
CPU2 channel 4 ☐

4. Software frameworks and drivers[edit | edit source]

Below are listed the software frameworks and drivers managing the IPCC peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit | edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.The IPCC peripheral is shared between the Arm Cortex-A and Cortex-M contexts. A particular attention must therefore be paid to have a complementary configuration on both contexts.