Last edited 8 months ago

STM32MP257x-EV1 - hardware description

Applicable for STM32MP25x lines

This article provides an overview of STM32MP257x-EV1 Evaluation boards.

1. Article purpose[edit | edit source]

This article briefly describes:

  • How to assemble the different elements provided in the commercial box
  • The different components on the boards
  • How to connect the boards to external material
  • How to configure the board for boot
  • The configurations of the connector pins

This article is valid for the STM32MP257F-EV1 Evaluation boards: the part numbers are specified in the STM32MP25 microprocessor part numbers article.

Information
This article is an introduction to the STM32MP257x-EV1 Evaluation board. For more detailed information, refer to the STM32MP257x-EV1 Evaluation boards user manuals.

2. Board assembly[edit | edit source]

The STM32MP257x-EV1 Evaluation board packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include the items listed below.

STM32MP257F-EV1 shown here (picture is not contractual)
Position Description
1 MB1936 main board
2 B-LVDS7-WSVGA 7” LVDS WSVGA display module with touch panel (optional)
3 LVDS display cable, provided with the B-LVDS7-WSVGA package (optional)
4 B-CAMS-IMX MB1854 MIPI CSI-2 camera board (optional)
5 Camera board FFC, provided with the B-CAMS-IMX package (optional)


B-LVDS7-WSVGA display and B-CAMS-IMX camera are available for purchase to complete the setup.

The complete set looks like this:

STM32MP257x-EV1 Evaluation board assembly
STM32MP257F-EV1 shown here (picture is not contractual)

2.1. Connecting the LVDS display to the board[edit | edit source]

Display board assembly (picture is not contractual)
  • Check the cable orientation shown above using the black mark and the white twisted pairs.
  • Find the LVDS ports on the STM32MP257x-EV1 Evaluation board (CN2) and the display (CN1). The LVDS display box contains one cable.
  • Insert the cable into each port as shown below:
Display board assembly (picture is not contractual)

2.2. Connecting the MB1854 camera board to the board[edit | edit source]

Camera board assembly (picture is not contractual)
  • Find the camera ports on the STM32MP257x-EV1 Evaluation board (CN4) and MB1854 (CN1). One FFC is provided in the camera box.
  • For each port:
    • Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the black plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)

2.3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]


STM32MP257x-EV1 Evaluation board assembled
STM32MP257F-EV1 shown here (picture is not contractual)



3. Board overview[edit | edit source]

Main board MB1936, revision D : part of the STM32MP257x-EV1 Evaluation board .

Information
It is highly recommended to work with a main board MB1936, revision D instead of a main board MB1936, revision C-01, because the latter presents the following restrictions:
  • Low-power modes are not functional
  • HDMI to DSI bridge B-LCDAD-HDMI1 is not functional


Position Description Position Description
1 (LED1) User LED (blue) [* 1] 2 (LD1) User LED (red) [* 1]
3 (LD2) User LED (orange) [* 1] 4 (LD3) User LED (green) [* 1]
5 (B1) RESET button 6 (B2) WAKE UP button
7(B3) TAMPER button 8 (B4) USER2 button
9 (B5) USER1 button 10 (CN2) LVDS connector
11(CN4) CSI connector 12(CN3) DSI connector
13 (CN1) microSD™ card connector 14 (SW1) Boot mode selection
15 (U22) S-NOR 512Mb 16 (CN5) GPIO expansion connector
17 (CN9) FDCAN1 18 (CN11) FDCAN2
19 (U26) STPMIC25 20 (U27) STM32MP257
21 (U24) eMMC 4GB 22 (U29) DDR4 2GB
23(U28) DDR4 2GB 24 (CN10) PWR measurements connector
25 (CN22) MIPI10 connector 26 (CN13) Mini-PCIe connector
27 (JP4) Power jumper 28 (CN20) 5V/3A power supply jack
29 (CN21) USB Power - ST-LINK Type-C 30 (CN16) ETHERNET 2 / PHY ETH2
31 (CN17) ETHERNET 1 / PHY ETH1 32 (CN18) ETHERNET 3 / PHY ETH3
33 (CN19) Dual USB Host TypeA 34 (CN15) USB2.0 DRD Type-C
35 (LD7) Ethernet LED (green)[* 2] 36 (LD8) Ethernet LED (green)[* 2]
37 (LD9) Ethernet LED (green)[* 2] 38 (LD11) Power LED (green)[* 3]
39 (LD5) ST-LINK/V3-1 LED (bicolor)[* 4] - -

Details about the LEDs:

  1. ↑ 1.0 1.1 1.2 1.3 LD2, LD3, LD4, LD5 (MB1936): some user LEDs are used to reflect the system activity, while others are left free for use by the application, as explained in the LEDs and buttons on STM32 MPU boards article.
  2. ↑ 2.0 2.1 2.2 LD7, LD8, LD9 (MB1936): these LEDs blink in green when an Ethernet connection has been established
  3. ↑ LD11 (MB1936): turns green when a power connection has been established.
  4. ↑ LD6 (MB1263): blinks in red if the ST-LINK/V3-1 connection was not established, otherwise it is green.
STM32MP257x-EV1 Evaluation board front side
STM32MP257F-EV1 shown here (picture is not contractual)


STM32MP257x-EV1 Evaluation board back side
STM32MP257A-EV1 shown here (picture is not contractual)


Position Description
40 (CN25) mikroBUS™ connector


4. Board connection[edit | edit source]

The images below shows the recommended connections for getting started with the STM32MP257x-EV1 Evaluation boards. As shown in the board overview, other connectors are available for this board (for example, CAN).




USB Power Delivery Type-C (Power or STLINK)ETHERNET 2/PHY ETH2 (Ethernet)2 x USB type A (host) (such as a mouse or keyboard USB driver)USB2.0 DRD Type-C  (programmable through CubeProgrammer)microSD<sup>™</sup> card slotMB1936 5V/3A power supply jack (Power)RESET button
STM32MP257x-EV1 Evaluation board connections

STM32MP257F-EV1 shown here (picture is not contractual)
Warning
If the supply is provided via the USB Power Delivery Type-C (1), to have the possibility to use ST-Link or the consoles, the USB Power Delivery Type-C (1) must be connected to a PC with USB Type-C/Type-C cable. The USB Type-C on the PC must be a USB Power Delivery Type-C.
Information
Via ST-LINK, it is possible to have access to 2 consoles: one for Cortex-M and one for Cortex-A.


5. Switches and jumpers[edit | edit source]

Most of the default settings for the switches and jumpers must be kept as they are in the commercial box.

There are two exceptions:

  • The jumpers related to power
  • The switches related to boot

The sections below provide further details for the main boot switches and power jumpers.

5.1. Power jumper[edit | edit source]

Depending on the positions presented in the table below, the power jumper (JP4) provides the the MB1936 board with either:

  • A 5V/3A power supply unit (not provided with the STM32MP25 Evaluation board package) on the jack CN20
  • A USB PD Type-C CN21 (USB cable not provided with the STM32MP25 Evaluation board package)
Jumper Setting Configuration
JP4 JP[1-2] Select the USB Power Delivery Type-C CN21 as the main board supply (USB Type-C cable)
JP4[2-3] Select the 5V/3A power supply unit on jack CN20 as the main board supply
MB1936 board supplied via USB Power Type-C CN21 (picture is not contractual)


MB1936 board supplied via 5V/3A power supply unit CN20 (picture is not contractual)


5.2. Boot-related switches[edit | edit source]

The STM32MP257x-EV1 Evaluation boards can boot from different flash memory devices (such as microSD, eMMC, or serial NOR) based on ROM code selection; using the microSD card is recommended.


Boot mode Boot 0 Boot 1 Boot 2 Boot 3 Boot-related switches for (SW1 on the board overview picture) Boot device used for the Cortex-A35 Boot device used for the Cortex-M33
Forced serial boot for flash memory programming 0 0 0 0
Boot from UART/USB
UART/USB
for programming
NA
Boot from microSD card for A35-TD flavor 1 0 0 0
microSD NA
Boot from eMMC for A35-TD flavor 0 1 0 0
eMMC NA
Boot from NOR for A35-TD flavor 0 0 1 0
serial NOR NA
Boot from NOR for M33-TD flavor 1 1 0 1
serial NOR serial NOR
Boot from microSD card for M33-TD flavor 1 1 1 0
microSD card microSD card
Boot from eMMC for M33-TD flavor 0 0 0 1
eMMC eMMC
Boot from NOR and eMMC for M33-TD flavor 1 0 1 1
eMMC serial NOR
Boot from NOR and microSD card for M33-TD flavor 0 1 1 1
microSD card serial NOR
Developer mode 1 1 0 0
Development mode
NA NA

When the switch is set to the "OPEN" position, the BOOTx value is "0"; otherwise it is "1".

6. GPIO mapping[edit | edit source]


6.1. GPIO expansion connector[edit | edit source]

The table below describes the pins of the GPIO expansion connector (CN5 in the board overview image):

Function STM32 pin Pin Pin STM32 pin Function
3V3 - 1 2 - 5V
GPIO2 / I2C8_SDA PZ3 3 4 - 5V
GPIO3 / I2C8_SDL PZ4 5 6 - GND
GPIO4 / MCO1 PF11 7 8 PF13 GPIO14 / USART6_TX
GND - 9 10 PF14 GPIO15 / USART6_RX
GPIO17 / USART6_RTS PG5 11 12 PJ11 GPIO18 / SAI2_SCKA
GPIO27 / SDMMC3_D3 PI11 13 14 - GND
GPIO22 / SDMMC3_CK PB13 15 16 PD12 GPIO23 / SDMMC3_CMD
3V3 - 17 18 PB14 GPIO24 / SDMMC3_D0
GPIO10 / SPI3_MOSI PB8 19 20 - GND
GPIO9 / SPI3_MISO PB10 21 22 PD13 GPIO25 / SDMMC3_D1
GPIO11 / SPI3_SCK PB7 23 24 PB1 GPIO8 / SPI3_NSS
GND - 25 26 PJ1 GPIO7
ID_SD/I2C2_SDA PB4 27 28 PB5 ID_IC/I2C2_SCL
GPIO5 / TIM8_CH4 PJ4 29 30 - GND
GPIO6 / TIM12_CH2 PB11 31 32 PB9 GPIO12 / TIM10_CH1
GPIO13 / TIM8_CH1 PJ5 33 34 - GND
GPIO19 / SAI2_FSA PJ3 35 36 PF15 GPIO16 / USART6.CTS
GPIO26 / SDMMC3_D2 PB12 37 38 PJ12 GPIO20 / SAI2_SDA
GND - 39 40 PJ2 GPIO21 / SAI2_SDB

6.2. User buttons and LEDs[edit | edit source]

The tables below describe the GPIO assignments for the user buttons and LEDs. Refer to the LEDs and buttons on STM32 MPU boards article for more details.

GPIO for LEDs

LED color and label GPIO
Orange LED (LD3) PJ6
Red LED (LD1) PH4
Green LED (LD2) PD8
Blue LED (LD4) PJ7

GPIO for user buttons

Button GPIO
USER1 (B5) PD2
USER2 (B4) PA13

7. References[edit | edit source]